Running Next-Generation Policies on OMY with LeRobot
Run GR00T N1.7, MolmoAct2, VLA-JEPA, and FastWAM on OMY with LeRobot and a ROS 2 Zenoh bridge.
LeRobot has recently released four new 2026-generation Vision-Language-Action (VLA) and world models (GR00T N1.7, MolmoAct2, VLA-JEPA, and FastWAM) and trained them on the teleoperation-collected dataset, and ran them on a pick-and-organize long-horizon task on a OMY-F3M arm. This page covers the setup, how the models compare, and how they are deployed.
Full demo
What you'll learn
- How the LeRobot native environment connects to the OMY robot through
lerobot_robot_ros2_zenoh. - How to train and deploy the newest VLA and world-action models on an OMY.
- How these models work, and how they perform once they are on the arm.
1. System Architecture
The models are LeRobot policies, trained with lerobot-train and run with lerobot-rollout. The OMY-F3M
exposes its state and cameras as ROS 2 topics and accepts trajectory_msgs/JointTrajectory commands, so
the two are joined by a bridge that implements LeRobot's Robot interface on top of those topics.

The full control loop, from the arm through the bridge to the policy and back.
- Robot Arm
- Bridge
- Policy
OMY-F3M — 6 joints (joint1–joint6) plus a gripper joint (rh_r1_joint).
Publishes
| Topic | Type |
|---|---|
/joint_states | sensor_msgs/JointState, 7 positions at 30 Hz |
/camera/cam_wrist/.../compressed | wrist camera, mounted on the gripper |
/camera1/image_raw/compressed | external camera, workspace view |
/cam_external2/image_raw/compressed | external camera, second workspace view |
Subscribes to /leader/joint_trajectory (trajectory_msgs/JointTrajectory).
A JointTrajectory is a list of timestamped waypoints, not one setpoint. ros2_control's
JointTrajectoryController interpolates cubic splines between them and closes the servo loop at 400 Hz,
so the arm stays in motion between waypoints.
lerobot_robot_ros2_zenoh — a LeRobot Robot
implementation whose transport is Zenoh.
It registers as ros2_zenoh through RobotConfig.register_subclass, which is what makes
--robot.type=ros2_zenoh valid in any LeRobot command.
Two methods carry the loop
| Method | Direction |
|---|---|
get_observation() | Subscribes to the four topics, decodes the images, and returns observation.state (7 values) plus observation.images.rgb.camera1, .camera2_external, .cam_wrist |
send_action() | Takes 7 action values, applies the velocity and acceleration clamp, and publishes a JointTrajectory |
The clamp bounds are derived from the training dataset, so commanded motion never exceeds what the demonstrations contained.
Any LeRobot policy, loaded from a checkpoint directory or the Hub via --policy.path.
Per control tick
get_observation()returns the observation dict- the preprocessor normalizes it using the dataset statistics
predict_action_chunk()returns a chunk of future joint positionsselect_action()pops one step from that chunk
| Policy | Chunk |
|---|---|
| GR00T N1.7 | 40 steps (≈1.3 s) |
| MolmoAct2, VLA-JEPA | 30 steps (≈1.0 s) |
| FastWAM | 32 steps |
The policy never touches ROS 2. It receives the observation dict the bridge assembled.
The VLAs and world-action models on this page are the ones we tested. The bridge runs any policy LeRobot has, and the SDK can communicate with other ROBOTIS arms, so an OMX or an AI Worker can expand its available models the same way.
2. Running a Trained Policy
This section assumes a trained checkpoint exists and is ready for inference.
The episodes were recorded by teleoperating the arm through
Cyclo Intelligence, which writes a LeRobot dataset
directly; training was lerobot-train on that dataset (§3 and §6). With a checkpoint in hand, running it
on the arm is one command.
1. Install. LeRobot, the bridge, and its Zenoh SDK:
git clone https://github.com/huggingface/lerobot.git
git clone https://github.com/ROBOTIS-GIT/lerobot_robot_ros2_zenoh.git
git clone https://github.com/ROBOTIS-GIT/zenoh_ros2_sdk.git
pip install -e lerobot -e zenoh_ros2_sdk -e lerobot_robot_ros2_zenoh
2. Bring up the arm so it publishes /joint_states and the camera topics. See the
Zenoh quick start.
3. Run the policy. --robot.type=ros2_zenoh is the bridge; --policy.path is any LeRobot
checkpoint, local or from the Hub:
# set these once
CKPT="path/to/checkpoint/pretrained_model"
TASK="your task instruction"
JOINTS='[joint1, joint2, joint3, joint4, joint5, joint6, rh_r1_joint]'
CAMS='{
<camera_key>: {type: ros2, topic: <image topic>, width: <W>, height: <H>, fps: 30, domain_id: <domain>},
...
}'
# run
lerobot-rollout \
--robot.discover_packages_path=lerobot_robot_ros2_zenoh \
--strategy.type=base \
--policy.path="$CKPT" \
--robot.type=ros2_zenoh \
--robot.joint_names="$JOINTS" \
--robot.cameras="$CAMS" \
--task="$TASK" \
--fps=30 --duration=60
LeRobot loads the checkpoint, the bridge carries observations and actions, the arm moves. Swap
--robot.discover_packages_path registers the bridge with LeRobot; without it --robot.type=ros2_zenoh
is rejected as an unknown robot. joint_states_topic and joint_trajectory_topic are omitted because
their defaults already match the OMY.
Swap CKPT for another checkpoint and the rest stays the same. Each <camera_key> must match a camera
name the checkpoint was trained with.
If the policy is too slow to keep up: --inference.type=rtc
A policy that takes longer than one control tick to run leaves the arm without a fresh command. LeRobot's Real-Time Chunking backend covers that gap: it keeps executing the current chunk while the next one is still being computed, and blends the two where they overlap.
lerobot-rollout \
--robot.discover_packages_path=lerobot_robot_ros2_zenoh \
--strategy.type=base \
--policy.path=<checkpoint> \
--inference.type=rtc \
--inference.rtc.execution_horizon=10 \
--robot.type=ros2_zenoh \
--task="..." --fps=30
Useful for the larger VLAs, whose inference latency does not fit inside one control tick.
3. LeRobot v0.6.0
All four models were trained and evaluated on LeRobot v0.6.0.
They are already implemented in LeRobot. The changes below are the policy-side fixes we needed to train and run them on the OMY.
- NaN-gradient guard (
lerobot_train.py): non-finite gradients poison a whole run (VLA-JEPA: 248/873NaNtensors in every later checkpoint), and norm-clipping does not stop them. Skip the step. - Mixed-resolution cameras (
processor_groot.py): 640×480 externals and 424×240 wrist cannot stack into one tensor. Upscale smaller views first. - FastWAM cameras + proprio (
fastwam/*): a 3-camera width that is not a multiple of 16 crashes the Wan VAE (split in units of 16); 7-dim proprio ≠ pretrained dim (pad/truncate). - Inverted gripper (
processor_vla_jepa.py): the gripper mapping was flipped for the OMY joint-position convention (gripper MAE 1.58). Flip the sign. - Backbone LR (
configuration_vla_jepa.py): addqwen_lrfor a separate backbone learning rate.
Three of the fixes, in code (NaN guard, mixed-resolution cameras, inverted gripper)
# NaN/Inf-gradient guard (lerobot_train.py): a single non-finite step poisons every later checkpoint.
_skip_step = not torch.isfinite(grad_norm)
if _skip_step:
logging.warning(f"non-finite grad_norm ({grad_norm.item()}); skipping optimizer step")
optimizer.zero_grad(set_to_none=True)
else:
optimizer.step()
# Mixed-resolution camera stacking for GR00T (processor_groot.py).
# 480x640 externals + 240x424 wrist cannot stack into one (B,T,V,H,W,C) tensor.
shapes = set(c.shape[2:4] for c in cams)
if len(shapes) > 1:
tgt_h = max(s[0] for s in shapes); tgt_w = max(s[1] for s in shapes)
cams = [c if c.shape[2:4] == (tgt_h, tgt_w) else resize_view(c, tgt_h, tgt_w) for c in cams]
# Inverted-gripper fix for VLA-JEPA (processor_vla_jepa.py).
# Targets are {0 = closed/low, 1 = open/high}; emit +1 for OPEN, -1 for closed.
# The original starVLA mapping (1 - 2*(x>thr)) INVERTED this -> gripper MAE 1.58, ~60% agreement.
a[..., gripper_dim] = 2.0 * (a[..., gripper_dim] > threshold).float() - 1.0
4. Task and Data
The arm starts at a fixed home pose. In front of it are three plates: gray (#1), blue (#2), and green (#3), and a rack of slots. The task is to place plate #1 in the first (left-most) slot, plate #2 in the third slot, and plate #3 in the fifth. Each plate is a separate subtask with its own language instruction. A subtask is not a simple pick-and-place, though; the arm must grab the plate at sufficient depth, tilt it, and insert it into the slot.

The OMY-F3M arm and the three-plate / wooden-slot layout used throughout the study.
Dataset. All four models were fine-tuned on the same dataset with 100 episodes,
184,459 frames at 30 fps, three RGB cameras, and a 7-DOF action/state space (six arm joints plus the
gripper joint rh_r1_joint). Actions are absolute joint positions, not deltas.
Data Collection. Every episode was recorded by teleoperating the OMY-F3M through Cyclo Intelligence.

Recording an episode.

Reviewing the episodes.
Three cameras. A wrist RealSense (a close, moving view of the gripper and plate), a top-down camera
(camera1, which sees all plates and slots at once), and a side external camera (camera2_external),
so the policy sees roughly three sides of the workspace.
Camera placement matters because it decides how much of the environment the robot can actually perceive. Thinking of the workspace as a cube, the three cameras must jointly cover enough of its faces for the policy to localize the plates and slots; here it sees the top, front, and right.

Camera layout: wrist RealSense, overview (camera1), and side external (camera2_external).

Camera1 covers the top, cam_wrist the front, camera2_external the right; the bottom, back, and left have no camera.
During inference the cameras are published by the robot and only subscribed to by our tool, so the first step is to bring the camera drivers up on the robot side.
Camera bring-up commands (User computer side)
Each camera runs in its own terminal, inside the open_manipulator Docker container. In every terminal, first enter the container and point Zenoh at the robot (replace robot_ip with the arm's IP):
cd open_manipulator
./docker/container.sh enter
# run these in every terminal/window
export RMW_IMPLEMENTATION=rmw_zenoh_cpp
export ZENOH_CONFIG_OVERRIDE='transport/shared_memory/enabled=true;mode="client";connect/endpoints=["tcp/robot_ip:7447"]'
Two driver packages are used: usb_cam for the two USB cameras and realsense2_camera for the wrist RealSense. Bring each camera up in its own terminal.
Launch one usb_cam node per USB camera:
ros2 run usb_cam usb_cam_node_exe --ros-args \
--remap __node:=usb_cam_NODE \
-p video_device:=DEVICE \
-r image_raw:=CAM_KEY/image_raw \
-r image_raw/compressed:=CAM_KEY/image_raw/compressed \
-r camera_info:=CAM_KEY/camera_info
Fill in the three blanks:
NODEis a unique node name so twousb_camprocesses do not clash, for examplecamera1orexternal2.DEVICEis the V4L2 path for that camera, for example/dev/video6. List the candidates withv4l2-ctl --list-devices. One physical camera often exposes several/dev/videoNnodes, and the one that streams is usually the lowest-numbered capture node.CAM_KEYis the topic namespace, and it must be the exact key the dataset was recorded under (herecamera1andcam_external2). The subscriber matches by this name, so a typo lands the frame nowhere and the policy conditions on a blank image.
Bring the wrist camera up with the RealSense launch file:
ros2 launch realsense2_camera rs_launch.py \
camera_name:=CAM_KEY \
enable_depth:=false \
depth_module.color_profile:=WIDTHxHEIGHTxFPS \
depth_module.enable_auto_exposure:=false \
depth_module.exposure:=EXPOSURE_US \
depth_module.gain:=GAIN
Here CAM_KEY follows the same rule as above (the wrist key is cam_wrist), and WIDTHxHEIGHTxFPS is the color stream profile, for example 424x240x60. Depth is disabled because the policy only reads RGB. EXPOSURE_US and GAIN set a fixed manual exposure (in microseconds) and sensor gain: auto-exposure is turned off so the wrist image does not brighten and darken as the arm moves, which would drift the pixels away from what training saw. Start from 11000 and 25 and adjust until the live image matches the recorded look.
The concrete values used in this study are:
| Camera | CAM_KEY | Driver | Device or profile |
|---|---|---|---|
| Overview | camera1 | usb_cam | /dev/video6 |
| Side | cam_external2 | usb_cam | /dev/video0 |
| Wrist | cam_wrist | realsense2_camera | 424x240x60 |
If a USB camera looks too dark or its color drifts, reset its controls to a neutral baseline. This is only needed when the live image does not match training:
for d in DEVICE_A DEVICE_B; do
v4l2-ctl -d $d --set-ctrl \
brightness=128,contrast=128,saturation=128,sharpness=128,gain=0,backlight_compensation=0,white_balance_automatic=1,auto_exposure=3
done
List the same /dev/videoN devices you launched in place of DEVICE_A and DEVICE_B. The values recenter brightness, contrast, saturation, and sharpness to mid-range, drop the extra gain and backlight compensation, and re-enable automatic white balance and exposure (auto_exposure=3 is the V4L2 automatic mode).
Camera keys must match training. On the subscriber side, each camera's width/height and its image_keys value must match training, not the live stream. A wrong key means the image lands nowhere and the policy will predict on a blank frame.
5. Four Models
Each model is a Vision-Language-Action or World Model policy: it reads the three camera images, the joint state, and (if it uses language) the instruction, and outputs a short chunk of future joint commands. What differs is the visual/language backbone, how the action "head" turns understanding into motion, and how much of the network is actually trained.
Also, note that, compared to regular VLAs that directly translate vision or language data as actions, world models internally simulates how the physical environment will change over time before deciding what to do.
5.1 GR00T N1.7
GR00T N1.7 is NVIDIA's Isaac GR00T, ported into LeRobot. Its backbone is Cosmos-Reason2-2B, a Qwen3-VL-family vision-language model; features are read from an intermediate layer. The action head is a flow-matching cross-attention Transformer (a 32-layer "DiT"): rather than emitting joints directly, it starts from noise and refines a candidate action chunk over a few integration steps, cross-attending to the vision-language features. Chunk length is 40 steps, ~3.1 B parameters.
It is the only model whose backbone stays frozen — only the projector, the vision-language LayerNorm, the action head, and the top four LLM layers are trained (~2.1 B), because a full fine-tune on 100 episodes would erode the pretrained priors.

GR00T N1.7: Cosmos-Reason2-2B backbone + flow-matching DiT action head.
5.2 MolmoAct2
MolmoAct2 is AllenAI's Action Reasoning Model, with three parts: a SigLIP-style vision Transformer, an OLMo-class 7B language model, and a separate flow-matching action expert that cross-attends to the vision-language context. It can also emit discrete "FAST" action tokens, but we use the continuous flow-matching head.
Chunk length 30, ~5.4 B parameters, fully fine-tuned. Only the input word-embedding table (~0.4 B) is frozen, so ~5.0 B are trained. It is the largest trained model here.

MolmoAct2: SigLIP ViT + OLMo LLM + flow-matching action expert.
5.3 VLA-JEPA
VLA-JEPA is a world-model. A frozen Qwen3-VL-2B fuses the images and the instruction; the hidden states of special action tokens condition a flow-matching DiT-B action head (16 layers). Separately, a V-JEPA2 video encoder is meant to predict the latent embedding of the next frame, the Joint-Embedding Predictive Architecture idea of imagining the future in feature space, not pixels.
In this study the world-model branch is switched off (it is auto-disabled when the Qwen backbone is frozen -- using the preconfigured world model but not fine-tuned), so only the ~155 M-parameter action head is trained. Chunk length 30.


VLA-JEPA (frozen Qwen3-VL + V-JEPA2 next-latent predictor + DiT flow head), and its teacher-forcing vs. rollout loss (immediate-step versus multi-step autoregressive forecasting).
5.4 FastWAM
FastWAM is the largest world model here. Its backbone is Wan2.2-TI2V-5B, a video-generation Transformer arranged as a Mixture-of-Transformers: a 5 B-parameter video expert and a smaller action expert share attention, alongside a video VAE and a UMT5-XXL text encoder. The paper's premise is whether a world model must actually imagine future video at test time, or whether that step can be skipped.
The action head is again flow-matching; action horizon 32. ~6 B trainable (full fine-tune), and it does not fit on a 24 GB GPU — forcing the CPU-offload deployment discussed in §8.

FastWAM: Wan2.2-5B video DiT + action expert + UMT5-XXL text encoder + VAE.
What "latent state" and "flow-matching" mean
Every action head above reads a latent state and produces motion by flow-matching.
Latent state. The vision-language backbone does not output joint angles. It squeezes the camera images and the instruction into one compact vector, the latent state, that captures what is in front of the arm and what it was asked to do, as features rather than pixels. Everything downstream reads only this vector.
Flow-matching. The action head does not predict the motion in one shot. It starts from pure random noise and cleans it up over a few small steps, and each step nudges the guess a little closer to a real action, until the noise has become a full (or continuous) chunk of joint commands. The network only has to point the direction of each nudge:
Running that from noise to a clean chunk is the whole sampling process. More steps mean smaller, finer nudges, so the chunk comes out smoother and more accurate but takes longer to compute. That step count is the number of denoising steps each policy's flow-matching head takes.
5.5 At a glance
| GR00T N1.7 | MolmoAct2 | VLA-JEPA | FastWAM | |
|---|---|---|---|---|
| Backbone | Cosmos-Reason2-2B | SigLIP + OLMo 7B | Qwen3-VL-2B (frozen) | Wan2.2-5B video |
| Action head | flow-matching DiT | flow-matching | flow-matching DiT-B | flow-matching |
| World model | none | none | V-JEPA2 (frozen) | Wan video expert |
| Chunk (steps) | 40 | 30 | 30 | 32 |
| Total params | ~3.1 B | ~5.4 B | ~2.5 B | ~6 B |
| Trained params | ~2.1 B | ~5.0 B | ~155 M | ~6 B (full) |
| Fits 24 GB? | yes | no | yes | no |

Total vs. trained parameters. VLA-JEPA trains only its ~155 M head; GR00T about two-thirds of its network (backbone frozen); MolmoAct2 and FastWAM are larger fine-tunes.
6. Training and Offline Accuracy
Each model was trained with its authors' most-recommended or publicly verified configs. The training hardware or GPU count was chosen on size and availability. One thing modified was VLA-JEPA's learning rate (, published); it diverged into NaNs on two runs, so we used .
| GR00T N1.7 | MolmoAct2 | VLA-JEPA | FastWAM | |
|---|---|---|---|---|
| Regime | partial (head + top-4 LLM) | full FT | head-only (Qwen frozen) | full FT |
| Final ckpt | 57643 | 20000 | 230574 | 165000 |
| Hardware | 2×A100-80GB | 4×H100-80GB | 1×RTX 4090 | 2×A100-80GB |
| Wall-clock | ~9 h | ~6 h | ~36 h | ~36 h |
| Global batch | 32 | 32 | 8 | 8 |
| Precision | bf16 | bf16 | bf16 | bf16 |

Training curves (loss vs. step) exported from Weights & Biases.
Offline accuracy (held-out MAE). Before running inference, each checkpoint is scored by replaying held-out episodes and measuring the mean absolute error between commanded and demonstrated joints.
| Model | Held-out arm MAE (rad) | End-effector error | Source (best ckpt) |
|---|---|---|---|
| GR00T N1.7 | 0.017 | 7.5 mm | ckpt 57643, held-out |
| MolmoAct2 | 0.019 | 9.9 mm | ckpt 12000, held-out |
| FastWAM | 0.034 | 24.8 mm | ckpt 105000, held-out |
| VLA-JEPA | 0.038 | 21.2 mm | ckpt 184000, held-out |

Held-out arm MAE as training proceeds. GR00T and MolmoAct2 improve sharply over their (short) schedules; VLA-JEPA and FastWAM stay essentially flat over much longer ones. Read the trend of each line rather than comparing absolute heights; a "step" is not comparable across different batch sizes.
Offline accuracy is not task success. MolmoAct2 is nearly as accurate as GR00T offline (0.019 vs. 0.017 rad). As §8 shows, that did not translate to the robot at all. Low offline MAE is a necessary standard, but does not promise success.
7. Inference Smoothing
A policy returns a chunk of future joint positions each tick, and LeRobot plays it out one step at a time. Each new chunk starts wherever the last one ended, so the command stream steps at every re-plan.
The full inference path is: observe → pre-process → predict → post-process → smooth → clamp → send.

Each tick, one observation becomes a short chunk of future joint commands, smoothed and rate-limited, published as a single trajectory the controller splines at 400 Hz. The arm is homed and approach-ramped once before the loop begins.
7.1 Temporal ensembling & age weighting
Smoothing does not affect the policy itself. It takes whatever chunks a model produces and averages the overlapping ones, so it works with any chunk-predicting policy.
The version used here comes from ACT temporal ensembling, which LeRobot implements as
ACTTemporalEnsembler,
referenced to work on these VLA models as well.
It re-infers every tick, and for each upcoming timestep averages all the overlapping chunk predictions that cover it.

Overlapping chunk predictions are blended by an age weight into one smooth command; the coefficient c controls how strongly the older, committed reach is favored — and that sets grab depth.
The predictions covering a timestep are not equal: some come from a chunk planned several ticks ago,
some from the one just computed. ACT weights each by its age i as wᵢ = exp(-c·i), normalised to sum
to 1, so older predictions count for slightly more.
This matters most on the grasp, which needs depth. An older chunk already planned the full descent, while a chunk re-planned halfway down predicts less descent still to go - so following only the newest one lets the gripper creep back up and stop shallow. Keeping weight on the older plans holds the descent to the depth the policy first committed to, which is where the gain in success rate comes from.
- Without ensembling
- With ensembling
Every joint oscillates while the arm is holding position. The command stream steps at each chunk boundary and the controller follows it.
Joint velocity, all six arm joints, fixed ±66 deg/s axis.
The same six joints on the same axis. Velocity stays at zero through the holds and ramps into each reach.
Joint velocity, all six arm joints, fixed ±66 deg/s axis.
Not only depth - the motion also comes out much smoother.
Why ensembling moves GR00T from 40% to 60%
Plates 1 and 2 are 100% in both chunk and ensembling, so the change is plate 3, and it comes down to grabbing.
At the same instant (orange), the oldest chunk is already at a deep step while the newest restarts shallow. The red arrows are the lag: each chunk's deepest step is discarded and the next chunk begins again near the arm's trailing pose.
Why chunk mode lands short. Every chunk is planned from where the arm is right now, and the arm always trails the command. So at any instant an older chunk is already deep into its reach, while a brand-new chunk is still on its first steps, near the arm's trailing position.
Chunk mode always jumps to the newest chunk, so it keeps restarting from behind and the command settles slightly shallow. This does not wash out with time nor chunk length either, because each chunk is replaced after a few steps due to the late-responding robot, so its deep steps are discarded before the arm ever reaches them and the replacement starts from the same trailing pose.
Why the age weight helps it. That shortfall sits almost entirely in the newest chunks. Giving older chunks more weight lets the chunk that already reached full depth lead the blend, so the command keeps its depth and still follows the live scene. The old chunk keeps contributing after the point where chunk mode would have thrown it away, so depth carries across each seam instead of resetting.
However, it mitigates rather than fixes: the weighting can only re-use plans the policy already produced, so it cannot add reach that was never predicted. Leaning harder on the old plans gets us the last of the depth but may ignore fresh grab corrections. Also, ensembling is nevertheless still an averaging method, mixing chunks and dampening overall actions (with constant, low c). Due to these two, this is maybe why plate 3 is at 60% and not 100%.
A variable c scheduler may fix this issue, with a custom curriculum, but that is set as future work.

Sketch of the idea, not an evaluated result. A fixed c has to serve the whole subtask at once. A scheduled c could stay low while the arm approaches and still tracks the scene, rise into the grasp where the committed depth matters, then relax again for the lift and place.
Smoother motion helps too. The blend is continuous across the seams, so the arm stops decelerating and re-accelerating at every re-plan (because of robot latency, following newest chunk). That removes the start-stop jerk of chunk mode, which matters most as the gripper closes.
Implementing it
LeRobot's ACTTemporalEnsembler, for reference. It keeps a running average rather than a history: the weights
are fixed up front, and each update folds the new chunk into the average it already holds.
# lerobot/policies/act/modeling_act.py, abridged
self.ensemble_weights = torch.exp(-temporal_ensemble_coeff * torch.arange(chunk_size))
self.ensemble_weights_cumsum = torch.cumsum(self.ensemble_weights, dim=0)
def update(self, actions):
self.ensembled_actions *= self.ensemble_weights_cumsum[self.ensembled_actions_count - 1]
self.ensembled_actions += actions[:, :-1] * self.ensemble_weights[self.ensembled_actions_count]
self.ensembled_actions /= self.ensemble_weights_cumsum[self.ensembled_actions_count]
self.ensembled_actions_count = torch.clamp(self.ensembled_actions_count + 1, max=self.chunk_size)
return self.ensembled_actions[:, 0] # oldest timestep is executed and popped
Around a policy that has no such flag, the same idea written out: keep the chunks still in flight, weight each prediction by its age, average.
import numpy as np
buffer = [] # [age, chunk] for chunks still in flight
def step(observation, policy, c=0.01):
chunk = policy.predict_action_chunk(observation)[0] # (horizon, n_joints)
buffer.append([0, chunk])
votes = [(age, ch[age]) for age, ch in buffer if age < len(ch)]
ages = np.array([a for a, _ in votes], dtype=np.float32)
w = np.exp(-c * ages); w /= w.sum() # older predictions weigh more
action = np.sum([wi * a for wi, (_, a) in zip(w, votes)], axis=0)
for entry in buffer:
entry[0] += 1
buffer[:] = [e for e in buffer if e[0] < len(e[1])]
return action
8. Deployment Results
Success is measured per plate and split into grab (did the arm pick the plate up) and place (did it seat the plate). "Task" is the full three-plate completion; place can never exceed grab. Each rate is first-try success over 10 trials per plate with the robot.
| Model | P1 grab | P1 place | P2 grab | P2 place | P3 grab | P3 place | Task |
|---|---|---|---|---|---|---|---|
| GR00T N1.7 | 100 | 100 | 100 | 100 | 50 | 40 | 40 |
| GR00T N1.7 + ensemble | 100 | 100 | 100 | 100 | 60 | 60 | 60 |
| MolmoAct2 | 20 | 0 | 0 | 0 | 0 | 0 | 0 |
| VLA-JEPA | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| FastWAM | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
GR00T completed plates 1 and 2 every time. Plate 3 is harder because it requires extending the arm further, and the ensemble mode lifted it from 50/40 to 60/60. MolmoAct2 managed only a partial first grab; VLA-JEPA and FastWAM did not grasp the first plate at all.
Inference latency (one predict_action_chunk on a single RTX 4090; "per action" divides by chunk
length). All are at 30 Hz.
| Model | Latency (ms/chunk) | Chunk | Per action (ms) | Notes |
|---|---|---|---|---|
| GR00T N1.7 | 76 | 40 | 1.90 | n/a |
| GR00T N1.7 + ensemble | 76 | 40 | 1.90 | no additional latency cost |
| MolmoAct2 | 137 | 30 | 4.57 | n/a |
| VLA-JEPA | 74 | 30 | 2.47 | n/a |
| FastWAM | 240 | 32 | 7.5 | 5B DiT needs CPU offload |
Only GR00T N1.7 with ensembling completes the task best, but plate 3 needs to be trained more. MolmoAct2 moves okay and grabbed the first plate about one run in five but never finished; more training doesn't seem to improve. VLA-JEPA is strong offline yet fails to grasp on the arm. FastWAM produces sensible chunks but its 5 B video DiT does not fit on 24 GB (the UMT5 text encoder stays on the CPU), carries the highest per-chunk latency, and also fails.
9. Limitations
The table summarizes where each model falls short on this setup.
| Model | Main limitations |
|---|---|
| GR00T N1.7 | Plate 3 only ~50-60%; occasionally dwells at the initial position before starting; requires ≥24 GB GPU. |
| MolmoAct2 | ~5B params; training needs 4×80 GB; 12k checkpoint grasps but never completes; training converged, but further steps did not improve it. |
| VLA-JEPA | Low offline error; flow head sensitive to learning rate; world model imagination dropped at inference. |
| FastWAM | ~6B params; highest latency, CPU offload required; native action space mismatched to a joint-space robot. |
10. Practical Tips
The smoothing command run on the robot
On the robot, bring the arm controller up in its smoothed ros2_control mode before inference. This loads the smoothed
control profile, so the servos ease between waypoints instead of snapping to each one:
ros2 launch open_manipulator_bringup omy_f3m_follower_ai.launch.py ros2_control_type:=omy_f3m_smooth
11. Resources
- LeRobot: training/inference framework
- ROBOTIS lerobot_robot_ros2_zenoh: the ROS2/Zenoh transport
- GR00T N1.7 · MolmoAct2 · FastWAM · VLA-JEPA · LeRobot Policies