Skip to main content

GPT-6 Astra on the AI Worker

· 19 min read

Connect GPT-6 Astra to AI Worker through the Codex App Server and ROS 2 to carry out natural-language instructions.

1. Overview​

This technical story explains how we connected GPT-6 Astra to AI Worker so the robot could carry out natural-language instructions using camera images and robot state. It walks through the system, shows how to run it, and shares what we learned from pick-and-place tasks.

By the end, you will understand how to:

  • Connect model decisions to robot actions. Follow the loop from the Codex App Server through the harness to ROS 2 commands, and see how execution results and new observations guide the next action (Section 2).
  • Run a task in simulation or on a real robot. Set up Codex, launch Gazebo or a real SG2, start an episode, and follow it in the live viewer (Section 3).
  • Work with the robot tools. Understand the available actions, coordinate conventions, units, and observation checks used by the harness (Section 4).
  • Assess the approach's strengths and limitations. Review examples of feedback-based recovery, the tradeoffs of smaller movements, and limitations involving depth, collisions, repeatability, and response time (Sections 5–6).

The demos illustrate these ideas through shelf-to-basket picking and ball placement. The robot adjusts its lift to reach objects, pulls a basket closer with its free hand, or moves its base to carry an object to the basket. These examples show how different action sequences can achieve the same goal.

The harness uses the Codex App Server, allowing newly supported models to be evaluated with the same robot tools and execution environment.


2. System Architecture​

Codex system architecture overview

Codex system architecture

Each task runs in one Codex App Server session. The model selects a robot tool and its inputs; the App Server routes the call to the harness.

The harness validates the tool inputs and execution conditions, then creates a ROS 2 message for the target component and publishes it to the corresponding topic. Arm commands specify a target position and orientation, along with a motion duration. Gripper, head, and lift commands specify target joint values and a motion duration. Base commands specify linear and angular velocities.

After publishing a command, the harness checks the robot's actual state to determine whether it has reached the target and assess the motion result. It then collects camera images and robot state and returns them to the model along with the execution result. The model uses this feedback to decide its next action. This cycle continues until the task ends.

The following table lists the control topics and message types used by the harness.

ComponentTopicMessage typeCommand contents
Left arm/l_goal_moverobotis_interfaces/msg/MoveLTarget position and orientation, motion duration
Right arm/r_goal_moverobotis_interfaces/msg/MoveLTarget position and orientation, motion duration
Left gripper/leader/joint_trajectory_command_broadcaster_left/raw_joint_trajectorytrajectory_msgs/msg/JointTrajectoryTarget gripper joint values, motion duration
Right gripper/leader/joint_trajectory_command_broadcaster_right/raw_joint_trajectorytrajectory_msgs/msg/JointTrajectoryTarget gripper joint values, motion duration
Head/leader/joystick_controller_left/joint_trajectorytrajectory_msgs/msg/JointTrajectoryTarget head joint values, motion duration
Lift/leader/joystick_controller_right/joint_trajectorytrajectory_msgs/msg/JointTrajectoryTarget lift joint values, motion duration
Base/cmd_velgeometry_msgs/msg/TwistLinear and angular velocities

3. Getting Started​

Follow the common setup, then choose Gazebo or Real SG2. The live viewer is optional.

  1. Set up: Clone the code, start the container, install Codex, and sign in (3.1).
  2. Run: Start Gazebo (3.2) or the real robot (3.3), then start Cyclo and an episode.
  3. Watch (optional): Open the live viewer (3.4).

Keep four terminals open for a run:

TerminalGazeboReal SG2
1ZenohZenoh
2GazeboRobot bringup
3Cyclo motion controllerCyclo motion controller
4Episode: run_codex_gazebo.pyEpisode: run_codex.py

Run the clone and container-management commands on the host. Run subsequent robot commands inside the container unless otherwise noted. Use ./container.sh enter from ai_worker/docker for each additional terminal.

3.1 Common Setup​

Before You Start​

Gazebo

If you will run Gazebo on a PC with an NVIDIA GPU, read the tip at the start of 3.2 before ./container.sh start.

Real SG2

Before starting the container, complete the Real SG2 preparation checklist. It covers power, USB connections, network access, cameras, and workspace safety.

Step 1 - Clone the Code and Start the Container (Host)​

git clone -b feature-codex https://github.com/ROBOTIS-GIT/ai_worker.git
cd ai_worker/docker
./container.sh start
./container.sh enter

Step 2 - Install Codex​

The installation does not persist when the container is recreated. If codex --version already returns a version number, skip this step.

mkdir -p /root/.codex_robot && chmod 700 /root/.codex_robot
curl -fsSL https://chatgpt.com/codex/install.sh -o /tmp/codex-install.sh
CODEX_HOME=/root/.codex_robot CODEX_INSTALL_DIR=/usr/local/bin sh /tmp/codex-install.sh
codex --version

At the end the installer asks Start Codex now? [y/N]. Answer N.

/root/.codex_robot and /usr/local/bin/codex must match codex.home and codex.bin in both config files. Don't set codex.home to /root/.codex, the default location for interactive Codex: the harness writes and deletes config.toml in that folder on every run.

The installer installs the latest Codex. This version of the harness was tested with Codex 0.163.0.

Step 3 - Sign In to Codex​

Choose one of the two sign-in methods below. Always prefix login commands with CODEX_HOME=/root/.codex_robot so the harness can find your credentials. Without this prefix, Codex saves them to /root/.codex. The harness uses the saved sign-in and does not pass an API key to Codex directly.

  • Option A: OpenAI API Key (usage-based billing)

    read -rsp 'OpenAI API key: ' CODEX_LOGIN_KEY; printf '\n'

    Input your OpenAI API key, then run:

    printf '%s' "$CODEX_LOGIN_KEY" | CODEX_HOME=/root/.codex_robot codex login --with-api-key
    unset CODEX_LOGIN_KEY

    Paste only the read command first, enter your API key, and press Enter. Then paste the remaining commands. If you paste everything at once, the subsequent lines will be read as the API key. Your key will not be displayed as you type.

  • Option B: Sign in to ChatGPT account via device code (uses your ChatGPT plan's quota)

    CODEX_HOME=/root/.codex_robot codex login --device-auth

    The terminal displays a URL and a one-time code. Open the URL in a browser on any device, sign in to ChatGPT, and enter the code. Sign-in completes automatically in the terminal. No browser is required inside the container.

Check the result with either method:

CODEX_HOME=/root/.codex_robot codex login status
Do not start interactive Codex with this CODEX_HOME

Running plain codex with CODEX_HOME=/root/.codex_robot creates /root/.codex_robot/config.toml and leaves a background codex app-server --managed-daemon process running. The harness writes its own config.toml for each run and refuses to start if the file already exists (config.toml exists; another run may be active).

If you already did, make sure no episode is running, stop the codex app-server --managed-daemon processes (pgrep -af 'codex app-server'), and delete /root/.codex_robot/config.toml.

Step 4 - Start Zenoh (Terminal 1)​

Both setups below use Terminal 1 for Zenoh. Keep it running.

zenohd
Optional: change the model or execution settings

The harness defaults to gpt-6-astra (reasoning effort low). To use a different model or reasoning effort, edit the model: block in both config files:

  • /root/ros2_ws/src/ai_worker/ffw_codex/config_gazebo.yaml (Gazebo)
  • /root/ros2_ws/src/ai_worker/ffw_codex/config.yaml (real SG2)

These files also contain other settings, including episode limits, per-move step limits, tolerances, and base motion limits. You can change these settings in the same way.

3.2 Run in Gazebo​

Pick and Place in Gazebo

Use the NVIDIA GPU for Gazebo

docker/docker-compose.yml in this branch doesn't give the container a GPU, so Gazebo renders on the CPU and runs slowly. On a PC with an NVIDIA GPU and the NVIDIA Container Toolkit, add the following to the ai_worker service before ./container.sh start in 3.1 Step 1:

environment:
- NVIDIA_DRIVER_CAPABILITIES=all
- __NV_PRIME_RENDER_OFFLOAD=1
- __GLX_VENDOR_LIBRARY_NAME=nvidia
gpus: all

Add the three entries to the existing environment: list, and gpus: all at the same level as privileged: true. If the container is already running, ./container.sh stop and start recreate it, so you have to redo Codex installation and sign-in (3.1 Step 2–3).

Terminal 2: Gazebo

ros2 launch ffw_bringup ffw_sg2_follower_ai_gazebo.launch.py \
world:=/root/ros2_ws/src/ai_worker/ffw_bringup/worlds/table \
use_cam:=true
  • use_cam:=true is required. It defaults to false, and without the cameras the harness times out while waiting for observations.
  • Give world:= without the .sdf extension. You can use other worlds in ffw_bringup/worlds/ as well, but the example task in Terminal 4 assumes table. To reset the scene between runs, restart the Gazebo launch in Terminal 2.
  • RViz opens too but isn't used. Run pkill rviz2 to save resources.
Optional: explore other Gazebo worlds
World fileScene contentsMain tasksExample instruction
table.sdfTable, blue cube, black cubeBasic grasping, single-arm motion checks"pick up the blue block"
tabletop_sorting.sdfTable, red and blue bins, five cubes, yellow cylinderSorting by color, pick-and-place, stacking"put the red cubes in the red bin"
shelf_lift.sdfTwo-tier shelfMoving forward, lowering the lift, and tilting the head down to access the lower shelf"take the green cube from the lower shelf and put it on the orange square"
articulated_cabinet.sdfCabinet with a drawer, box with a lid, three cubesOpening and closing drawers and lids"open the drawer and take out the blue cube"
kitchen_counter.sdfKitchen counter with a plate, bowl, two cans, apple, cereal box, sponge, and cutting boardPick-and-place using everyday object names"put the apple in the bowl"
pick_and_deliver.sdfTwo rooms connected by a doorway, starting table with three cubes, green and blue tables, obstacles, colored wall panelsPicking up and delivering objects across rooms"bring the blue cube to the blue bin"

Gazebo tabletop_sorting

Gazebo tabletop_sorting.sdf

Gazebo tabletop_sorting.sdf

Terminal 3: Cyclo

ros2 launch cyclo_motion_controller_ros ai_worker_controller.launch.py controller_type:=movel

The arms and grippers are controlled through Cyclo. Commands for the head and lift are sent directly to their respective trajectory topics. While Cyclo is running, do not publish commands directly to the arm controllers' topics.

Terminal 4: Episode

cd /root/ros2_ws/src/ai_worker/ffw_codex
python3 run_codex_gazebo.py --task "pick up the blue block" --run-id gz_01

Use a new --run-id for each run; an existing run folder is not reused.

Head and lift commands have no timeout in Gazebo

In Gazebo, head and lift commands wait until the joint stops moving, since the simulated lift can be much slower than commanded. The model is idle and uses no tokens meanwhile.

3.3 Run on a Real SG2​

Pick and Place on a Real SG2

Before You Start​

Complete this checklist before starting the container in 3.1 Step 1.

  • Power on the robot and connect the follower board and cameras via USB before running ./container.sh start, which installs and reloads the udev rules. Verify that /dev/follower exists.
  • Connect the robot's onboard Jetson AGX Orin to the internet via an Ethernet cable and keep it connected throughout the episode. Codex communicates with the model over the network, so a lost connection interrupts the episode.
  • RealSense serial numbers vary by robot. Use rs-enumerate-devices to check them, then set camera1_serial and camera2_serial in ffw_bringup/config/common/rs_serial.yaml to match your robot.
  • The ZED head camera must be connected. head_camera_type defaults to zed.
  • Clear the robot's workspace and keep the emergency stop button within reach. The robot moves during bringup (init_position) and during the episode. Commands already sent by the episode cannot be canceled by the harness.

Terminal 2: Bringup

ros2 launch ffw_bringup ffw_sg2_follower_ai.launch.py

The bringup waits 10 seconds after the initial pose is set before it starts the swerve drive controller, to give the hardware more time to settle. Wait for the hardware to initialize, then check from another terminal:

timeout 7 ros2 control list_controllers # arm, head, lift controllers active
timeout 7 ros2 topic echo --once /joint_states # includes gripper, head, lift joints
ros2 topic list | grep -E "zed|camera_left|camera_right"

If /joint_states lists only the wheel joints, the follower hardware hasn't come up. Check /dev/follower, the power, and the bringup log.

Terminal 3: Cyclo

ros2 launch cyclo_motion_controller_ros ai_worker_controller.launch.py controller_type:=movel

Terminal 4: Episode

cd /root/ros2_ws/src/ai_worker/ffw_codex
python3 run_codex.py --task "task description" --run-id real_01

Use a new --run-id for each run; an existing run folder is not reused.

  • Write the task to match the actual scene.
  • For the first run, lower episode.max_actions and episode.max_seconds in config.yaml.
  • For delicate work, reduce limits.max_step_m in config.yaml (currently 0.1 m per move) to limit how far the hand can move in a single step.
  • Pressing Ctrl+C prevents new actions and waits for the current tool call to finish. It does not stop the robot. In an emergency, use the emergency stop button.
  • When the episode ends, the robot remains in its last pose. Manually return the robot and objects to their initial positions before the next run.

3.4 Watch a Run Live​

Tidy up the table

ffw_codex/run_viewer.html displays live camera feeds from the robot and tracks the episode as it runs. It shows the rationale, command, and result for each tool call, along with the observation used by the model. It works with both Gazebo and the physical robot.

1. Start the video bridge

The live cameras come from web_video_server on port 7085, which cyclo_intelligence starts with its orchestrator bringup. Start cyclo_intelligence on the same machine as the bringup.

Host

git clone https://github.com/ROBOTIS-GIT/cyclo_intelligence.git
cd cyclo_intelligence/docker
./container.sh start
./container.sh enter

Container

cyclo_intelligence

2. Open the viewer through Live Server

In VS Code, open the ai_worker folder (over Remote-SSH for the robot), right-click ffw_codex/run_viewer.html and choose Open with Live Server. The page must be opened through Live Server (for example http://localhost:5500/ffw_codex/run_viewer.html). Following a run doesn't work from a file opened by double-click. Over SSH, forward ports 5500 and 7085 to your PC.

3. Connect the cameras

Open Live cameras, keep the bridge URL http://localhost:7085, choose the topic preset (Robot or Gazebo), and click Connect / Reconnect. The presets match the cameras: topics in config.yaml and config_gazebo.yaml. If you change those topics, change the fields in the viewer too.

4. Follow the run

Enter the --run-id of the episode (e.g. gz_01) under Run folder and click Follow run.

The page checks ffw_codex/runs/<run_id>/ for updates approximately every 1.2 seconds and stops polling when host_result.json appears. Live camera streams remain connected.

  • The live cameras and the call records aren't synchronized. The model decided from the saved observation, not from the live image.

4. Robot Tools for the Model (Harness)​

4.1 Tool List​

ToolRoleMain inputs
robot_startStart the episode and obtain the initial observationNone
robot_observeObtain updated images from all three cameras and the robot stateNone
robot_moveChange the position and orientation of one handarm, x, y, z, roll, pitch, yaw
robot_gripperAdjust how far one gripper is open or closedarm, value
robot_headAdjust the head's tilt and panhead_joint1, head_joint2
robot_liftAdjust the upper-body heightposition_m
robot_baseTranslate and rotate the mobile basevx, vy, wz, duration_s
robot_execute_planExecute a short sequence of actions in ordersteps
task_completeDeclare task completion and end the episodereason explaining why the task is complete

robot_execute_plan accepts up to 5 steps (plan.max_steps) of robot_move, robot_gripper, robot_head, and robot_lift; robot_base is not allowed. A head, lift, or gripper step must be the last step. Each step runs only after the previous one returns arrived, and the harness does not interpret intermediate images.

The action tools, robot_execute_plan, and task_complete also require the following inputs:

  • request_id: The action_context.request_id from the latest response. This links the request to a valid observation.
  • reason: The observed evidence and the purpose of the action. For example: "The object is between the fingers, so close the gripper."

These two inputs are not required for robot_start or robot_observe. Call robot_start once at the beginning of the episode, then use robot_observe to refresh observations.

4.2 Coordinates and Units​

robot_move takes an absolute target position and orientation for the selected hand.

  • The reference frame is base_link: x points forward, y points left, and z points up.
  • Positions are in meters, and angles are in radians.
  • arm must be left or right.
  • roll, pitch, and yaw specify the end-effector orientation. They are neither individual wrist joint angles nor rotation offsets added to the current orientation.
  • Rotations are interpreted as Rz(yaw) · Ry(pitch) · Rx(roll). Setting all three angles to 0 requests the zero orientation.

For robot_gripper, a value of 0 means fully open, and 1 means the configured maximum closure. robot_head takes the absolute angles of its two joints, while robot_lift takes the absolute displacement of the lift joint. The lift is at its highest position at 0 m; increasingly negative values lower it.

robot_base takes velocities and an execution duration rather than a target position. vx and vy specify forward and leftward velocities (m/s), and wz specifies counterclockwise angular velocity (rad/s). duration_s includes acceleration and deceleration time.

4.3 Observation Validity Checks​

Each action request includes the request_id from the latest response. The harness uses it to verify that the model's request is linked to a valid observation.

Immediately before an action, the harness checks the time elapsed since the observation and the current robot state. If the observation has expired, the robot state has changed beyond the allowed tolerances, or the measurements are stale, the harness does not send the command and requires a new observation. It also blocks the next action while the base is still moving.


5. Observations​

  • Task execution without depth or predefined scene coordinates
    AI Worker is equipped with LiDAR and depth cameras, but the current harness did not use their distance measurements. The model was not given the desk height or the objects' positions or distances in advance. Even so, it performed the tasks by adjusting its approach height and travel distance based on RGB images and robot state.

  • Using feedback during a task
    Within an episode, the model used the results of previous actions to inform its next decisions. The recoveries shown in the demos, such as lowering the lift or pulling the basket closer, were not scripted in the harness; the model chose them from the returned results and observations.

  • Differences across reasoning effort levels
    We expected higher reasoning effort (high vs. low) to improve task success rates, but we observed no clear difference across the tasks and runs tested.

  • Maximum movement distance and token usage
    Reducing the maximum distance allowed per command limits.max_step_m increased token usage and episode time but also improved task success rates in our tests. Smaller movements appear to have helped by providing more opportunities to observe the scene and correct subsequent actions.


6. Limitations and Next Steps​

  • Lower success rates for tasks involving height differences
    Pick-and-place tasks between tables at different heights had lower success rates than tasks on a single table. Because the harness does not use depth measurements, the model must estimate height differences from RGB images alone.

  • Variability in task execution
    Even with the same instruction in the same environment, the model varied its action sequence and approach. While this produced different solutions, it limited the repeatability of specific motions.

  • Limited collision response during motion
    Once a motion command begins executing, the model receives no intermediate observations, so it cannot detect or respond to a collision until the motion ends. This applies to every step of robot_execute_plan, and commands already sent cannot be canceled by the harness.

  • Waiting for model responses
    Each step requires a model response, causing pauses between actions and limiting suitability for tasks that require rapid responses. Smaller step sizes, which improved success rates (Section 5), also increase the number of these pauses.

We plan to evaluate newly supported models on the same robot tasks and compare their performance. We also plan to extend the harness beyond the Codex App Server so that other models, such as Claude, can use the same robot tools.