Skip to main content

Navigation

WARNING: While following these instructions, your TurtleBot3 may move and rotate unexpectedly. Please place the robot in safe location on the ground.

info

NOTE

  • Navigation should be run on the Remote PC.
  • Make sure to launch Bringup on your TurtleBot3 before executing the following operations.
  • Navigation uses maps created by SLAM. Please prepare a map before running Navigation.

Navigation is used move the robot from one location to a specified destination in a given environment. For this purpose, a map that contains geometry information describing furniture, objects, and walls of the given environment is required. As described in the previous SLAM section, a map was created with the distance information obtained by the sensor and the pose information of the robot itself.

Run Navigation Nodes

  1. If Bringup is not running on the TurtleBot3 SBC, launch Bringup.
  • Open a new terminal from Remote PC with Ctrl + Alt + T and connect to Raspberry Pi with its IP address. The default password is ubuntu.
    [Remote PC]
$ ssh ubuntu@{IP_ADDRESS_OF_RASPBERRY_PI}
$ export TURTLEBOT3_MODEL=${TB3_MODEL}
$ ros2 launch turtlebot3_bringup robot.launch.py
  1. Open a new terminal from Remote PC with Ctrl + Alt + T and launch the Navigation node. ROS 2 uses [Navigation2][nav2]. Specify your TurtleBot3 model (burger, waffle, waffle_pi) using the TURTLEBOT3_MODEL parameter.
    [Remote PC]
$ export TURTLEBOT3_MODEL=burger
$ ros2 launch turtlebot3_navigation2 navigation2.launch.py map:=$HOME/map.yaml

How to save the TURTLEBOT3_MODEL parameter?

The $ export TURTLEBOT3_MODEL=${TB3_MODEL} command can be omitted if the TURTLEBOT3_MODEL parameter is predefined in your .bashrc file.
The .bashrc file is automatically loaded when a terminal window is created.

  • Example defining TurtlBot3 Burger as the default model.
    [Remote PC]
$ echo 'export TURTLEBOT3_MODEL=burger' >> ~/.bashrc
$ source ~/.bashrc
  • Example defining TurtlBot3 Waffle Pi as the default model.
    [Remote PC]
$ echo 'export TURTLEBOT3_MODEL=waffle_pi' >> ~/.bashrc
$ source ~/.bashrc

Estimate Initial Pose

Initial Pose Estimation must be performed before running Navigation as this process initializes the AMCL parameters that are critical for Navigation. The TurtleBot3 has to be correctly located on the map with LDS sensor data that overlaps the displayed map.

  1. Click the 2D Pose Estimate button in the RViz2 menu.
  2. Click on the map where the actual robot is located and drag the large green arrow toward the direction where the robot is facing.
  3. Repeat step 1 and 2 until the LDS sensor data is overlayed on the saved map.
  4. Launch the keyboard teleoperation node to precisely locate the robot on the map.
    [Remote PC]
$ ros2 run turtlebot3_teleop teleop_keyboard
  1. Move the robot back and forth a bit to collect the surrounding environment information and narrow down the estimated location of the TurtleBot3 on the map (displayed with tiny green arrows).
  2. Terminate the keyboard teleoperation node with Ctrl + C to prevent different cmd_vel values from being published from multiple nodes during Navigation.

Set Navigation Goal

  1. Click the Navigation2 Goal button in the RViz2 menu.
  2. Click on the map to set the destination of the robot and drag the green arrow toward the direction where the robot will be facing.
  • This green arrow is a marker to can specify the destination of the robot.
  • The root of the arrow is the x, y coordinate of the destination, and the angle θ is determined by the orientation of the arrow.
  • As soon as x, y, θ are set, the TurtleBot3 will start moving to the destination immediately.

Read more about Navigation2

  • The robot will create a path to reach the Navigation2 Goal based on the global path planner. Then, the robot moves along the path. If an obstacle is placed in the path, Navigation2 will use local path planner to avoid the obstacle.

  • Setting a Navigation2 Goal might fail if the path to the Navigation2 Goal cannot be created. If you wish to stop the robot before it reaches to the goal position, set the current position of TurtleBot3 as a Navigation2 Goal.

  • [Official ROS2 Navigation2 Wiki][nav2]

Tuning Guide

The Navigation2 stack has many parameters to change performances for different robots. Although it's similar to ROS1 Navigation, please refer to the Configuration Guide of Navigation2 or ROS Navigation Tuning Guide by Kaiyu Zheng for more details.

Costmap Parameters

inflation_layer.inflation_radius

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • This parameter defines an inflation area of inaccesability around detected obstacles. Generated paths will be planned not to cross this area. It is safe to set this value to be slightly bigger than robot radius. For more information, please refer to costmap_2d wiki.

inflation_layer.cost_scaling_factor

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • This is an inverse proportional factor that is multiplied by the value of the costmap. If this parameter is increased, the value of the costmap is decreased.

The optimal path for the robot to pass through obstacles is to take a median path between them. Setting a smaller value for this parameter will create a farther path from the obstacles.

dwb_controller

max_vel_x

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • This factor sets the maximum value for translational velocity.

min_vel_x

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • This factor sets the minimum value for translational velocity. If set this negative, the robot can move backwards.

max_vel_y

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The maximum y velocity for the robot in m/s.

min_vel_y

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The minimum y velocity for the robot in m/s.

max_vel_theta

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • Value setting the maximum rotational velocity. The robot can not spin faster than this.

min_speed_theta

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • Value setting the minimum rotational velocity. The robot can not spin slower than this.

max_speed_xy

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The absolute value of the maximum translational velocity for the robot in m/s.

min_speed_xy

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The absolute value of the minimum translational velocity for the robot in m/s.

acc_lim_x

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The x acceleration limit of the robot in meters/sec^2.

acc_lim_y

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The y acceleration limit of the robot in meters/sec^2.

acc_lim_theta

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The rotational acceleration limit of the robot in radians/sec^2.

decel_lim_x

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The deceleration limit of the robot in the x direction in m/s^2.

decel_lim_y

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The deceleration limit of the robot in the y direction in m/s^2.

decel_lim_theta

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The deceleration limit of the robot in the theta direction in rad/s^2.

xy_goal_tolerance

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The x,y distance allowed when the robot reaches its goal pose.

yaw_goal_tolerance

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The yaw angle allowed when the robot reaches its goal pose.

transform_tolerance

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • The allowance for latency for tf messages.

sim_time

  • Defined in turtlebot3_navigation2/param/${TB3_MODEL}.yaml
  • This factor sets forward simulation time in seconds. Setting this too small makes it difficult for the robot to pass through narrow spaces while large values limit dynamic turns. You can observe the differences in length of the yellow line in the below image that representing the simulation path.