Skip to main content

home_service_challenge

TurtleBot3 Home Service Challenge

note

NOTE:

Home Service Challenge Stadium and Objects

Getting Started

note

NOTE: Be sure to complete the following instructions before installing Home Service Challenge packages in the pc.

Prerequisites:

  • ROS 2 Humble installed Laptop or desktop PC.
  • This instruction is based on Gazebo simulation.

Remote PC Setup
Install Home Service Challenge packages.
[Remote PC]

$ cd ~/turtlebot3_ws/src/
$ git clone -b humble https://github.com/ROBOTIS-GIT/turtlebot3_home_service_challenge.git
$ cd ~/turtlebot3_ws && colcon build --symlink-install

Simulation

Simulate TurtleBot3 with OpenMANIPULATOR-X in Gazebo.
[Remote PC]

  1. Run the Gazebo Simulation.
$ ros2 launch turtlebot3_manipulation_gazebo turtlebot3_home_service_challenge.launch.py

gazebo_simulation

  1. Run a Nav2 for Gazebo and set 2D Pose Estimate in Rviz.
$ ros2 launch turtlebot3_home_service_challenge_tools navigation2.launch.py

simulation_rviz

  1. Run the core package used to carry out Home Service Challenge's mission.
$ ros2 launch turtlebot3_home_service_challenge_core core_node.launch.py

NOTE: core_node contains nodes for ArUco marker detection, parking, and manipulator control, which core_node uses to perform scenario integration control. The core_node performs and controls the behavior in the scenario sequence. After running core_node, we can see the TF of the ArUco marker in rviz and we can run the scenario. See Missions for more detailed descriptions and to run the scenario.

Actual robot

Ready for actual robot

  • If you want to run the scenario with TurtleBot3 with OpenMANIPULATOR-X, check the below lists.
    • Create a custom map, then create and save the map with SLAM.
    • Set up the Rpi-camera.

Run Home Service Challenge with actual robot

  1. Run hardware bringup.
    [TurtleBot SBC]
$ ros2 launch turtlebot3_manipulation_bringup hardware.launch.py
  1. Run camera node.
    [TurtleBot SBC]
$ ros2 run camera_ros camera_node --ros-args -p format:='RGB888' -p width:=320 -p height:=240
  1. Run a Nav2 and set 2D Pose Estimate in Rviz. If you want to use a custom map, run it with the launch argument.
    [Remote PC]
$ ros2 launch turtlebot3_home_service_challenge_tools navigation2.launch.py map_yaml_file:=$HOME/map.yaml
  1. Run the core package used to carry out Home Service Challenge's mission. Specify the launch mode and ArUco marker size with the launch argument.
    [Remote PC]
$ ros2 launch turtlebot3_home_service_challenge_core core_node.launch.py launch_mode:='actual' marker_size:=0.04

Arguments
launch_mode

  • default: simulation
  • describtion: Select whether you want to run the Home Service Challenge as a simulation or as an actual robot.

marker_size

  • default: 0.088

  • describtion: Specifies the size of the ArUco markers used in the custom map.

    NOTE: core_node contains nodes for ArUco marker detection, parking, and manipulator control, which core_node uses to perform scenario integration control. The core_node performs and controls the behavior in the scenario sequence. After running core_node, we can see the TF of the ArUco marker in rviz and we can run the scenario. See Missions for more detailed descriptions and to run the scenario.

Missions

Commands

Use the following commands during Home Service Challenge.
[Remote PC]
Individual actions

  • Park in front of the ArUco marker: Put the marker's ID for integer to $MARKER_ID.

    $ ros2 topic pub -1 /target_marker_id std_msgs/msg/Int32 "{data: $MARKER_ID}"

    NOTE: When using this command, be sure to include one of the ArUco marker's ID from a scenario.yaml file. In the provided map, IDs 0 through 7 exist. For detailed information on the scenario, see Configuration description below at this section.

  • Control Manipulator : Use the Manipulator to pick up or place objects.

$ ros2 topic pub -1 /manipulator_control std_msgs/msg/String "{data: 'pick_target'}"
$ ros2 topic pub -1 /manipulator_control std_msgs/msg/String "{data: 'place_target'}"

Run scenario
TurtleBot3 will perform individual actions for $SCENARIO_NAME based on the scenario written.

$ ros2 topic pub -1 /scenario_selection std_msgs/msg/String "{data: '$SCENARIO_NAME'}"

NOTE: When using this command, be sure to include one of the scenario name from a scenario.yaml file. The provided scenario file contains room1 through room4. For detailed information on the scenario, see Details description below at this section.

Configuration

Modify data in configuration files according to the given environment.
[Remote PC]

  • scenario.yaml : This file contains a scenario's data. In the simulation, there are initially markers on the front of the TurtleBot with ID 0 through 3, which are assigned as target_marker_id. And in each room, there are markers with ID 4 through 7.
    • File Path : /turtlebot3_home_service_challenge/turtlebot3_home_service_challenge_core/config/scenario.yaml
    • Script
      scenario:
      room1: # SCENARIO_NAME
      target_marker_id: 0 # ArUco Marker's ID
      goal_pose: [0.9, 0.5, 0.0, 0.0, 0.0, 0.7071, 0.7071] # The coordinates and orientation of the room where the goal marker is located.
      goal_marker_id: 4 # ArUco Marker's ID
      end_pose: [0.0, 0.0, 0.0, 0.0, 0.0, 0.0, 1.0] # Coordinates and orientation of the location to return to.

  • turtlebot3_hsc_manipulation.srdf : This configuration file contains manipulator's position data. By changing the joint values or adding new group_state, you can specify the tmanipulator's pose.
    • File Path : /turtlebot3_home_service_challenge/turtlebot3_home_service_challenge_tools/config/turtlebot3_hsc_manipulation.srdf
    • Script
      <group_state name="target" group="arm">
      <joint name="joint1" value="0"/>
      <joint name="joint2" value="0.9076"/>
      <joint name="joint3" value="-0.9425"/>
      <joint name="joint4" value="0.0873"/>
      </group_state>

Details about the Home Service Mission

The goal of the Home Service Challenge is to move four different objects from a living room to a specific place with given rules, and to return to the starting point. (Used topic for run demo : /scenario_selection)

Using the demo package, the process of moving objects in Home Service Challenge is as follows.

  1. Approaching the target.
  • For the approach to the target with precise, TurtleBot3 wheels are directly controlled by computing target's location from AR marker. (Used Topic : /target_maker_id, /cmd_vel) Try twice for reliable performance.

    demo1

  1. Picking the target with OpenMANIPULATOR-X's gripper.
  • Use the MoveIt package to perform joint space control, workspace control, and gripper control to pick the target object. (Used Topic : /manipulator_control)

    manipulation_diagram

    MoveIt Diagram

  1. Navigating to the next room where the object will be placed. -Reach the next room saved in a yaml file using the Nav2 package.

    demo2

  2. Approaching the target.

  3. Placing the object using the gripper.

  4. Returning to the starting point using the Nav2 package.

    demo3