Status Constants
-
File:
robotis_controller_msgs/msg/StatusMsg.msg -
Message Definition
# Status Constants
uint8 STATUS_UNKNOWN = 0
uint8 STATUS_INFO = 1
uint8 STATUS_WARN = 2
uint8 STATUS_ERROR = 3
std_msgs/Header header
uint8 type
string module_name
string status_msg
-
Description
This message is used to identify the status of each module.-
header(std_msgs/msg/Header)
This field specifies recorded time of the status message. -
type
This field specifies the type of status message.
- STATUS_UNKNOWN : Unknown type of status message.
- STATUS_INFO : Status message includes information.
- STATUS_WARN : Status message includes warnings.
- STATUS_ERROR : Status message includes errors. -
module_name
This field specifies the module name that transmits the status message. -
status_msg
This field contains contents of the status message.
-