Skip to main content

Advanced Tutorials

Real-Time Ball Detection with YOLOv8 and OpenVINO on ROBOTIS-OP3

This tutorial provides a comprehensive guide to implementing real-time ball detection on the ROBOTIS-OP3 humanoid robot using the YOLOv8 object detection model and Intel OpenVINO toolkit. The goal is to transition from traditional computer vision methods to a deep learning-based approach, significantly improving detection accuracy and robustness in dynamic sports environments.

Limitations and Problems of Existing Methods

The current ball detection method of ROBOTIS-OP3 relies on multi-stage manual feature extraction and rule-based processing. This approach sequentially applies HSV color space filtering, morphological operations, and Hough circle transform to detect balls. However, this approach reveals several serious limitations.

  • Vulnerability of color-based filtering: Dramatic degradation in detection performance when the ball's color changes due to lighting variations, shadows, reflections, etc.
  • Lack of response to shape changes: Hough circle transform assumes perfect circular objects, so it fails to detect when balls appear elliptical due to motion blur from high-speed movement or when balls are partially occluded.
  • Complexity of parameter adjustment: 23 different parameters must be manually adjusted according to the environment, which greatly limits the system's versatility.

Deep Learning-Based Object Detection Solution

Deep learning-based object detection models provide an innovative approach that can fundamentally solve the limitations of traditional methods.

  • Automatic feature learning: Deep learning models automatically learn complex features and patterns from large amounts of data instead of manually designed features. This enables robust detection performance even under various lighting conditions, viewpoint changes, and partial occlusion situations.
  • Real-time processing performance: YOLO (You Only Look Once) series models perform object detection with a single network pass, enabling real-time processing and efficient operation even on high-resolution videos.
  • Utilization of transfer learning: By applying transfer learning based on pre-trained models, high performance can be achieved with relatively small amounts of specialized data.

Necessity and Expected Effects of System Transition

The transition from existing rule-based systems to deep learning-based object detection represents not just a technical upgrade but a fundamental paradigm shift.

  • Performance improvement: Latest deep learning models achieve high detection accuracy and show stable performance even in complex situations that are difficult to solve with traditional methods.
  • Improved maintainability: System performance can be improved through data-centric approaches instead of complex parameter adjustments, and adaptation to new environments can be automated through retraining.
  • Securing scalability: Once built, deep learning models can be easily applied to various environments and are easy to integrate with additional object detection tasks.

Under this background, this tutorial will provide step-by-step guidance on the specific methods and actual implementation process for transitioning from existing traditional computer vision-based ball detection systems to state-of-the-art deep learning-based object detection models.

Lightweight Object Detection Model Selection and Performance Analysis

One of the most important decisions in building a deep learning-based ball detection system is selecting an appropriate object detection model. In real-time sports environments, the balance between accuracy and speed is crucial, and hardware constraints must also be considered.

YOLO Series Model Performance Comparison

Let's compare major candidates from the YOLO series, which is currently the most widely used real-time object detection model.

ModelParametersmAP@0.5-0.95CPU Inference TimeGPU Inference Time
YOLOv5n2.6M28.0%73.6ms1.12ms
YOLOv8n3.2M37.3%80.4ms1.47ms
YOLOv8s11.2M44.9%128.4ms2.66ms
YOLOv8m25.9M50.2%234.7ms5.86ms
YOLOv8l43.7M52.9%375.2ms9.06ms

YOLOv8 Advantage: The YOLOv8 series achieves 9-10% higher mAP compared to YOLOv5 models of the same size, with YOLOv8n showing 33% improved accuracy over YOLOv5n. This is the result of latest architectural improvements, enabling more stable detection performance in complex sports environments.

Comparison with Lightweight Models

Comparison with lightweight models for mobile and edge devices is also important:

ModelSizeInference TimeAverage Precision
EfficientDet-Lite04.4MB37ms25.69%
EfficientDet-Lite419.9MB260ms41.96%
SSD MobileNetV26.7MB24ms20.2%
YOLOv8n-80.4ms37.3%

EfficientDet and SSD MobileNet series have smaller model sizes and faster inference speeds, but show significant differences in accuracy compared to YOLOv8. Especially considering the complex backgrounds and fast movements in sports environments, these accuracy differences greatly affect practicality.

Performance Improvement through OpenVINO Optimization

Using Intel OpenVINO toolkit can improve YOLOv8 model CPU inference speed by up to 3 times. This is key technology that enables real-time processing even in environments without GPUs.

  • Optimization effect: For YOLOv8m model, OpenVINO optimization can reduce inference time from 234.7ms to about 78ms, achieving 12-13FPS performance even on a single CPU.

OpenVINO automatically utilizes various hardware including Intel CPUs, integrated GPUs, and VPUs to provide additional performance improvements. This allows maximum utilization of available hardware resources without code changes.

Final Model Selection

Based on comprehensive analysis, using YOLOv8m model with OpenVINO optimization is the optimal choice.

  • Accuracy advantage: Provides the highest detection accuracy among real-time models with 50.2% mAP, ensuring stable performance in complex sports environments.
  • Real-time performance: Achieves real-time processing goals even on CPU through OpenVINO optimization, enabling efficient operation without separate GPUs.
  • Robustness: Maintains consistent detection performance under various lighting conditions and complex backgrounds, fundamentally solving traditional method limitations.
  • Scalability: Easy customization for specific sports or environments through transfer learning based on pre-trained models.

Through this selection, we can overcome the limitations of existing HSV + Hough transform methods and build a ball detection system that simultaneously satisfies the high accuracy and real-time performance required in actual sports environments.

Environment Setup

  • Python Environment: Create a Python virtual environment to prevent package conflicts.
sudo apt install python3.12-venv
python3 -m venv ~/yolo_env
source ~/yolo_env/bin/activate
pip install --upgrade pip
  • Ultralytics YOLOv8 Installation:
pip install ultralytics
pip install typeguard

After installation, loading the model with YOLO('yolov8m.pt') will automatically download pre-trained weights.

  • OpenVINO Installation: Use Intel's PyPI distribution for OpenVINO acceleration. After installing OpenVINO runtime, check available devices.
pip install openvino
python3 -c "from openvino import Core; print(Core().available_devices)"
  • ICD (Installable Client Driver) Installation: Driver system that enables OpenCL parallel computing on Intel integrated graphics cards
sudo apt install intel-opencl-icd
  • NumPy Version Downgrade:
    • Binary compatibility issues occur due to version mismatch between NumPy version installed in virtual environment (NumPy 2.2.6) and NumPy version used when building cv_bridge, one of ROS2 Jazzy's core libraries (typically NumPy 1.x version).
    • Need to downgrade NumPy version in yolo_env virtual environment to version below 2.0 compatible with cv_bridge
  1. Activate yolo_env virtual environment (skip if already activated):
source ~/yolo_env/bin/activate
  1. Downgrade NumPy version:
pip install "numpy<2.0"

ROS2 Package Creation and Node Implementation (YOLOv8m + OpenVINO-based Ball detection)

This section explains the complete process of creating a ROS2 package from scratch for use in ROBOTIS-OP3, completing and running a YOLOv8m + OpenVINO-based ball detection node.

1. ROS2 Package Creation (Python-based)

cd ~/robotis_ws/src
ros2 pkg create op3_advanced_detector \
--build-type ament_python \
--dependencies rclpy std_msgs sensor_msgs geometry_msgs cv_bridge op3_ball_detector_msgs

2. Package Directory Structure

The created op3_advanced_detector directory has the following structure:

op3_advanced_detector/
├── op3_advanced_detector/
│ └── __init__.py
├── package.xml
└── setup.py

3. Node Basic File Creation

The final created op3_advanced_detector directory has the following structure:

op3_advanced_detector/
├── config/
│ ├── camera_param.yaml
│ └── detector_config.yaml
├── launch/
│ ├── advanced_detector.launch.py
│ └── ball_detector_from_usb_cam.launch.py
├── op3_advanced_detector/
│ ├── __init__.py
│ └── op3_advanced_detector.py
├── resource/
│ └── op3_advanced_detector
├── package.xml
├── setup.cfg
└── setup.py

Code Structure and Description

Main Class: OP3AdvancedDetector class

class OP3AdvancedDetector(Node):
"""Advanced object detector for ROBOTIS OP3"""

Key Features:

  • Inherits ROS2 Node for integration with ROS system
  • Real-time ball detection based on YOLO v8 + OpenVINO
  • Built-in performance optimization and monitoring functions

Class Constants:

SUPPORTED_MODELS = {'yolov8n', 'yolov8s', 'yolov8m', 'yolov8l', 'yolov8x'}
DEFAULT_INPUT_SIZE = (320, 320)

# === Class constants ===
BALL_CLASS_ID = 32 # COCO sports ball class
DEFAULT_CONF_THRESHOLD = 0.25
DEFAULT_IOU_THRESHOLD = 0.5
MAX_DETECTIONS = 3 # Maximum number of balls to detect for better performance

Initialization Functions

__init__(self): Main Constructor

def __init__(self):
super().__init__('op3_advanced_detector')

# === Initialization sequence ===
self._init_parameters()
self._setup_environment()
self._init_ros_interfaces()
self._init_detection_model()
self._init_performance_tracking()

self.get_logger().info(f"✅ Ball Detector ready | {self.device_info}")

Role:

  • ROS2 node initialization
  • Execute 5-stage initialization process
  • Output system ready message

Why initialization order is important:

  • Parameters first: Basis for all other settings
  • Environment setup: System variables for performance optimization
  • ROS interfaces: Build communication channels
  • AI model: Most time-consuming task
  • Performance tracking: Prepare for post-execution monitoring

_init_parameters(self): ROS2 Parameter Initialization

def _init_parameters(self) -> None:
"""Initialize ROS2 parameters and configuration"""
# Declare ROS2 parameters
params = [
('yolo_model', 'yolov8s'),
('openvino_precision', 'FP32'),
('camera_topic', '/usb_cam_node/image_raw'),
('confidence_threshold', 0.25),
('iou_threshold', 0.5),
('input_size', [320, 320]),
('frame_skip', 2),
('debug_mode', True),
('enable_performance_log', True)
]

for name, default in params:
self.declare_parameter(name, default)

Key Functions:

  • Parameter declaration: Register with ROS2 parameter system
  • Value validation: Input value validity check
  • Default value setting: Provide safe default settings

Key Parameter Description:

ParameterDefaultDescriptionImpact
yolo_model'yolov8s'YOLO model to useAccuracy vs speed
confidence_threshold0.25Detection confidence thresholdSensitivity control
input_sizeInput image sizePerformance vs accuracy
frame_skip2Processing frame intervalCPU usage

_setup_environment(self): System Environment Optimization

def _setup_environment(self) -> None:
"""System environment optimization"""
# Multithreading optimization
env_vars = {
'OMP_NUM_THREADS': '2',
'MKL_NUM_THREADS': '2',
'NUMEXPR_NUM_THREADS': '2',
'OV_CACHE_DIR': '/tmp/ov_cache'
}

for key, value in env_vars.items():
os.environ[key] = value

Optimization Purpose:

  • Memory usage limitation: Prevent memory explosion due to multithreading
  • Performance stabilization: Minimize thread contention
  • Cache management: Specify OpenVINO model cache location

_init_ros_interfaces(self): ROS2 Communication Interface Setup

def _init_ros_interfaces(self) -> None:
"""Initialize ROS2 communication interfaces"""
self.bridge = CvBridge()

# Detect image topic type and create appropriate subscriber
self._setup_image_subscriber()

# Publishers - compatible with original op3_ball_detector
self.circle_pub = self.create_publisher(CircleSetStamped, '/ball_detector_node/circle_set', 10)
self.status_pub = self.create_publisher(String, '/ball_detector_node/status', 10)

# Debug publishers
self.debug_pub = (
self.create_publisher(Image, '/ball_detector_node/image_out', 10)
if self.debug_mode else None
)

# Additional publishers for backward compatibility
self.ball_pub = self.create_publisher(Point, '/ball_position', 10)

Topic Structure:

  • Input: /usb_cam_node/image_raw (camera image)
  • Output:
    • /ball_detector_node/circle_set (detected ball information)
    • /ball_position (first ball position)
    • /ball_detector_node/status (system status)
    • /ball_detector_node/image_out (debug image)

_init_detection_model(self): AI Model Initialization

def _init_detection_model(self) -> None:
"""Initialize ball detection model"""
self.device_info = "Unknown"
self.is_openvino = False

# Try OpenVINO
if OPENVINO_AVAILABLE and self._try_openvino_setup():
return

# PyTorch fallback
self._setup_pytorch_model()

Model Selection Priority:

  1. OpenVINO (Intel optimization): Best performance
  2. PyTorch CPU: Compatibility backup

Image Processing Functions

image_callback(self, msg): Main Image Processing Loop

def image_callback(self, msg: Image) -> None:
"""Main image processing loop"""
self.frame_count += 1

# Frame skipping (performance optimization)
if self.frame_count % self.frame_skip != 0:
return

start_time = time.time()

try:
# Image preprocessing
cv_image = self.bridge.imgmsg_to_cv2(msg, "bgr8")
processed_img, transform_info = self._preprocess_image(cv_image)

# Store original frame for debug visualization
self._current_frame = processed_img.copy()

# Ball detection
detections = self._detect_balls(processed_img)

# Publish results
self._publish_results(detections, transform_info, cv_image.shape)

# Performance tracking
self._update_performance(time.time() - start_time, len(detections))

except Exception as e:
self.get_logger().error(f"❌ Image processing failed: {e}")

Processing Pipeline:

ROS Image → OpenCV Conversion → Preprocessing → AI Inference → Post-processing → ROS Publishing

Frame Skipping Effects:

  • frame_skip=2: 30fps → 15fps (50% CPU usage reduction)
  • frame_skip=3: 30fps → 10fps (67% CPU usage reduction)

_preprocess_image(self, image): Image Preprocessing

def _preprocess_image(self, image: np.ndarray) -> Tuple[np.ndarray, Dict]:
"""Image preprocessing and return transformation info"""
h, w = image.shape[:2]
target_w, target_h = self.input_size

# Resize maintaining aspect ratio
scale = min(target_w / w, target_h / h)
new_w, new_h = int(w * scale), int(h * scale)

resized = cv2.resize(image, (new_w, new_h))

# Center padding
pad_w = (target_w - new_w) // 2
pad_h = (target_h - new_h) // 2

padded = cv2.copyMakeBorder(
resized, pad_h, target_h - new_h - pad_h,
pad_w, target_w - new_w - pad_w,
cv2.BORDER_CONSTANT, value=(114, 114, 114)
)

transform_info = {
'scale': scale,
'pad_w': pad_w,
'pad_h': pad_h,
'original_size': (w, h)
}

return padded, transform_info

Why Preprocessing is Needed:

  • YOLO requirements: Square input needed
  • Aspect ratio preservation: Prevent image distortion
  • Standardization: Support various resolutions

Transformation Process Visualization:

Original (1280x720) → Resize (320x180) → Padding (320x320)
[ Image ] [ Image ] [ Padding ]
[ Image ]
[ Padding ]

compressed_image_callback(self, msg): Compressed Image Processing

def compressed_image_callback(self, msg: CompressedImage) -> None:
"""Compressed image processing callback"""
# ... Frame skipping ...

try:
# Decompress image
np_arr = np.frombuffer(msg.data, np.uint8)
cv_image = cv2.imdecode(np_arr, cv2.IMREAD_COLOR)

if cv_image is None:
self.get_logger().error("❌ Failed to decode compressed image")
return

# Process image using existing pipeline
processed_img, transform_info = self._preprocess_image(cv_image)
# ...

Reasons for Compressed Image Support:

  • Bandwidth saving: Network transmission optimization
  • Compatibility: Support various camera types

AI Model Inference Functions

_detect_balls(self, image): Execute Ball Detection

def _detect_balls(self, image: np.ndarray) -> List[Dict]:
"""Execute ball detection"""
try:
if self.is_openvino:
return self._openvino_inference(image)
else:
return self._pytorch_inference(image)
except Exception as e:
self.get_logger().error(f"❌ Detection failed: {e}")
return []

Dual Backup System:

  • Primary: OpenVINO (Intel optimization)
  • Secondary: PyTorch (general compatibility)

_openvino_inference(self, image): OpenVINO Inference

def _openvino_inference(self, image: np.ndarray) -> List[Dict]:
"""OpenVINO inference"""
# Input format conversion: HWC → CHW, BGR → RGB, normalize
input_tensor = cv2.cvtColor(image, cv2.COLOR_BGR2RGB)
input_tensor = input_tensor.transpose(2, 0, 1).astype(np.float32) / 255.0
input_tensor = np.expand_dims(input_tensor, 0)

# Execute inference
infer_request = self.compiled_model.create_infer_request()
infer_request.infer([input_tensor])
output = infer_request.get_output_tensor(0).data

# Post-processing
return self._postprocess_detections(output, image.shape)

OpenVINO Optimization Effects:

  • Speed: 2-3x faster than PyTorch
  • Memory: Efficient memory usage
  • Hardware: Intel GPU/CPU dedicated optimization

Input Transformation Process:

# Original: (320, 320, 3) BGR uint8
# ↓ Color conversion
# (320, 320, 3) RGB uint8
# ↓ Axis transformation and normalization
# (3, 320, 320) RGB float32 [0-1]
# ↓ Add batch dimension
# (1, 3, 320, 320) RGB float32 [0-1]

_pytorch_inference(self, image): PyTorch Inference (Backup)

def _pytorch_inference(self, image: np.ndarray) -> List[Dict]:
"""PyTorch YOLO inference (fallback)"""
results = self.yolo_model.predict(
image,
classes=[self.BALL_CLASS_ID],
conf=self.DEFAULT_CONF_THRESHOLD,
iou=self.DEFAULT_IOU_THRESHOLD,
verbose=False,
save=False,
device='cpu'
)

detections = []
for result in results:
if result.boxes is not None:
for box in result.boxes:
x1, y1, x2, y2 = box.xyxy[0].cpu().numpy()
conf = float(box.conf[^0].cpu().numpy())

detections.append({
'bbox': (int(x1), int(y1), int(x2), int(y2)),
'confidence': conf,
'center': (int((x1 + x2) / 2), int((y1 + y2) / 2))
})

# Sort by confidence
return sorted(detections, key=lambda x: x['confidence'], reverse=True)

PyTorch Mode Features:

  • Simplicity: Use high-level API
  • Stability: More error handling
  • Compatibility: Support various hardware

_postprocess_detections(self, output, img_shape): Detection Result Post-processing

def _postprocess_detections(self, output: np.ndarray, img_shape: Tuple) -> List[Dict]:
"""OpenVINO output post-processing"""
detections = []

# YOLOv8 output format: (1, 84, 8400)
predictions = output[^0].T # (8400, 84)

# Confidence filtering
ball_scores = predictions[:, 4 + self.BALL_CLASS_ID]
valid_mask = ball_scores > self.DEFAULT_CONF_THRESHOLD

if not np.any(valid_mask):
return detections

valid_preds = predictions[valid_mask]
valid_scores = ball_scores[valid_mask]

# Bounding box conversion (center coordinates → corner coordinates)
boxes = valid_preds[:, :4]
x_centers, y_centers = boxes[:, 0], boxes[:, 1]
widths, heights = boxes[:, 2], boxes[:, 3]

x1s = x_centers - widths / 2
y1s = y_centers - heights / 2
x2s = x_centers + widths / 2
y2s = y_centers + heights / 2

# Apply NMS
indices = cv2.dnn.NMSBoxes(
boxes.tolist(), valid_scores.tolist(),
self.DEFAULT_CONF_THRESHOLD, self.DEFAULT_IOU_THRESHOLD
)

if len(indices) > 0:
for i in indices.flatten():
x1, y1, x2, y2 = x1s[i], y1s[i], x2s[i], y2s[i]
conf = valid_scores[i]

# Minimum size filter
if (x2 - x1) > 8 and (y2 - y1) > 8:
detections.append({
'bbox': (int(x1), int(y1), int(x2), int(y2)),
'confidence': float(conf),
'center': (int((x1 + x2) / 2), int((y1 + y2) / 2))
})

# Limit to MAX_DETECTIONS
return sorted(detections, key=lambda x: x['confidence'], reverse=True)[:self.MAX_DETECTIONS]

YOLOv8 Output Structure:

Output tensor: (1, 84, 8400)
├── 1: Batch size
├── 84: [x, y, w, h] + 80 class scores
└── 8400: Number of prediction boxes (various grid sizes)

Class score positions:
- 0-3: Bounding box coordinates (x, y, w, h)
- 4-83: 80 COCO class scores
- Index 36 (4+32): Sports ball class

NMS (Non-Maximum Suppression):

  • Purpose: Remove duplicate detections
  • Method: Remove boxes with lower confidence among those with IoU > threshold
  • Effect: Leave only one box per ball

Result Publishing Functions

_publish_results(self, detections, transform_info, original_shape): Integrated Result Publishing

def _publish_results(self, detections: List[Dict], transform_info: Dict, original_shape: Tuple) -> None:
"""Publish detection results"""
try:
# Publish CircleSetStamped message (main output)
self._publish_circle_set(detections, transform_info, original_shape)

if detections:
# Publish first ball position for backward compatibility
self._publish_ball_position(detections[^0], transform_info, original_shape)
self._publish_status(f"DETECTED:conf={detections[^0]['confidence']:.3f}")
self.ball_lost_count = 0
else:
self._handle_no_detection()

# Debug image (optional)
if self.debug_pub and self.debug_pub.get_subscription_count() > 0:
self._publish_debug_image(detections, transform_info)

except Exception as e:
self.get_logger().error(f"❌ Result publishing failed: {e}")

Publishing Priority:

  1. Essential: CircleSetStamped (main output)
  2. Compatibility: Point message (for existing systems)
  3. Status: System status string
  4. Optional: Debug image (only when subscribers exist)

_publish_circle_set(self, detections, transform_info, original_shape): Circle Information Publishing

def _publish_circle_set(self, detections: List[Dict], transform_info: Dict, original_shape: Tuple) -> None:
"""Publish CircleSetStamped message compatible with original op3_ball_detector"""
circle_msg = CircleSetStamped()
circle_msg.header.stamp = self.get_clock().now().to_msg()
circle_msg.header.frame_id = "camera_frame"

circles = []
for detection in detections:
center_x, center_y = detection['center']
bbox = detection['bbox']

# Coordinate inverse transformation: remove padding → restore scale
orig_x = int((center_x - transform_info['pad_w']) / transform_info['scale'])
orig_y = int((center_y - transform_info['pad_h']) / transform_info['scale'])

# Calculate radius from bounding box
bbox_width = bbox[^2] - bbox[^0]
bbox_height = bbox[^3] - bbox[^1]
radius = int(max(bbox_width, bbox_height) / 2 / transform_info['scale'])

# Boundary clipping
orig_w, orig_h = transform_info['original_size']
orig_x = np.clip(orig_x, 0, orig_w - 1)
orig_y = np.clip(orig_y, 0, orig_h - 1)

# NORMALIZE COORDINATES TO (-1, +1) RANGE
# top(-1), bottom(+1) for y-axis
# left(-1), right(+1) for x-axis
normalized_x = orig_x / orig_w * 2 - 1 # Convert to (-1, +1)
normalized_y = orig_y / orig_h * 2 - 1 # Convert to (-1, +1)

# Create Point message (x, y are normalized coordinates, z is radius)
point = Point()
point.x = float(normalized_x) # Normalized x (-1 ~ +1)
point.y = float(normalized_y) # Normalized y (-1 ~ +1)
point.z = float(radius) # radius in pixels
circles.append(point)

circle_msg.circles = circles
self.circle_pub.publish(circle_msg)

Coordinate Transformation Process:

1. AI output coordinates (based on 320x320)

2. Remove padding: x' = x - pad_w, y' = y - pad_h

3. Restore scale: x'' = x' / scale, y'' = y' / scale

4. Original resolution coordinates (based on original size)

5. Normalize: nx = x'' / width * 2 - 1, ny = y'' / height * 2 - 1

6. Normalized coordinates (-1 ~ +1 range)

Advantages of Normalization:

  • Resolution independent: Same coordinate system for any camera
  • Robot control standardization: Direct connection to head movement angles
  • Mathematical convenience: Simplified trigonometric calculations

_publish_ball_position(self, detection, transform_info, original_shape): Ball Position Publishing

def _publish_ball_position(self, detection: Dict, transform_info: Dict, original_shape: Tuple) -> None:
"""Publish ball position information"""
center_x, center_y = detection['center']

# Coordinate inverse transformation: remove padding → restore scale
orig_x = int((center_x - transform_info['pad_w']) / transform_info['scale'])
orig_y = int((center_y - transform_info['pad_h']) / transform_info['scale'])

# Boundary clipping
orig_w, orig_h = transform_info['original_size']
orig_x = np.clip(orig_x, 0, orig_w - 1)
orig_y = np.clip(orig_y, 0, orig_h - 1)

# NORMALIZE COORDINATES TO (-1, +1) RANGE
normalized_x = orig_x / orig_w * 2 - 1 # Convert to (-1, +1)
normalized_y = orig_y / orig_h * 2 - 1 # Convert to (-1, +1)

# Publish
point = Point()
point.x = float(normalized_x) # Normalized x (-1 ~ +1)
point.y = float(normalized_y) # Normalized y (-1 ~ +1)
point.z = detection['confidence']
self.ball_pub.publish(point)

Point Message Structure:

  • x: Normalized x coordinate (-1 ~ +1)
  • y: Normalized y coordinate (-1 ~ +1)
  • z: Detection confidence (0 ~ 1)

_publish_debug_image(self, detections, transform_info): Debug Image Publishing

def _publish_debug_image(self, detections: List[Dict], transform_info: Dict) -> None:
"""Publish debug image with detection visualizations"""
try:
# Use original frame as base for debug image
if hasattr(self, '_current_frame') and self._current_frame is not None:
# Resize debug image to match detection input size for consistency
debug_img = cv2.resize(self._current_frame, self.input_size)
else:
# Fallback: create empty image with detection input size
debug_img = np.zeros((*self.input_size[::-1], 3), dtype=np.uint8)

img_height, img_width = debug_img.shape[:2]

# Calculate appropriate text scale based on image size (smaller for 320x320)
text_scale = 0.4 # Fixed smaller scale for 320x320 resolution
text_thickness = 1

# Draw detection results directly on resized debug image (no coordinate transformation needed)
for i, detection in enumerate(detections):
# Use detection coordinates directly since debug image is same size as detection input
center_x, center_y = detection['center']
bbox = detection['bbox']
x1, y1, x2, y2 = bbox

# Ensure coordinates are within image bounds
x1 = max(0, min(x1, img_width - 1))
y1 = max(0, min(y1, img_height - 1))
x2 = max(0, min(x2, img_width - 1))
y2 = max(0, min(y2, img_height - 1))
center_x = max(0, min(center_x, img_width - 1))
center_y = max(0, min(center_y, img_height - 1))

# Color coding by detection order
color = (0, 255, 0) if i == 0 else (0, 255, 255) # Green for best, yellow for others

# Draw bounding box
cv2.rectangle(debug_img, (x1, y1), (x2, y2), color, 2)

# Draw center point
cv2.circle(debug_img, (center_x, center_y), 4, color, -1)

# Draw confidence text
conf_text = f"Ball {i+1}: {detection['confidence']:.3f}"
text_y = y1 - 10 if y1 > 20 else y2 + 20
cv2.putText(debug_img, conf_text, (x1, text_y),
cv2.FONT_HERSHEY_SIMPLEX, text_scale, color, text_thickness)

# Add performance info
fps_text = f"FPS: {self.current_fps:.1f} | Device: {self.device_info}"
cv2.putText(debug_img, fps_text, (5, 20),
cv2.FONT_HERSHEY_SIMPLEX, text_scale, (255, 255, 255), text_thickness)

# Convert and publish
debug_msg = self.bridge.cv2_to_imgmsg(debug_img, "bgr8")
debug_msg.header.stamp = self.get_clock().now().to_msg()
debug_msg.header.frame_id = "camera_frame"
self.debug_pub.publish(debug_msg)

except Exception as e:
self.get_logger().error(f"❌ Debug image publishing failed: {e}")

Debug Image Elements:

  • Bounding boxes: Detected ball areas (rectangles)
  • Center points: Ball center positions (circles)
  • Confidence: Detection confidence (text)
  • Performance info: FPS and device used (text)
  • Color coding: First ball (green), others (yellow)

Performance Monitoring Functions

_update_performance(self, process_time, ball_count): Performance Update

def _update_performance(self, process_time: float, ball_count: int) -> None:
"""Update performance statistics"""
self.process_times.append(process_time)
self.fps_counter += 1

# Periodic logging (every 15 frames)
if self.fps_counter % 15 == 0:
self._log_performance(ball_count)

Performance Tracking Items:

  • Processing time: Time taken to process each frame
  • FPS: Frames processed per second
  • Detection count: Number of balls detected per frame

_log_performance(self, ball_count): Performance Logging

def _log_performance(self, ball_count: int) -> None:
"""Log performance information"""
elapsed = time.time() - self.fps_timer
self.current_fps = 15 / elapsed

recent_times = self.process_times[-15:]
avg_ms = np.mean(recent_times) * 1000
max_ms = np.max(recent_times) * 1000

self.get_logger().info(
f"📊 {self.device_info} | FPS: {self.current_fps:.1f} | "
f"Process time: {avg_ms:.0f}ms (max: {max_ms:.0f}ms) | Balls: {ball_count}"
)

# Reset timer
self.fps_timer = time.time()

# Memory management
if len(self.process_times) > 30:
self.process_times = self.process_times[-15:]

Log Example:

📊 OpenVINO GPU | FPS: 15.1 | Process time: 62ms (max: 64ms) | Balls: 3
📊 PyTorch CPU | FPS: 12.3 | Process time: 81ms (max: 125ms) | Balls: 0

Performance Indicator Interpretation:

  • FPS > 20: Real-time processing possible
  • Process time < 50ms: Good performance
  • Max time: Worst-case latency

Utility Functions

_try_openvino_setup(self): Attempt OpenVINO Setup

def _try_openvino_setup(self) -> bool:
"""Attempt OpenVINO model setup"""
try:
# Set model file paths
model_dir = Path(f"{self.yolo_model_name}_openvino_model")
xml_path = model_dir / f"{self.yolo_model_name}.xml"

# Create model if needed
if not xml_path.exists():
self.get_logger().info(f"⚙️ Creating OpenVINO model... ({self.yolo_model_name})")
self._create_openvino_model()

# Re-check after creation
if not xml_path.exists():
self.get_logger().warn(f"❌ OpenVINO model creation failed: {xml_path}")
return False

# Initialize OpenVINO core
self.ov_core = ov.Core()

# Select device and compile model
device = self._select_best_device()
self.ov_model = self.ov_core.read_model(str(xml_path))
self.compiled_model = self.ov_core.compile_model(self.ov_model, device)

self.device_info = f"OpenVINO {device}"
self.is_openvino = True

# Warmup
self._warmup_model()

self.get_logger().info(f"🚀 OpenVINO model loaded | Device: {device}")
return True

except Exception as e:
self.get_logger().warn(f"⚠️ OpenVINO setup failed: {e}")
return False

_create_openvino_model(self): Create OpenVINO Model

def _create_openvino_model(self) -> None:
"""Create OpenVINO optimized model"""
try:
# Load PyTorch model
yolo_model = YOLO(f"{self.yolo_model_name}.pt")

# Export to OpenVINO format
export_path = yolo_model.export(
format="openvino",
half=(self.precision == "FP16"),
imgsz=self.input_size[^0],
dynamic=False,
simplify=True
)

self.get_logger().info(f"✅ OpenVINO model created: {export_path}")

except Exception as e:
self.get_logger().error(f"❌ OpenVINO model creation failed: {e}")
raise

Model Conversion Options:

  • FP16: 50% memory usage reduction, slight accuracy loss
  • FP32: High accuracy, more memory usage
  • Dynamic=False: Faster inference with fixed size
  • Simplify=True: Remove unnecessary operations

_select_best_device(self): Select Optimal Device

def _select_best_device(self) -> str:
"""Select optimal inference device"""
try:
available_devices = self.ov_core.available_devices

# Prefer Intel GPU
if 'GPU' in available_devices:
return 'GPU'
elif 'CPU' in available_devices:
return 'CPU'
else:
return 'AUTO'
except:
return 'CPU' # Safe fallback

Device Priority:

  1. GPU: Intel integrated graphics (fastest)
  2. CPU: Intel CPU (medium performance)
  3. AUTO: Automatic selection (safe)

_warmup_model(self): Model Warmup

def _warmup_model(self) -> None:
"""Model warmup (remove initial latency)"""
dummy_input = np.zeros((1, 3, *self.input_size), dtype=np.float32)

try:
for _ in range(2):
infer_request = self.compiled_model.create_infer_request()
infer_request.infer([dummy_input])
self.get_logger().info("🔥 Model warmup complete")
except Exception as e:
self.get_logger().warn(f"Warmup failed: {e}")

Need for Warmup:

  • Initial latency: First inference is slow due to cache loading
  • Memory allocation: Pre-allocate GPU memory
  • Optimization: Complete runtime optimization

Error Handling and State Management

_handle_no_detection(self): Handle Detection Failure

def _handle_no_detection(self) -> None:
"""Handle no ball detection"""
self.ball_lost_count += 1
if self.ball_lost_count > 10: # No detection for 10 consecutive frames
self._publish_status("NO_BALL")

Detection Failure Logic:

  • Counter increment: Track consecutive failures
  • Threshold application: 10 frames = about 0.5 seconds (30fps basis)
  • Status publishing: Notify other nodes of situation

_publish_status(self, status): Status Publishing

def _publish_status(self, status: str) -> None:
"""Publish status message"""
msg = String()
msg.data = status
self.status_pub.publish(msg)

Status Message Types:

  • "DETECTED:conf=0.856": Detection success + confidence
  • "NO_BALL": Detection failure (long-term)
  • "ERROR:...": System error

Main Execution Function

main(args=None): Program Entry Point

def main(args=None):
"""Main execution function"""
rclpy.init(args=args)

try:
detector = OP3AdvancedDetector()
detector.get_logger().info("🎯 Ball Detector running... (Ctrl+C to stop)")
rclpy.spin(detector)

except KeyboardInterrupt:
print("\n👋 User terminated")
except Exception as e:
print(f"❌ System error: {e}")
finally:
try:
rclpy.shutdown()
except:
pass

Execution Flow:

  1. ROS initialization: rclpy.init()
  2. Node creation: OP3AdvancedDetector()
  3. Main loop: rclpy.spin() - callback processing
  4. Cleanup: rclpy.shutdown()

Conclusion

In this tutorial, we solved the vulnerabilities of the HSV + Hough method with AI object detection. The YOLOv8m + OpenVINO combination enabled robust ball detection even with environmental changes and achieved real-time performance of ≥15FPS even in CPU-only environments. The code structure is easily extensible to various objects (e.g., goals, opposing players). For example, by retraining the YOLOv8 model with goal data or training additional classes, the same node can be extended to detect multiple objects.

Voice Control System Implementation

Introduction

Limitations of the Existing ROBOTIS-OP3

The ROBOTIS-OP3 is a humanoid robot with powerful hardware capabilities, but its basic software does not include the functionality to interact with the robot through voice. This meant that users could only control the robot through buttons or a remote GUI.

This tutorial provides a comprehensive guide to building a system that adds real-time Speech-to-Text and Text-to-Speech (TTS) capabilities to the ROBOTIS-OP3, allowing users to communicate with and control the robot using voice commands.

Tutorial Goals

  • Implement a stable voice recognition system that works even in environments with robot motor noise.
  • Build a hybrid TTS system that can handle both online and offline environments.
  • Implement multi-stage filtering to prevent the echo phenomenon where TTS output is fed back into the microphone.
  • Integrate the implemented voice control system with the existing OP3 demo framework.

Voice Recognition Model and TTS Selection Rationale

Voice Recognition: Vosk Engine

In this system, Vosk was chosen as the primary voice recognition engine.

FeatureVoskGoogle Speech APIMozilla DeepSpeech
Offline Operation✓ (Fully offline)✗ (Online required)✓ (Offline)
Model Size50MB (lightweight model)N/A (Cloud)~200MB
Language Support20+ languages100+ languagesEnglish-centric
AccuracyMedium-HighVery HighMedium-High
Resource UsageLowNetwork dependentMedium
Real-time Processing✓ (Streaming API)✓ (Streaming)
Customization✓ (Vocabulary reconfiguration)Limited✓ (Model training)
Ease of Installation✓ (pip install)✓ (API key required)Complex
Suitability for Robot Environment★★★★★★★☆☆☆★★★☆☆

Reasons for choosing Vosk:

  • Complete Offline Operation: All voice recognition is processed inside the NUC without an internet connection. This ensures the robot's autonomy and fundamentally blocks issues like network latency or instability.
  • Lightweight and High Performance: It uses a lightweight model of about 50MB, making it suitable for embedded systems, while enabling real-time continuous voice processing through its streaming API.
  • Easy Integration: It can be easily installed with Python's pip and is easy to integrate into a ROS2 node.

Speech Synthesis: Multi-layered TTS System Configuration

This system adopts a hybrid approach that utilizes different TTS engines depending on the situation.

FeaturegTTSFestivalespeak
Offline Operation✗ (Online required)✓ (Fully offline)✓ (Fully offline)
Voice QualityVery High (Natural speech)Medium (Robotic)Low (Robotic)
Language Support100+ languagesEnglish-centric100+ languages
Ease of Installation✓ (pip install)Complex (Compilation required)✓ (Package manager)
Resource UsageNetwork dependentMediumVery Low
Suitability for Robot Environment★★★☆☆★★★★☆★★★★★
Response SpeedNetwork dependentFastVery Fast
CustomizationLimited✓ (High)Medium

Role of each TTS engine:

  1. gTTS (Primary Engine): An online engine that uses Google's TTS API, providing the most natural and high-quality voice. It is used preferentially in an online environment.
  2. Festival (1st Offline Fallback): An offline engine that automatically switches over if gTTS fails (e.g., network disconnection). It is highly stable and uses few system resources.
  3. espeak (2nd Offline Fallback): The final backup engine in case Festival also fails. It is very light and fast, but the voice quality is relatively robotic.

Environment Preparation and Installation

Dependency Package Installation

Open a terminal and run the following commands in order to install the necessary system libraries and Python packages.

# Update system packages
sudo apt update && sudo apt upgrade -y

# Install audio and TTS related system libraries
sudo apt install -y python3-pip portaudio19-dev python3-pyaudio
sudo apt install -y festival festival-dev espeak espeak-data

# Create and activate a Python virtual environment (recommended)
sudo apt install -y python3.12-venv
python3 -m venv ~/yolo_env
source ~/yolo_env/bin/activate

# Install Python dependencies
pip install vosk sounddevice numpy scipy librosa noisereduce
pip install gtts pygame rclpy std-msgs geometry-msgs
pip install PyYAML jinja2 setuptools typeguard

Download Vosk Model

# Create model directory
mkdir -p ~/op3_voice_tutorial/models
cd ~/op3_voice_tutorial/models

# Download and unzip the lightweight English model (approx. 45MB)
wget https://alphacephei.com/vosk/models/vosk-model-small-en-us-0.15.zip
unzip vosk-model-small-en-us-0.15.zip
mv vosk-model-small-en-us-0.15 vosk-model-small-en-us

Package Creation and Code Addition

Create ROS2 Package

# Move to workspace
cd ~/robotis_ws/src/ROBOTIS-OP3-Tutorials

# Create package
ros2 pkg create --build-type ament_python op3_voice_control \
--dependencies rclpy std_msgs geometry_msgs

Set Up Package Structure

op3_voice_control/
├── launch/
│ └── voice_control.launch.py # ROS2 launch file
├── op3_voice_control/
│ ├── __init__.py # Python package initialization
│ ├── speech_recognition_node.py # Speech recognition node
│ └── command_processor.py # Command processor node
├── scripts/
│ └── start_voice_control.sh # System start script
├── package.xml # Package metadata
└── setup.py # Python installation setup

Note: You can download the complete package source from the GitHub repository:
https://github.com/ROBOTIS-GIT/ROBOTIS-OP3-Tutorials/op3_voice_control

Modify Existing OP3 Demo Code

Some modifications to the existing demo code are required for the voice control system to interact with the OP3's basic motion modules.

op3_demo/src/demo_node.cpp modifications:

// Add demo mode command callback for voice control
void demoModeCommandCallback(const std_msgs::msg::String::SharedPtr msg)
{
// ... existing code ...

else if(msg->data == "action")
{
desired_status = ActionDemo;
apply_desired = true;
// Enable voice control mode
action_demo->setVoiceControlMode(true);
RCLCPP_INFO(node->get_logger(), "Voice control mode enabled for action demo");

dxlTorqueChecker();
playSound(default_mp3_path + "Start motion demonstration.mp3");
if (DEBUG_PRINT)
RCLCPP_INFO(node->get_logger(), "= Start Demo Mode : %d", desired_status);
}
}

op3_demo/include/op3_demo/action_demo.h modifications:

class ActionDemo : public OPDemo
{
public:
// ... existing methods ...
void setVoiceControlMode(bool voice_mode);

// Public methods for voice control
void playAction(int motion_index);
void stopAction();
void brakeAction();
bool isActionRunning();

protected:
// ... existing members ...
bool voice_control_mode_; // Voice control mode flag
bool stop_action_executed_; // Flag to prevent duplicate stops
};

Key Code Explanation

System Architecture and Data Flow

The voice control system consists of two core nodes that communicate organically through ROS2 topics.

  1. Microphone Input: sounddevice captures the audio stream.
  2. speech_recognition_node:
    • Applies noise filtering to the audio stream.
    • Converts the filtered audio to text via the Vosk engine.
    • Publishes the recognized text to the /voice_command topic.
  3. command_processor:
    • Subscribes to the /voice_command topic.
    • Analyzes the received text to determine if it is an echo and matches it against registered command patterns.
    • Publishes robot control commands to the /robotis/action/page_num or /robotis/mode_command topics based on the matched command.
    • Simultaneously calls the TTS engine to play audio for user feedback.


  • speech_recognition_node.py: Speech Recognition and Noise Filtering
    This node is responsible for receiving microphone input in real-time and converting it to text.

    • 2-Stage Noise Filtering
      To handle both specific frequency noises like motor sounds, a major problem in robot environments, and general background noise, a 2-stage filtering strategy is used.

      1. Notch Filter: Precisely removes noise in specific frequency bands (50Hz, 100Hz, 200Hz, etc.) commonly generated by robot motors using scipy.signal.iirnotch.

      2. Broadband Noise Reduction: Generally reduces the remaining background noise (like fan noise) not caught by the notch filter using the noisereduce library.

        def apply_noise_filtering(self, audio_data):
        """Apply noise filtering"""
        if not self.noise_reduction:
        return audio_data

        # Type conversion
        audio_float = audio_data.astype(np.float32) / 32768.0

        # Apply notch filter (motor noise removal)
        filtered_audio = audio_float
        for b, a in self.notch_filters:
        filtered_audio = signal.filtfilt(b, a, filtered_audio)

        # Apply advanced noise reduction
        try:
        # Use first 0.5 seconds as noise profile
        if len(filtered_audio) > self.sample_rate // 2:
        noise_sample = filtered_audio[:self.sample_rate // 2]
        filtered_audio = nr.reduce_noise(
        y=filtered_audio,
        sr=self.sample_rate,
        y_noise=noise_sample,
        prop_decrease=0.8
        )
        except Exception as e:
        self.get_logger().warn(f"Advanced noise reduction failed: {e}")

        # Convert back to int16
        return (filtered_audio * 32768.0).astype(np.int16)
    • Asynchronous Processing: Audio Callback and Recognition Thread

      • audio_callback: Called automatically by the sounddevice library whenever data comes in from the audio hardware. This function only applies noise filtering and puts the processed data into self.audio_queue to prevent audio drops.
      • recognition_loop: Runs in a separate thread and continuously checks for data accumulating in the audio_queue. The actual recognition work of fetching data from the queue and passing it to the Vosk engine is done in this thread, so it does not interfere with real-time processing like audio capture.
  • command_processor.py: Command Processing and Multi-level Echo Prevention
    This node acts as the brain of the system, interpreting recognized text, controlling the robot, and responding with voice.

    • Multi-level Echo Cancellation Architecture

      To break the feedback loop where TTS speech is fed back into the microphone, a 5-stage echo prevention system is implemented in the voice_command_callback function.

      1. TTS Playback Status Flag (is_speaking): Immediately ignores all incoming voice commands while TTS is active.
      2. TTS Cooldown Timer (tts_cooldown): Ignores commands that come in for 2.0 seconds after TTS playback finishes to prevent echoes from slight audio delays.
      3. Echo Pattern Filtering (is_tts_echo): If a pattern matching the system's frequent response phrases like "entering ready mode" is detected, it is considered an echo and filtered out.
      4. Recent TTS Text Similarity Check (is_similar_to_recent_tts): Calculates the word similarity between recent TTS output history and the received text. If they match by 70% or more, it's judged as an echo.
      5. Physical Microphone Deactivation: Just before TTS playback, it publishes a "disable" message to the /mic_control topic, and an "enable" message after playback ends, fundamentally blocking echo influx at the hardware level. This topic is received by speech_recognition_node to control the audio stream.
    • Flexible Command Matching

      Regular expressions (re) are used to match various forms of commands like "stand up", "get up", and "standup" to the same action (stand_up), enhancing user convenience.

    • Duplicate Command Filtering

      A cooldown of 0.5 seconds for emergency commands like "stop" and 1.0 second for general commands is applied to prevent users from unintentionally executing the same command in quick succession.

    • Non-blocking TTS Playback (speak function)

      The process of generating and playing a TTS file can take time. If this task were handled in the main thread, the entire ROS node would freeze. To prevent this, the speak function creates a separate thread called tts_thread to handle TTS-related tasks asynchronously.

      def speak(self, text):
      """High-quality TTS speech (with echo prevention)"""
      def tts_thread():
      with self.tts_lock: # Prevent simultaneous thread access
      try:
      self.disable_microphone()
      self.is_speaking = True
      # ... gTTS, Festival, etc. TTS playback logic ...
      finally:
      self.is_speaking = False
      self.enable_microphone()

      # Run TTS in a separate thread to avoid blocking the main node
      thread = threading.Thread(target=tts_thread)
      thread.daemon = True
      thread.start()
  • C++ Code Integration: Control Transfer through State Management

    The voice_control_mode_ flag added to action_demo.h is a key state management device that prevents system malfunction by clearly distinguishing the control subject (button or voice) within the same ActionDemo mode.

    • When entering mode via voice: setVoiceControlMode(true) is called from demo_node.cpp. This puts ActionDemo in a state where it waits for an external voice command topic.
    • When entering mode via button: setVoiceControlMode(false) is called from the buttonHandlerCallback in demo_node.cpp. In this state, the existing logic based on button input operates.
  • voice_control.launch.py: Flexible System Execution

    The launch file is designed to go beyond simply running nodes, allowing for flexible system configuration.

    • Launch Arguments: Key settings like model_path or device_id are exposed as launch arguments, allowing settings to be changed from the terminal, such as ros2 launch … model_path:=/path/to/my/model, without modifying the code.
    • Virtual Environment Integration (prefix): The prefix='/home/robotis/yolo_env/bin/python3' setting ensures that these nodes run within the specified Python virtual environment. This is a crucial setting that prevents conflicts with system-wide installed packages and facilitates project-specific dependency management.

Execution and Testing Methods

System Build and Execution

  1. Build ROS2 Package

    cd ~/robotis_ws
    colcon build --packages-select op3_voice_control
  2. Set Environment and Run

    The provided start_voice_control.sh script handles virtual environment activation, ROS2 environment setup, and launch file execution all at once.

    # Grant execution permission
    chmod +x ~/robotis_ws/src/ROBOTIS-OP3-Tutorials/op3_voice_control/scripts/start_voice_control.sh

    # Run the script
    ~/robotis_ws/src/ROBOTIS-OP3-Tutorials/op3_voice_control/scripts/start_voice_control.sh

    Alternatively, you can run the launch file manually:

    # Activate virtual environment
    source ~/yolo_env/bin/activate
    # Set up ROS2 environment
    source ~/robotis_ws/install/setup.bash
    # Run launch file
    ros2 launch op3_voice_control voice_control.launch.py

Testing

Once the system is running, you can test its functionality with the following voice commands.

  • Mode Change: "action mode", "motion mode", "ready mode"
  • Basic Actions: "stand up", "sit down"
  • Stop: "stop", "halt"
  • Emotions: "bye bye", "clap", "wow"
  • Status Check: "status", "how are you"

Expected Results:

  • When you speak a command, the recognized text will be printed in the terminal.
  • The robot will respond with voice, such as "Entering action mode".
  • The robot motion corresponding to the command will be executed.
  • While the robot is speaking, it will not recognize new voice commands.

Troubleshooting Tips

  • If "Failed to initialize audio stream" error occurs:

    Check if the microphone device ID is correct. You can check the list of available devices using sounddevice and modify the device_id argument in the launch file.

    # Check device list
    python3 -c "import sounddevice as sd; print(sd.query_devices())"

    # Run with a specific device ID (e.g., if ID is 2)
    ros2 launch op3_voice_control voice_control.launch.py device_id:=2
  • If voice recognition is poor:

    Check if the microphone is too far away or if there is excessive ambient noise. You can test by setting the noise_reduction parameter to False in the voice_control.launch.py file to turn off the noise filtering feature.