Skip to main content

Getting Started with Cyclo Lab

Overview

Cyclo Lab is a research-oriented repository based on Isaac Lab, designed to enable reinforcement learning and imitation learning experiments using Robotis robots in simulation. This project provides simulation environments, configuration tools, and task definitions tailored for Robotis hardware, leveraging NVIDIA Isaac Sim’s powerful GPU-accelerated physics engine and Isaac Lab’s modular RL pipeline.

info

This repository currently depends on IsaacLab v2.2.0 or higher.

Installation (Docker)

Docker installation provides a consistent environment with all dependencies pre-installed.

Prerequisites:

  • Docker and Docker Compose installed
  • NVIDIA Container Toolkit installed
  • NVIDIA GPU with appropriate drivers

Steps:

  1. Clone the cyclo_lab repository with submodules:

    git clone --recurse-submodules https://github.com/ROBOTIS-GIT/cyclo_lab.git
    cd cyclo_lab

    If you already cloned without submodules, initialize them:

    git submodule update --init --recursive
  2. Build and start the Docker container:

    ./docker/container.sh start
  3. Enter the container:

    ./docker/container.sh enter

Docker Commands:

  • ./docker/container.sh start - Build and start the container
  • ./docker/container.sh enter - Enter the running container
  • ./docker/container.sh stop - Stop the container
  • ./docker/container.sh logs - View container logs
  • ./docker/container.sh clean - Remove container and image

What's included in the Docker image:

  • Isaac Sim 5.1.0
  • Isaac Lab v2.3.0 (from third_party submodule)
  • CycloneDDS 0.10.2 (from third_party submodule)
  • robotis_dds_python (from third_party submodule)
  • LeRobot 0.3.3 (in separate virtual environment at ~/lerobot_env)
  • All required dependencies and configurations

Running Examples

Reinforcement Learning

OMY Reach Task

Sim2Sim

You can train and run the OMY Reach Task using the following commands:

# Train
python scripts/reinforcement_learning/rsl_rl/train.py --task Cyclo-Reach-OMY-v0 --num_envs=512 --headless

# Play
python scripts/reinforcement_learning/rsl_rl/play.py --task Cyclo-Reach-OMY-Play-v0 --num_envs=16

Sim2Real

# Play
python scripts/sim2real/reinforcement_learning/inference/OMY/reach/run_omy_reach.py --model_dir 2025-07-10_08-47-09

--model_dir is the run folder under logs/rsl_rl/reach_omy/. The script loads exported/policy.pt and params/env.yaml from that folder.

Imitation Learning

Cyclo Lab supports imitation learning pipelines for ROBOTIS robots. Using the OMY robot as an example, you can collect demonstration data, process it, convert it into the Lerobot dataset format, and run inference or training using physical_ai_tools.

OMY Pick and Place Task

Sim2Sim

Sim2Real

  1. Teleoperation and Demo Recording
    Record demonstrations using teleoperation while capturing camera observations and robot states.
python scripts/sim2real/imitation_learning/recorder/record_demos.py \
--task=Cyclo-Real-Pick-Place-Bottle-OMY-v0 \
--robot_type OMY \
--dataset_file ./datasets/omy_pick_place_task.hdf5 \
--num_demos 10 \
--enable_cameras
  1. [Optional] Dataset Processing and Generation You can further process recorded demos, annotate them, and generate augmented datasets for better coverage.
# Convert actions from joint space to end-effector pose
python scripts/sim2real/imitation_learning/mimic/action_data_converter.py \
--robot_type OMY \
--input_file ./datasets/omy_pick_place_task.hdf5 \
--output_file ./datasets/processed_omy_pick_place_task.hdf5 \
--action_type ik

# Annotate dataset
python scripts/sim2real/imitation_learning/mimic/annotate_demos.py \
--task Cyclo-Real-Mimic-Pick-Place-Bottle-OMY-v0 \
--auto \
--input_file ./datasets/processed_omy_pick_place_task.hdf5 \
--output_file ./datasets/annotated_dataset.hdf5 \
--enable_cameras --headless

# Generate augmented dataset
python scripts/sim2real/imitation_learning/mimic/generate_dataset.py \
--device cuda \
--num_envs 10 \
--task Cyclo-Real-Mimic-Pick-Place-Bottle-OMY-v0 \
--generation_num_trials 500 \
--input_file ./datasets/annotated_dataset.hdf5 \
--output_file ./datasets/generated_dataset.hdf5 \
--enable_cameras --headless

# Convert actions back to joint space
python scripts/sim2real/imitation_learning/mimic/action_data_converter.py \
--robot_type OMY \
--input_file ./datasets/generated_dataset.hdf5 \
--output_file ./datasets/processed_generated_dataset.hdf5 \
--action_type joint
  1. Convert IsaacLab Dataset to Lerobot Format The processed datasets can be converted to the Lerobot dataset format, which is compatible with physical_ai_tools for training and inference.
lerobot-python scripts/sim2real/imitation_learning/data_converter/isaaclab2lerobot.py \
--task=Cyclo-Real-Pick-Place-Bottle-OMY-v0 \
--robot_type OMY \
--dataset_file ./datasets/<processed_generated_dataset.hdf5> # or processed_omy_pick_place_task.hdf5
  1. Training and Inference with physical_ai_tools
Physical AI Tools Page
  1. Inference in Simulation If you want to verify inference in the simulator, run the inference using physical_ai_tools, and then launch the simulator using the command below.
python scripts/sim2real/imitation_learning/inference/inference_demos.py \
--task Cyclo-Real-Pick-Place-Bottle-OMY-v0 \
--robot_type OMY \
--enable_cameras