Skip to main content

Install Cyclo Manager

info

After Cyclo Manager is installed and set up once, it starts automatically when the robot boots. When you power on the robot later, you only need to open Cyclo Manager from your browser.

Cyclo Manager runs inside Docker containers. The Python package cyclo-manager on PyPI provides the cyclo_manager CLI, which uses Docker images and Compose to bring up and configure the container stack.

How to Install​

info

Cyclo Manager runs on the OMY robot PC. Install it on the robot PC.

  1. Connect to OMY via SSH.

Replace SNPR44B9999 with the serial number printed on the robot.

ssh root@omy-SNPR44B9999.local
  1. Install the Python package cyclo-manager on the OMY robot PC.
pip3 install cyclo-manager
  1. Add the CLI to your PATH and set up the Cyclo Manager environment.
export PATH="$HOME/.local/bin:$PATH"
cyclo_manager up
info

After you run cyclo_manager up once to set up the environment, Cyclo Manager keeps running unless you run cyclo_manager down. You do not need to run cyclo_manager up again after powering the robot off and on.

CLI commands

Use the cyclo_manager CLI from your terminal:

cyclo_manager up # optional: --pull to fetch the latest images from the registry
cyclo_manager down
cyclo_manager update
  • cyclo_manager up:

    • Registers a host-agent systemd service so it always runs.
    • Creates and starts the cyclo_manager API and cyclo_manager_ui containers.
    • Creates the zenoh-daemon and novnc-server containers.
  • cyclo_manager down:

    • Stops and removes the containers created by cyclo_manager up.
    • Removes the host-agent service from systemd.
  • cyclo_manager update:

    • Upgrades the cyclo-manager package with pip.
    • Stops the running containers and starts new ones with the updated stack.
    • Restarts the host-agent service.

Open the Cyclo Manager Web UI​

Open the Cyclo Manager web UI on port 3000 in your browser.

info

Connect using the robot IP address or the mDNS hostname. Replace SNPR44B9999 with your robot's serial number. http://omy-SNPR44B9999.local:3000

Cyclo Manager App Page

From the main page, open the Cyclo Manager dashboard.

Dashboard Page

Update the s6 Agent​

After the first installation, the s6 agent inside a managed container may not match the installed Cyclo Manager version. If the container agent and Cyclo Manager are not compatible, some Cyclo Manager operations may not work as expected.

Check the Container Agents section in Version Management after opening the dashboard. If an agent update is available, update the s6 agent before using Cyclo Manager for regular operation. For details, see Agent Update.