Setup
Cyclo Intelligence runs as a set of Docker containers with a web UI.
Requirements
The machine that runs Cyclo Intelligence handles the web UI, the containers, recording, dataset conversion, and inference. It needs:
| Requirement | How to check |
|---|---|
| Docker 24 or later, with Compose | docker compose version |
git | git --version |
| 35 GB free disk space | df -h ~ |
| Port 7080 free | ss -ltn 'sport = :7080' — no output means free |
| NVIDIA GPU — to run trained models | nvidia-smi |
More about these requirements
The installer only needs git. It does not install Docker or the NVIDIA Container Toolkit for you.
A GPU is optional at this stage. Recording data and using Data Tools work without one. A GPU is required only when you run a trained model. To confirm Docker can reach your GPU:
docker info | grep -i runtimes
The nvidia runtime should appear in the output.
To use a port other than 7080, set CYCLO_UI_PORT before starting the container.
Cyclo Intelligence uses public Docker images, so you do not need a Docker Hub login.
1. Install
curl -fsSL https://raw.githubusercontent.com/ROBOTIS-GIT/cyclo_intelligence/main/install.sh | bash
This clones the cyclo_intelligence repository and its submodules into ~/cyclo_intelligence. No container starts yet.
If you already have a checkout, update it instead of reinstalling:
cd ~/cyclo_intelligence
git pull
git submodule update --init --recursive
2. Start The Main Container
The main container provides the web UI, data recording, and Data Tools.
cd ~/cyclo_intelligence
./docker/container.sh start
./docker/container.sh enter
3. Connect To The Robot Network (Zenoh)
Cyclo Intelligence reaches the robot over Zenoh-based ROS 2 communication. Two things must be true:
- A Zenoh daemon is running on the robot network.
- Cyclo Intelligence knows where it is, through
ZENOH_CONFIG_OVERRIDE.
Start the Zenoh daemon before launching Cyclo Intelligence. Follow the OMY Zenoh Communication guide.
Run the commands below inside the Cyclo Intelligence container. First check whether the variable is already set, so you do not end up with two conflicting lines:
grep ZENOH_CONFIG_OVERRIDE ~/.bashrc
If that prints a line, edit it with nano ~/.bashrc instead of appending. If it prints nothing, pick your case:
- Daemon on the same machine
- Daemon on another machine
echo "export ZENOH_CONFIG_OVERRIDE='transport/shared_memory/enabled=true'" >> ~/.bashrc
source ~/.bashrc
Cyclo Intelligence connects as a client. Replace 192.168.0.42 with the IP address of the machine running the daemon.
echo "export ZENOH_CONFIG_OVERRIDE='transport/shared_memory/enabled=true;mode=\"client\";connect/endpoints=[\"tcp/192.168.0.42:7447\"]'" >> ~/.bashrc
source ~/.bashrc
4. Open The Web UI
Launch Cyclo Intelligence inside the container:
cyclo_intelligence
Then open the UI in a browser:
http://localhost:7080/
If it runs on another machine, replace localhost with that machine's IP address, for example http://192.168.0.42:7080/.
Setup is done — you can now record demonstrations from the Record page.
cyclo_intelligence is an alias for ros2 launch orchestrator cyclo_intelligence_bringup.launch.py.