Skip to main content

Model Inference

Use Model Inference to load a trained policy and test it in simulation mode before moving the real robot. It also supports TensorRT conversion for faster inference and provides both Async and Sync action request modes.

Cyclo Brain System Architecture

Cyclo Brain runs policy backends as separate Docker containers. The UI sends inference commands to the selected backend, the backend loads the model and computes action chunks, and Cyclo Brain publishes robot commands only when Real Robot Deploy is selected.

Cyclo Brain architecture. 1: the host sends a service call with LOAD, START or PAUSE into Main Runtime. 2: InferenceRequester sends EngineCmd to the EngineWorker in Engine Process. 3: Robot Client reads observations from the robot. 4: the InferenceEngine returns an action_list to ActionChunkProcessor. 5: RobotClient sends the command out to the robot.
  1. Service Call — the host sends LOAD / START / PAUSE into Main Runtime.
  2. EngineCmdInferenceRequester asks the EngineWorker for an action.
  3. Read — the engine's Robot Client reads observations from the robot.
  4. action_list — the InferenceEngine returns predicted actions to ActionChunkProcessor.
  5. Command OutRobotClient publishes the commands to the robot.

Inference Workflow

Use 3D Sim Deploy first to run one action chunk from the current robot state in simulation. This helps check whether the first policy motion is normal before sending commands to the real robot.

Model Inference Workflow

Inference Page

Inference Page

warning

Before running inference on the real robot, stop the teleoperation node or any leader-follower bringup used during data recording. Teleoperation and model inference should not command the robot at the same time.

Then launch the robot follower bringup from OMY Follower Bringup for Inference before using Real Robot Deploy.

Inference Settings

Select The Model And Pull Its Image

Start by choosing the model you trained. Selecting the model also decides which policy backend has to run, and the panel then tells you whether that backend's Docker image is already on the machine.

When the selected policy Docker image has not been downloaded yet, the backend panel shows Image missing. Click Pull to download the policy Docker image that matches the selected model.

Policy Docker Image Pull Button

Pre-built ACT and GR00T policy Docker images are supported only on Blackwell-based amd64 or arm64 environments. If the host environment is not supported, use a compatible machine or prepare a policy backend image that matches the target hardware.

Deploy Target

TargetWhat it does
3D Sim Deploy
  • Runs one action chunk from the robot’s current state, in simulation.
  • Blocks commands to the physical robot.
Real Robot Deploy
  • Sends the policy’s actions to the physical robot.
  • Clear the workspace before you start.

Action Request

ModeUse when
Async
  • Asks for the next action chunk while the control loop keeps running.
  • Not recommended when inference takes a long time.
Sync
  • Waits for the policy to respond before continuing.
  • Use it when inference timing has to line up step by step.

Rates

SettingWhat it controls
Inference Hz
  • How often the model generates a new set of actions.
Control Hz
  • How often commands are published to the robot.

LeRobot Inference

LeRobot inference supports multiple policy families, including ACT, Diffusion, SmolVLA, XVLA, Pi0, and Pi0.5.

LeRobot Task Information

Use this panel when the selected model belongs to the LeRobot group. The main input is Policy Path. If the selected policy uses language conditioning, also enter Task Instruction.

For LeRobot checkpoints, select the exported pretrained_model directory:

/workspace/model/lerobot/<run_name>/checkpoints/<step>/pretrained_model

GR00T N1.7 Inference

GR00T N1.7 uses a task instruction and can optionally use TensorRT acceleration.

GR00T N1.7 Task Information

Use this panel for GR00T N1.7 checkpoints. GR00T uses Task Instruction as part of the inference input, so enter the task instruction before starting inference. Enable TensorRT only when using a TensorRT engine for the selected checkpoint.

For GR00T checkpoints, select the checkpoint folder:

/workspace/model/groot/<run_name>/checkpoint-<step>

Docker Backend Control

After selecting a model, the matching Docker backend control appears in the right panel.

ButtonBehavior
ONCreates or starts the matching policy container.
RestartRestarts the policy container after model-load failures or stale runtime state.
OFFStops the policy container.

If Start is disabled, check the backend status first. Common causes are Policy Docker is off, Not created, Warming up, Main Down, or Engine Down.