Skip to main content

Dataset Preparation - Visualization

Once data collection is complete, you can preview and inspect your recorded dataset using the following steps.

Launch the Dataset Visualization Tool:

Enter the physical_ai_tools Docker container

USER PC

cd physical_ai_tools/docker && ./container.sh enter

Move to the physical_ai_tools/lerobot directory inside the container:

USER PC 🐋 PHYSICAL AI TOOLS

cd /root/ros2_ws/src/physical_ai_tools/lerobot/src

Run the following command to launch the dataset visualization tool:

python lerobot/scripts/visualize_dataset_html.py \
--host 0.0.0.0 \
--port 9091 \
--repo-id YOUR_REPO_ID
  • Replace YOUR_REPO_ID with the dataset ID found under the User ID section in the right sidebar.
  • For example: ROBOTIS/omy_f3m_Test
Web UI

You should see an output similar to the following:

WARNING:root:'torchcodec' is not available in your platform, falling back to 'pyav' as a default decoder
INFO 2025-07-28 06:55:31 set_html.py:364 Output directory already exists. Loading from it: '/tmp/lerobot_visualize_dataset_772b0wso'
* Serving Flask app 'visualize_dataset_html'
* Debug mode: off
INFO 2025-07-28 06:55:31 _internal.py:97 WARNING: This is a development server. Do not use it in a production deployment. Use a production WSGI server instead.
* Running on all addresses (0.0.0.0)
* Running on http://127.0.0.1:9091
* Running on http://192.168.50.127:9091
INFO 2025-07-28 06:55:31 _internal.py:97 Press CTRL+C to quit

Access http://127.0.0.1:9091 to view the dataset. You should see a web interface similar to the one below:

Web UI
tip

Once the server is running, open http://127.0.0.1:9091 in your browser to preview the dataset.