Version Update
Use Version Update to update Cyclo Manager and the container agent.
Package version update is not supported for OMX yet. Only Agent Update and Cyclo Manager Update are currently available.
The Version Management section shows two update targets:
- Agent Update: Updates the Cyclo Manager agent inside a managed container. The agent receives service control requests, streams logs, and reports service status to Cyclo Manager.
- Cyclo Manager Update: Updates the Cyclo Manager CLI, API server, and web UI stack. Use this when a new Cyclo Manager release is available.
Cyclo Manager Update
Use Cyclo Manager Update when a new Cyclo Manager version is available.

This updates the cyclo-manager CLI package on the user PC and restarts the Cyclo Manager stack with the matching API server and web UI images.
- Updates the
cyclo-managerpackage. - Stops the running Cyclo Manager containers.
- Pulls or starts the configured Cyclo Manager API and web UI images.
- Restarts the host agent service.
- Starts Cyclo Manager again with the updated stack.
After the update finishes, reopen the Cyclo Manager web UI in your browser.
If the update fails from the web UI, run the update manually on the user PC:
cyclo-manager update
Agent Update
Use Agent Update when the s6 agent inside a managed container is older than, or not compatible with, the installed Cyclo Manager version. The s6 agent handles service control, log streaming, and status reporting from inside the container, so a version mismatch can cause Cyclo Manager operations to fail or behave unexpectedly.
When Cyclo Manager detects an incompatible container agent, the Container Agents section shows an Update button. Click Update to update the in-container agent to a version compatible with the current Cyclo Manager. The container may restart during the update.