Skip to main content

Assembly Guide

Step-by-Step Assembly Guide for OMX

info
  • Assemble exactly as shown in the official manual video (posture, cable routing, torque)
  • When all joints are at initial point (180°), the posture must match the following reference image exactly.
Reference posture at all joints = 0° (Left)
Reference posture at all joints = 0° (Right)
info
  • While the frame and mounting bolts are included as standard, please note that the camera is sold separately. Please find the external vendor link at the end note of the ROBOTIS eShop product detail page.
Example of anti-slip tape applied

Overview

OMX-AI is operated as a leader–follower system. Each arm has a dedicated role and naming:

  • Leader: OMX-L
    • Role: Human teleoperation input device that generates reference motions
  • Follower: OMX-F
    • Role: Executes the leader's motion precisely in real time

Assembly Guide — OMX-L

Motor Configuration (OMX-L)

JointMotorID
1XL330-M2881
2XL330-M2882
3XL330-M2883
4XL330-M2884
5XL330-M2885
6XL330-M0776
warning
  • Always orient the motor horn upward as shown in the photo.
    Assemble exactly as in the official manual video.
Motor horn orientation

Step 1

Step 2

Step 3

Step 4

Step 5

Step 6

Assembly Guide — OMX-F

Motor Configuration (OMX-F)

JointMotorID
1XL430-W250-T11
2XL430-W250-T12
3XL430-W250-T13
4XL330-M28814
5XL330-M28815
6XL330-M28816
warning
  • Always orient the motor horn upward as shown in the photo.
    Assemble exactly as in the official manual video.
Motor horn orientation

Step 1

Step 2

Step 3

Step 4

Step 5

Step 6


Video: Cable & Camera Assembly

🎉 Assembly Complete

Your OMX assembly is complete. Continue to the next step.

Appendix

tip
  • Applying anti-slip tape to the gripper/contact surfaces, as shown below, can significantly improve grasp efficiency.
Example of anti-slip tape applied