Skip to main content

std_msgs_header

  • File : std_msgs/Header.msg

  • Raw Message Definition

    # Standard metadata for higher-level stamped data types.
    # This is generally used to communicate timestamped data
    # in a particular coordinate frame.
    #
    # sequence ID: consecutively increasing ID
    uint32 seq
    #Two-integer timestamp that is expressed as:
    # * stamp.sec: seconds (stamp_secs) since epoch (in Python the variable is called 'secs')
    # * stamp.nsec: nanoseconds since stamp_secs (in Python the variable is called 'nsecs')
    # time-handling sugar is provided by the client library
    time stamp
    #Frame this data is associated with
    # 0: no frame
    # 1: global frame
    string frame_id
  • Compact Message Definition

    uint32 seq
    time stamp
    string frame_id