Skip to main content

This is a message that holds data to describe the state of a set of torque controlled joints.

  • File : sensor_msgs/JointState.msg
  • Raw Message Definition
# This is a message that holds data to describe the state of a set of torque controlled joints.
#
# The state of each joint (revolute or prismatic) is defined by:
# * the position of the joint (rad or m),
# * the velocity of the joint (rad/s or m/s) and
# * the effort that is applied in the joint (Nm or N).
#
# Each joint is uniquely identified by its name
# The header specifies the time at which the joint states were recorded. All the joint states
# in one message have to be recorded at the same time.
#
# This message consists of a multiple arrays, one for each part of the joint state.
# The goal is to make each of the fields optional. When e.g. your joints have no
# effort associated with them, you can leave the effort array empty.
#
# All arrays in this message should have the same size, or be empty.
# This is the only way to uniquely associate the joint name with the correct
# states.

Header header

string[] name
float64[] position
float64[] velocity
float64[] effort
  • Compact Message Definition
std_msgs/Header header
string[] name
float64[] position
float64[] velocity
float64[] effort