SetJointFeedBackGain srv
-
File:
thormang3_walking_module_msgs/SetJointFeedBackGain.srv -
Message Definition
float32 updating_duration
JointFeedBackGain feedback_gain
---
int32 result
int32 NO_ERROR = 0
int32 NOT_ENABLED_WALKING_MODULE = 2
int32 PREV_REQUEST_IS_NOT_FINISHED = 32
-
Description
A service that can modify joint feedback gain.-
Request
-
float32 updating_duration
Time duration when updating joint feedback gain.
The gains are gradually updated based on configured time.
0 or negative value will update the joint feedback gain immediately. -
JointFeedBackGain feedback_gain(thormang3_walking_module_msgs/JointFeedBackGain)
The joint feedback gain to be applied
-
-
Response
-
int32 result
Result of the "SetJointFeedBackGain" ServiceName Value Description NO_ERROR 0x00 There is no error. NOT_ENABLED_WALKING_MODULE 0x02 The thormang3_walking_module is not enabled. PREV_REQUEST_IS_NOT_FINISHED 0x20 The previous request is not finished.
-
-