SetBalanceParam srv
-
File:
thormang3_walking_module_msgs/SetBalanceParam.srv -
Message Definition
float32 updating_duration
BalanceParam balance_param
---
int32 result
int32 NO_ERROR = 0
int32 NOT_ENABLED_WALKING_MODULE = 2
int32 PREV_REQUEST_IS_NOT_FINISHED = 32
-
Description
A service that can modify Balance Algorithm Parameter.-
Request
-
float32 updating_duration
Time duration when updating Balance Parameter.
The Parameter is gradually updated based on configured time.
0 or negative value will update the Balance Parameter immediately. -
BalanceParam balance_param(thormang3_walking_module_msgs/BalanceParam)
The Balance Parameter to be applied
-
-
Response
-
int32 result
Result of the "SetBalanceParam" ServiceName Value Description NO_ERROR 0x00 There is no error. NOT_ENABLED_WALKING_MODULE 0x02 The thormang3_walking_module is not enabled. PREV_REQUEST_IS_NOT_FINISHED 0x20 The previous request is not finished.
-
-