Skip to main content

JointOffsetPositionData_msg

  • File: thormang3_offset_tuner_msgs/JointOffsetPositionData.msg

  • Message Definition

    string joint_name
    float64 goal_value
    float64 offset_value
    float64 present_value
    int32 p_gain
    int32 i_gain
    int32 d_gain
  • Description
    This message is used when creating GetPresentJointOffsetData.srv.

    • string joint_name
         joint name

    • float64 goal_value
         Joint position for Offset Tuning(Unit in rad)

    • float64 offset_value
         Offset(Unit in rad)

    • float64 present_value
         Current position of the joint

    • int32 p_gain
         P Gain of the joint Position

    • int32 i_gain
         I Gain of the joint Position(Not used for THORMANG3)

    • int32 d_gain
         D Gain of the joint Position(Not used for THORMANG3)