AddStepDataArray srv
-
File:
thormang3_walking_module_msgs/AddStepDataArray.srv -
Message Definition
bool auto_start
bool remove_existing_step_data
StepData[] step_data_array
---
int32 result
-
Description
A service to add StepData to thormang3_walking_module.-
Request
bool auto_start
A flag to initiate walking after adding StepData.bool remove_existing_step_data
A flag to delete existing StepData.StepData[] step_data_array(thormang3_walking_module_msgs/StepData)
An array of StepData to be added
-
Response
-
int32 result
Result of the "AddStepDataArray" Service
Walking will be enabled only with NO_ERRROR result.Name Value Description NO_ERROR 0x00 There is no error. NOT_ENABLED_WALKING_MODULE 0x02 The thormang3_walking_module is not enabled. PROBLEM_IN_POSITION_DATA 0x04 There is some problem in "Step Time Data". PROBLEM_IN_TIME_DATA 0x08 There is some problem in "Step Position Data". ROBOT_IS_WALKING_NOW 0x400 The Thormang3 is walking now.
-
-