Skip to main content

HX Friends

HX Friends is a collection of robot hand designs built on the DYNAMIXEL ecosystem.

The Community Showcase shows how individuals, universities, and companies already use DYNAMIXEL actuators to build open-source robots — including many robotic hands. HX Friends continues that idea: explore diverse hand layouts on the same modular foundation, then invent your own.

Why the DYNAMIXEL Ecosystem​

StrengthWhat it means for hand builders
Versatile actuatorsOne actuator family scales from a simple finger or gripper to high-DOF anthropomorphic hands and full robot platforms
Open-source cultureLabs and companies publish DYNAMIXEL-based designs and tools you can study, remix, and extend
Proven for handsPeer projects such as MIDAS Hand, Orca Hand, Leap Hand, House of Dextra, OpenHand, and others already choose DYNAMIXEL for dexterous manipulation
Modular building blocksFamiliar protocols and replaceable joints keep designs maintainable as you iterate
Global communityA worldwide network of makers and researchers sharing projects proudly Powered by DYNAMIXEL

Together, these strengths give you an open, modular, and practical path to invent the hand that fits your robot and your problem.

HX Friends: HX5-D20​

  • Type: Hand
  • Features: A 20 DOF anthropomorphic reference with a thumb and four fingers — useful when you want to explore human-like coverage and fine multi-finger coordination.
  • Components
HX5-D20 clips — Preset Movements
Preset Movements
HX5-D20 clips — VR Teleoperation
VR Teleoperation
Loading HX5-D20 URDF...

HX5-D20

Drag to orbit, scroll to zoom, and use the sliders to pose joints.

HX Friends: HX4-D12​

  • Type: Hand
  • Features: A 12 DOF design with a thumb and three fingers — a middle ground between dexterity and mechanical simplicity.
  • Components
HX4-D12 clips — Preset Movements
Preset Movements
HX4-D12 clips — VR Teleoperation
VR Teleoperation
Loading HX4-D12 URDF...

HX4-D12

Drag to orbit, scroll to zoom, and use the sliders to pose joints.

HX Friends: HX3-D11​

  • Type: Hand
  • Features: An 11 DOF three-finger reference — a more compact multi-finger option with fewer parts to manage.
  • Components
HX3-D11 clips — Preset Movements
Preset Movements
HX3-D11 clips — VR Teleoperation
VR Teleoperation
Loading HX3-D11 URDF...

HX3-D11

Drag to orbit, scroll to zoom, and use the sliders to pose joints.

HX Friends: HX2-D01​

  • Type: Gripper
  • Features: A gripper built with XM430-W210-R — an example of using a different DYNAMIXEL series for a simpler, robust grasp form factor.
  • Components
HX2-D1-X clip — Gripper Motion
Gripper Motion
info

Interactive 3D model coming soon.

HX Friends: HX1-D03​

  • Type: Finger
  • Features: A 3 DOF all-pitch finger — a minimal block for studying joint stacking and finger motion before you scale to a full hand.
  • Components
HX1-D3 clips — Wave Motion
Wave Motion
HX1-D3 clips — Grasp Motion
Grasp Motion
Loading HX1-D03 URDF...

HX1-D03

Drag to orbit, scroll to zoom, and use the sliders to pose joints.

Get Inspired​

Use these designs as references, not rules. Pose the joints, compare layouts, and notice how actuator choice and DOF change the feel of a hand.

Then invent something we have not shown: a new finger arrangement, a lighter gripper, a task-specific mechanism, or a hybrid that only your application needs. The best next HX Friend is the one you create.

Explore More from the Community​

HX Friends is one slice of a larger DYNAMIXEL world. See what universities, companies, and makers are already building — and bring your own project into that circle.

→ Community Showcase / Ecosystem

You can also dig into ROBOTIS Hand open-source resources: Open Source · Discord