Skip to main content

Software Overview

ROBOTIS Hand is a dexterous robotic hand system designed for real-world Physical AI research and manipulation tasks. It supports high-DOF finger control and enables smooth integration of both teleoperation and AI policy execution.

The platform runs on ROS 2 Jazzy and uses the ros2_control framework for real-time joint-level control. Each hand features 20 degrees of freedom powered by XM335 actuators operating in position mode via TTL communication. The actuators are connected through a Hand Controller Board that converts RS-485 signals from the U2D2 interface to 5 TTL channels, enabling distributed control of finger joints. The system also integrates tactile sensors that provide feedback through ros2_control state interfaces, enabling rich sensory perception for manipulation tasks.

This platform is designed for:

  • Collecting motion data through teleoperation
  • Training reinforcement learning or imitation learning models
  • Running AI-generated trajectories in real time without changing system code

It is suitable for researchers, developers, and integrators working with AI-enabled robotics.

System Architecture

The diagram below illustrates the overall control structure of ROBOTIS Hand.

External teleoperation or trajectory commands are received via ROS 2 topics, processed in real time by ros2_control, and executed by DYNAMIXEL Actuators via TTL.

software_architecture

LayerComponentDescription
Motion Controlros2_control100Hz joint control loop
ActuatorsXM335Position mode via TTL
Hand Controller BoardPCB Board (RS-485)RS-485 to 5 TTL channels
CommunicationU2D2 (RS‑485)4 Mbps, Dynamixel Protocol 2.0
SensorsTactile sensorsRead via ros2_control state_interfaces

Why ros2_control?

ros2_control is a real-time, modular control framework used in ROS 2. ROBOTIS Hand uses it without major changes.

  • Separates control logic from hardware drivers
  • Operates at a fixed 100Hz update rate
  • Supports dynamic loading or replacement of controllers
  • Allows AI policies to send trajectory commands using standard ROS topics

This structure supports both manual operation and AI-based control in the same system.

Motion Execution Pipeline

Input Source (Teleoperation)

ROS 2 JointTrajectory Topic

controller_manager (100Hz)

JointTrajectoryController(s)

resource_manager (interface arbitration)

DynamixelHardwareInterface (position / current)

RS‑485 via Dynamixel SDK

DYNAMIXEL Actuators

Step-by-Step

  1. Trajectory generation — Created by VR, GUI, or AI model
  2. ROS topic publishing — Commands sent to /leader/joint_trajectory_command_broadcaster_*
  3. Controller manager — Runs the main read → update → write loop at 100Hz
  4. JointTrajectoryController — Splits trajectory and commands each joint
  5. Resource manager — Controls access to command interfaces and prevents conflicts between controllers
  6. Hardware interface — Converts commands to RS-485 packets using Dynamixel SDK
  7. Actuators — Execute the motion and return position/current feedback

Controller Configuration & Joint Mapping

ControllerSegmentDOFInput Topic
hand_l_controllerLeft hand20/leader/joint_trajectory_command_broadcaster_left_hand/joint_trajectory
hand_r_controllerRight hand20/leader/joint_trajectory_command_broadcaster_right_hand/joint_trajectory
joint_state_broadcasterAll jointsPublishes to /joint_states
pressure_l_broadcasterLeft sensorsPublishes to /left_hand/finger_pressures
pressure_r_broadcasterRight sensorsPublishes to /right_hand/finger_pressures

Hand controllers use the JointTrajectoryController type.

By default, all joints operate in position mode.

/**:
controller_manager:
ros__parameters:
use_sim_time: False
update_rate: 100 # Hz

joint_state_broadcaster:
type: joint_state_broadcaster/JointStateBroadcaster

hand_l_controller:
type: joint_trajectory_controller/JointTrajectoryController

hand_r_controller:
type: joint_trajectory_controller/JointTrajectoryController

effort_l_controller:
type: effort_controllers/JointGroupEffortController

effort_r_controller:
type: effort_controllers/JointGroupEffortController

pressure_l_broadcaster:
type: robotis_hand_pressure_broadcaster/PressureBroadcaster

pressure_r_broadcaster:
type: robotis_hand_pressure_broadcaster/PressureBroadcaster

/**:
hand_l_controller:
ros__parameters:
joints:
- finger_l_joint1
- finger_l_joint2
- finger_l_joint3
- finger_l_joint4
- finger_l_joint5
- finger_l_joint6
- finger_l_joint7
- finger_l_joint8
- finger_l_joint9
- finger_l_joint10
- finger_l_joint11
- finger_l_joint12
- finger_l_joint13
- finger_l_joint14
- finger_l_joint15
- finger_l_joint16
- finger_l_joint17
- finger_l_joint18
- finger_l_joint19
- finger_l_joint20
command_interfaces:
- position
state_interfaces:
- position
- velocity
allow_nonzero_velocity_at_trajectory_end: true
allow_partial_joints_goal: true

/**:
hand_r_controller:
ros__parameters:
joints:
- finger_r_joint1
- finger_r_joint2
- finger_r_joint3
- finger_r_joint4
- finger_r_joint5
- finger_r_joint6
- finger_r_joint7
- finger_r_joint8
- finger_r_joint9
- finger_r_joint10
- finger_r_joint11
- finger_r_joint12
- finger_r_joint13
- finger_r_joint14
- finger_r_joint15
- finger_r_joint16
- finger_r_joint17
- finger_r_joint18
- finger_r_joint19
- finger_r_joint20
command_interfaces:
- position
state_interfaces:
- position
- velocity
allow_nonzero_velocity_at_trajectory_end: true
allow_partial_joints_goal: true

/**:
effort_l_controller:
ros__parameters:
joints:
- finger_l_joint1
- finger_l_joint2
- finger_l_joint3
- finger_l_joint4
- finger_l_joint5
- finger_l_joint6
- finger_l_joint7
- finger_l_joint8
- finger_l_joint9
- finger_l_joint10
- finger_l_joint11
- finger_l_joint12
- finger_l_joint13
- finger_l_joint14
- finger_l_joint15
- finger_l_joint16
- finger_l_joint17
- finger_l_joint18
- finger_l_joint19
- finger_l_joint20

/**:
effort_r_controller:
ros__parameters:
joints:
- finger_r_joint1
- finger_r_joint2
- finger_r_joint3
- finger_r_joint4
- finger_r_joint5
- finger_r_joint6
- finger_r_joint7
- finger_r_joint8
- finger_r_joint9
- finger_r_joint10
- finger_r_joint11
- finger_r_joint12
- finger_r_joint13
- finger_r_joint14
- finger_r_joint15
- finger_r_joint16
- finger_r_joint17
- finger_r_joint18
- finger_r_joint19
- finger_r_joint20

/**:
pressure_l_broadcaster:
ros__parameters:
topic_name: /left_hand/finger_pressures
sensor_names:
- finger_l_sensor1
- finger_l_sensor2
- finger_l_sensor3
- finger_l_sensor4
- finger_l_sensor5
interface_names:
- Present Pressure 1
- Present Pressure 2
- Present Pressure 3
- Present Pressure 4
- Present Pressure 5
- Present Pressure 6
- Present Pressure 7
- Present Pressure 8
- Present Pressure 9

/**:
pressure_r_broadcaster:
ros__parameters:
topic_name: /right_hand/finger_pressures
sensor_names:
- finger_r_sensor1
- finger_r_sensor2
- finger_r_sensor3
- finger_r_sensor4
- finger_r_sensor5
interface_names:
- Present Pressure 1
- Present Pressure 2
- Present Pressure 3
- Present Pressure 4
- Present Pressure 5
- Present Pressure 6
- Present Pressure 7
- Present Pressure 8
- Present Pressure 9

Debugging & Visualization Tools

Tool / TopicDescription
ros2 control list_controllersList loaded controllers and their status
/joint_statesReal-time joint position and velocity feedback
RViz23D view of robot model (URDF), TF, and movement

Safety & Fault Handling

  • Joint limits are enforced using the URDF and controller configuration
  • Out-of-range values are clamped by the hardware interface (YAML-defined limits)
  • The Dynamixel hardware interface checks for communication errors with each motor