VR Teleoperation Responds Slowly
Check the Wi-Fi connection. Network performance affects VR updates; a wired connection is recommended. See Cannot Connect to the Robot.
If wireless performance is insufficient, host the VR server on the Robot PC and use a USB-C to Ethernet adapter to connect the Meta Quest 3. Connect the Ethernet cable to the robot's LAN port, not the WAN port. See Hardware Setup for port identification.