Skip to main content

← All troubleshooting guides

Map Is Not Generated or LiDAR Data Is Missing

Check whether LiDAR data is being received. In a User PC container terminal with the same ROS 2 and Zenoh settings used for navigation, run:

ros2 topic echo /scan --qos-reliability best_effort

If /scan messages are received but the display is missing in RViz2, set the scan display's Reliability Policy to Best Effort. For connection checks, see ROS 2 Topics Are Not Visible.