Skip to main content

← All troubleshooting guides

Cannot Connect to the Robot

Follow these steps if you cannot connect to the robot through SSH, Cyclo Manager, or Cyclo Intelligence.

1. Check the Network Connection​

Connect your User PC to the same router as the robot. You can use either a wired LAN connection or Wi-Fi.

Connect your PC to the robot's built-in router. The router normally uses 192.168.6.1, and the robot's AGX Orin is configured with the fixed address 192.168.6.2/24.

2. Check for a Network Conflict (SG2 / W2)​

Check the IP address and default gateway of the User PC's connection to the robot's built-in router. On Ubuntu, use:

ip -4 addr
ip route | grep default

With the normal configuration, the PC has a 192.168.6.x address and the router's gateway is 192.168.6.1. Check the address for the interface connected to the robot; a PC can have more than one network connection.

If the PC is on a different network and an external network is connected to the robot's WAN port, check whether that external network also uses 192.168.6.x. When the networks overlap, the built-in router can change its LAN address. The AGX Orin remains at 192.168.6.2, so the PC may no longer be able to reach it. A different PC address alone does not confirm a conflict.

3. Restore the Built-in Router Network (SG2 / W2)​

If the built-in router's LAN address changed because of a network conflict, restore it as follows:

  1. Disconnect the external LAN cable from the robot's WAN port. Disconnecting the cable does not automatically restore the router's LAN settings.
  2. Connect your PC to the robot's Wi-Fi. Open the built-in router's administration page in a browser using the PC's current default gateway address.
  3. Sign in using the robot's full serial number as both the ID and password. For example, if the serial number is SNPR48A0000, use SNPR48A0000 for both.
  4. Change the router's LAN address to 192.168.6.1 with subnet mask 255.255.255.0 (/24). Configure its DHCP pool to assign addresses in 192.168.6.x, excluding 192.168.6.2, which the AGX Orin uses.
  5. After applying the settings, reconnect your PC to the robot's Wi-Fi and check that it receives a 192.168.6.x address.

If you reconnect the WAN cable, use an external network that does not overlap with 192.168.6.0/24. Otherwise, the conflict can happen again.

4. Verify the Connection​

Check the router's connected-device list for the AGX Orin and confirm its IP address. Then test the connection directly; an entry in the list alone does not confirm that SSH or a service is working.

For SG2 and W2, try connecting to the robot's fixed IP address:

  • SSH: ssh robotis@192.168.6.2
  • Cyclo Manager: http://192.168.6.2:3000
  • Cyclo Intelligence: http://192.168.6.2:7080 when Cyclo Intelligence is running on the robot PC and uses the default port.

For BG2 and W1, find the AGX Orin's IP address in the external router's connected-device list and use that address instead. If IP access works but the hostname does not, see Robot PC Access.

5. If the Robot Still Cannot Be Reached​

If the robot still cannot be reached, check its connection to the router. The AGX Orin may not have booted correctly; restart the robot, allow it to finish booting, and try again.