Skip to main content

Software Setup

This guide explains how to connect to the robot PC and prepare a development environment for AI Worker on a separate user PC.

info

The robot PC inside AI Worker is already pre-configured. Follow this guide when you want to access the robot remotely or set up a development environment on your own machine.

Accessing the Robot PC via SSH

AI Worker supports mDNS, allowing you to connect without manually checking the IP address.

  1. Connect the SBC (robot PC) to the same network as your user PC using a LAN cable.

  2. On your user PC terminal, run:

    ssh robotis@ffw-SNPR48A0000.local

Replace SNPR48A0000 with the serial number printed on the back of the robot body. Back of the Follower 3. When prompted, enter the system password root.

If hostname-based access is not available, use one of the following methods:

  1. Connect both your user PC and the AI Worker LAN port to the same router using Ethernet cables, then try SSH again.
  2. Connect a monitor to the Orin via HDMI, log in locally, and check the current IP address before connecting through SSH.
info

Both the Wi-Fi password and the system password are initially configured by ROBOTIS. Change them if required by your security policy.

Development Environment Overview

AI Worker relies on two main repositories:

  • ai_worker: Provides support for controlling DYNAMIXEL actuators using ros2_control and enables teleoperation functionality.
  • physical_ai_tools: Provides tools for data collection, training, model inference, and visualization.
danger

⚠️ On the AI Worker Orin: Do not run apt upgrade. Upgrading system packages may create conflicts and break robot functionality.

Prerequisites

  • Operating System: Ubuntu environment
    • The AI WORKER software runs inside a Docker container based on Ubuntu 24.04 (ROS 2 Jazzy), so the host Ubuntu version on the user PC does not need to match exactly.
  • Container Engine: Docker Engine
  • Version Control: Git
  • Graphics Support
    • NVIDIA Graphics Driver
      • (In Docker-based environments, the container is generally isolated from the host system. However, the graphics driver version on the host can have a direct impact on performance and compatibility—especially when using GPU acceleration. We recommend using the following driver version(s) for best results)
      • Install nvidia-driver-570-server-open for CUDA 12.8
      • Verify the driver with nvidia-smi
    • NVIDIA Container Toolkit

Configuration

Docker Volume Management

The Docker container uses the following volume mappings for data persistence and hardware access:

volumes:
# Hardware and System Access
- /dev:/dev
- /tmp/.X11-unix:/tmp/.X11-unix:rw
- /tmp/.docker.xauth:/tmp/.docker.xauth:rw

# Development and Data Storage
- ./workspace:/workspace
- ../:/root/ros2_ws/src/ai_worker/
- ./lerobot/outputs:/root/ros2_ws/src/physical_ai_tools/lerobot/outputs
- ./huggingface:/root/.cache/huggingface
warning

Container data is volatile and will be lost when the container is removed. Store important files in mapped volumes such as /workspace, the mapped source directory, model output directories, and the Hugging Face cache.

Container Management

  1. Clone the repository:

    cd ~/ # or your preferred directory
    git clone -b jazzy https://github.com/ROBOTIS-GIT/ai_worker.git
    cd ai_worker
  2. Use the container.sh helper script to manage the container:

    ./docker/container.sh start
    ./docker/container.sh enter
    ./docker/container.sh stop

Docker Command Guide

The container.sh script provides the following commands:

  • help: Display the help message.
  • start: Start the AI Worker container.
  • enter: Enter the running container.
  • stop: Stop the AI Worker container.

Example usage:

./container.sh help
./container.sh start
./container.sh enter
./container.sh stop

Software Update Guide

Follow these steps to update the AI Worker or Physical AI Tools packages:

  1. Move to the package directory:

    cd /path/to/ai_worker_package
    # or
    cd /path/to/physical_ai_tools_package
  2. Switch to the jazzy branch:

    git checkout jazzy
  3. Pull the latest code:

    git pull
  4. Restart the container:

    ./docker/container.sh stop
    ./docker/container.sh start
warning

Data stored outside mapped volumes may be lost during container restart. Save important files before restarting the container.

Checking Battery State

The FFW-SG2 model has two batteries. The FFW-BG2 model does not use a battery.

To check the battery state, run:

# Check the left battery
ros2 topic echo /ai_worker/battery/left/state --once

# Check the right battery
ros2 topic echo /ai_worker/battery/right/state --once

The output includes the following keys:

  • frame_id: Identifies which battery the message refers to.

    frame_id: battery_left
  • voltage: Shows the current battery voltage.

    voltage: 28.700000762939453 # Battery voltage 28.7V
  • percentage: Shows the remaining battery level as a value from 0.0 to 1.0.

    percentage: 0.934949517250061 # Battery 93% charged