Checking Battery State
The SG2 and W2 models each have two batteries. The BG2 and W1 models do not use batteries.
Check Battery State
To check the battery state, run:
# Check the left battery
ros2 topic echo /ai_worker/battery/left/state --once
# Check the right battery
ros2 topic echo /ai_worker/battery/right/state --once
The output includes the following keys:
-
frame_id: Identifies which battery the message refers to.frame_id: battery_left -
voltage: Shows the current battery voltage.voltage: 28.700000762939453 # Battery voltage 28.7V -
percentage: Shows the remaining battery level as a value from0.0to1.0.percentage: 0.934949517250061 # Battery 93% charged