Skip to main content

Bringup Guide

This guide explains how to bring up the AI Worker robot. Complete Hardware Setup before continuing.

1. Network Connection​

These models do not have a built-in router. Connect the robot's LAN port to an external router, then connect your PC to the same router using Wi-Fi or LAN. An external router is not included with the robot.

2. Open Cyclo Manager​

Open http://ffw-<serial_number>.local:3000 in a browser on your PC, replacing <serial_number> with the serial number printed on the robot. For example, if the serial number is SNPR48A0000, open http://ffw-SNPR48A0000.local:3000. You can also use the robot's IP address with port 3000.

Use Cyclo Manager to bring up the robot. Cyclo Manager is pre-installed on W1 and W2 models. If it has not been installed, follow Install.

Open the System page in Cyclo Manager to begin bringup.

System Page

3. Start the Zenoh Daemon​

RMW_ZENOH NOTIFICATION

AI Worker uses Zenoh as RMW since version 2.0.0. Start the Zenoh daemon before bringing up the robot stack. For more information about Zenoh, see Zenoh Communication.

Click the arrow icon in the Zenoh Daemon control box to start the Zenoh daemon. Check that the status light turns green. Once started, the Zenoh daemon restarts when the robot powers on.

Zenoh Daemon

4. Bringup the Robot​

warning

Starting robot bringup will cause the robot to move.
Before starting, make sure the area around the robot is clear and keep the emergency stop within reach.

Select the robot model to bring up and click the Robot Bringup(▶️) button. For W1 and W2, select F1 and F2, respectively, in Cyclo Manager. The status light turns green when the robot service starts. Click the paper icon on the far right to view the logs in the side panel.

Robot Bringup Button

After the robot stack starts, the 3D model and robot status panels update automatically. If the model or joint states do not update, check ROS_DOMAIN_ID, the robot bringup logs, and the relevant ROS 2 topics.

Robot bringup in Cyclo Manager

5. Check Robot Operation​

After bringup, check that the robot responds to movement commands.

warning

Keep the area around the robot clear and the emergency stop within reach. Leave leader teleoperation and other motion-command sources stopped while using Jog.

  1. Open Jog in Cyclo Manager and select the ai_worker container if prompted.

  2. Check that the robot bringup status and joint positions are available, then turn on Enable jog.

    Cyclo Manager Jog page with the Jog menu and Enable jog control highlighted

  3. Use the controls to check the following:

    • Joints: Check that each joint moves properly.
    • Mobile base: For models with a mobile base, check that it moves and rotates properly.

For more about the controls, see Jog.

6. Check Cameras​

Check that the robot's cameras provide live images in Cyclo Intelligence.

  1. Return to the System page in Cyclo Manager. Click the start arrow in Cyclo Intelligence and wait for the status light to turn green.

    Cyclo Intelligence start button in Cyclo Manager

  2. Click the I button in Cyclo Manager to open Cyclo Intelligence. You can also open http://ffw-<serial_number>.local:7080 in a browser on your PC. For example, use http://ffw-SNPR48A0000.local:7080 or the robot's IP address with port 7080.

    Cyclo Intelligence shortcut in Cyclo Manager

  3. On the Home page, select the robot type and click Set Robot Type.

    Robot type selection in Cyclo Intelligence

  4. Open Record and check Camera Views. Confirm that each configured camera displays a live image and that the image updates as the scene changes.

    Live camera images on the Cyclo Intelligence Record page

To connect directly to the robot and run it from the command line, see CLI Bringup & Teleoperation.