Skip to main content

Cyclo Intelligence

Cyclo Intelligence is a Physical AI workflow system for robots. It can be used with OMY, OMX, AI Worker, and other robots that provide ROS 2 topics.

It provides a web UI for collecting datasets, managing datasets, converting datasets to LeRobot format, and deploying trained models.

Cyclo Intelligence is organized around two major subsystems.

Cyclo Data handles dataset collection, dataset management, and LeRobot conversion. Cyclo Brain handles policy runtime, model loading, and robot inference.

Start Cyclo Intelligence

Start from the Cyclo Intelligence repository on the robot PC.

For a first-time installation:

ROBOT PC

cd $HOME
git clone --recurse-submodules https://github.com/ROBOTIS-GIT/cyclo_intelligence.git
cd $HOME/cyclo_intelligence
./docker/container.sh start

For an existing installation:

cd $HOME/cyclo_intelligence
git pull
git submodule update --init --recursive
./docker/container.sh start

Common container commands:

CommandDescription
./docker/container.sh startPull the published image if needed and start Cyclo Intelligence.
./docker/container.sh statusCheck the service status inside the running containers.
./docker/container.sh logsTail Cyclo Intelligence logs.
./docker/container.sh enterOpen an interactive shell inside the Cyclo Intelligence container.
./docker/container.sh stopStop and remove compose-managed containers.

Open the web UI in your browser.

http://<robot-ip>/

For local access on the robot:

http://127.0.0.1/

The container uses /workspace as its working data directory. On the host, this is bind-mounted from:

$HOME/cyclo_intelligence/docker/workspace

Home Page

On the Home page, select the robot type before using Record or Inference.

Cyclo Intelligence Home Page

  1. Click Refresh Robot Type List.
  2. Select the current robot in Select Robot Type.
  3. Click Set Robot Type.
  4. Check that the UI changes to the connected state.

The selected robot type is used by the orchestrator, recording pipeline, dataset conversion options, and Cyclo Brain inference runtime.

Cyclo Data Workflow

Cyclo Data System Architecture

Cyclo Data is operated from the Web UI. The user records robot demonstrations, edits the collected dataset with Data Tools, converts it to LeRobot format, and uploads or downloads datasets and models through Hugging Face.

UIrecorddata toolsconvertHub
Web UIOperate Everything from UISelect the robot, open Record, and use Data Tools without leaving Cyclo Intelligence.
Record PageAcquire DatasetCapture ROS 2 robot topics, camera streams, task metadata, and episode information.
Data ToolsEdit and Prepare DatasetDelete episodes, merge datasets, or prepare the dataset for LeRobot conversion.
OutputsLeRobot / Hugging FaceCreate LeRobot datasets and move datasets or models through Hugging Face.
Dataset AcquisitionRecord
  • Camera streams are stored as MP4 files with frame timestamps.
  • Non-camera ROS 2 topics are stored in MCAP format.
  • Camera rotation is saved according to the robot config file.
  • Each save creates an episode dataset.
Dataset EditingDelete / Merge
  • Delete unnecessary or failed episodes.
  • Merge multiple collected datasets.
  • Keep the dataset organized before conversion.
Dataset ConversionLeRobot Convert
  • Select the target FPS for LeRobot conversion.
  • Align sensor/action timelines and video frames.
  • Write LeRobot v2.1 and/or v3.0 output.
Repository OperationHugging Face
  • Upload collected or converted datasets.
  • Download datasets for editing or conversion.
  • Download models for later deployment.

Record Page

The Record page collects robot demonstrations and stores them through cyclo_data.

The current Record page is organized around a top status and control bar, a live image grid, a lower monitoring area, and a collapsible Task Information panel.

Record Page with Task Information

AreaDescription
Top status and control barRobot type, joystick mode, system status, and recording control buttons.
Center image gridCamera streams selected from the robot topics.
Lower monitoring area3D robot viewer and Record Topic Monitor.
Right Task Information panelTask number, task name, task instruction, and session preparation.

Recording Workflow

  1. Open the Record page after setting the robot type.
  2. Select or confirm the camera topics shown in the center view.
  3. Fill out Task Num, Task Name, and Task Instruction.
  4. Click the session preparation button to arm the task on the orchestrator.
  5. Use Record, Save, or Discard from the top control bar as needed.

Collected Dataset Location

Collected rosbag2 datasets are stored under /workspace/rosbag2 inside the Cyclo Intelligence container.

Container path:

/workspace/rosbag2/<dataset_name>/<episode_index>/

Host path:

$HOME/cyclo_intelligence/docker/workspace/rosbag2/<dataset_name>/<episode_index>/

Example:

/workspace/rosbag2/Task_1_1_MCAP/0/

Episode Folder Structure

Each episode is stored as a self-contained folder.

<episode_index>/
|-- metadata.yaml
|-- episode_info.json
|-- 0_0.mcap
|-- videos/
| |-- cam_head_left.mp4
| |-- cam_head_left_timestamps.parquet
| |-- cam_head_right.mp4
| |-- cam_head_right_timestamps.parquet
| |-- cam_wrist_left.mp4
| |-- cam_wrist_left_timestamps.parquet
| |-- cam_wrist_right.mp4
| `-- cam_wrist_right_timestamps.parquet
`-- camera_info/
|-- cam_head_left.yaml
|-- cam_head_right.yaml
|-- cam_wrist_left.yaml
`-- cam_wrist_right.yaml
File or folderPurpose
metadata.yamlrosbag2 metadata for the recorded episode.
episode_info.jsonTask instruction, episode metadata, recording diagnostics, and video status.
*.mcaprosbag2 MCAP file. Long recordings may be split into multiple MCAP files.
videos/*.mp4Camera streams recorded as MP4 files.
videos/*_timestamps.parquetPer-camera frame timestamps used for accurate LeRobot video synchronization.
camera_info/*.yamlCamera calibration snapshots captured with the episode.
tip

Recording stores camera video and timestamp sidecars separately from MCAP. Compared with storing camera frames inside MCAP, MP4 video is more storage-efficient and keeps conversion faster because LeRobot video synchronization can use the MP4 file and timestamp Parquet directly.

Cyclo Data Backend Responsibilities

cyclo_data owns the data plane for Cyclo Intelligence. The UI sends a record command to the orchestrator, and the orchestrator forwards the request to cyclo_data. From there, cyclo_data handles the bag writer, video encoding, dataset conversion, dataset editing, and Hugging Face operations.

StageOwnerDescription
Recordcyclo_data + rosbag_recorderRecords robot topics and camera streams into a task folder.
Encodecyclo_data.recorderWrites camera streams as MP4 files and tracks recording metadata.
Convertcyclo_data.converterConverts MCAP and MP4 data into LeRobot dataset formats.
Managecyclo_data.editor / cyclo_data.hubEdits datasets and uploads or downloads Hugging Face repositories.

The recording status is published by cyclo_data on /data/recording/status.

StatusMeaning
READYThe recorder is idle and ready for a new session.
RECORDINGThe current episode is being recorded.
SAVINGThe episode is being finalized and encoded.
CONVERTINGThe collected dataset is being converted from rosbag and MP4 into LeRobot dataset output.
PAUSEDRecording is paused and can be resumed.

Data Tools Page

The dataset tools use the same cyclo_data backend as recording.

Use Dataset Tools to manage collected datasets, move datasets or models through Hugging Face, and convert rosbag2 task folders into LeRobot dataset outputs.

Data Tools Overview

ToolDescription
Delete EpisodesRemoves selected episodes from a dataset.
Merge DatasetCombines multiple rosbag task folders into a single output dataset.
Convert DatasetConverts collected rosbag2 datasets into LeRobot dataset output.
Hugging Face upload/downloadManages dataset and model repositories through the configured Hugging Face endpoint.

Long-running data operations publish progress through Cyclo Intelligence status topics so the UI can show conversion and Hub progress without blocking the recording workflow.

Convert to LeRobot Dataset

Use Convert Dataset when the collected rosbag2 dataset is ready to be converted into a LeRobot-compatible dataset.

  1. Open Dataset Tools.
  2. Select the dataset folder under /workspace/rosbag2.
  3. Choose the target FPS. If no FPS is specified, the converter uses the default conversion FPS.
  4. Select LeRobot v2.1, LeRobot v3.0, or both.
  5. Start conversion and wait until the progress status completes.

Conversion output is written under /workspace/lerobot.

Output optionExample output path
LeRobot v2.1/workspace/lerobot/Task_1_1_MCAP_lerobot_v21
LeRobot v3.0/workspace/lerobot/Task_1_1_MCAP_lerobot_v30

During conversion, Cyclo Data parses the recorded MCAP topics, aligns actions and observations to the requested FPS, selects the matching MP4 frames using the camera timestamp Parquet files, and writes the LeRobot dataset metadata, Parquet data, and synced videos.

tip

In the current Cyclo Data conversion path, video synchronization streams selected MP4 frames directly into ffmpeg instead of creating temporary JPEG files. This reduces conversion time for recording-format-v2 datasets.

Hugging Face Dataset and Model Management

The Hugging Face tools can upload local folders or download remote repositories.

Data typeDefault local path
Dataset/workspace/rosbag2
Model/workspace/model

The folder browser opens from /workspace, so both collected datasets and downloaded models can be selected from the same root.

Cyclo Brain Workflow

Cyclo Brain is the model deployment and inference runtime inside Cyclo Intelligence. It runs policy backends as Docker containers and exposes them to the UI through one Inference page.

Cyclo Brain splits each policy backend into two processes.

ProcessResponsibility
main-runtimeReceives external inference commands, owns session state, manages the action chunk buffer, and publishes robot command topics.
engine-processLoads the policy model, reads robot observations, and computes action chunks. It does not publish robot commands directly.

The architecture map below shows how Host, main-runtime, engine-process, the open-source backend island, and Robot are connected.

Cyclo Brain System Architecture

Cyclo Brain separates command handling, model inference, open-source policy backends, and robot I/O into distinct runtime areas. The diagram below shows the system blocks first; detailed data flow is summarized after the diagram.

external commandengine request / action_listsensor / state readrobot command publishopen-source backend

Host

Command SourceUI / OrchestratorStandalone CLI argssame command shape
InferenceCommandLOAD / START / PAUSERESUME / STOP / UNLOADexternal service

Policy Container: <backend>_server

Main Runtime

main-runtimeServiceHandlercommand entry
main-runtimeSessionStateruntime gate
main-runtimeInferenceRequesterone GET_ACTION at a timetimeout + seq_id stale guard
main-runtimeActionChunkProcessorbuffer + optional match / RTCinterpolate / blend / smooth
main-runtimeControlLoopself-running tick
main-runtimeRobotClientcommand output

Engine Process

engine-processEngineWorkerhosts internal EngineCommand serviceusing Zenoh ROS2 SDK
engine-processBackend InferenceEnginemodel-specific implementationbehind stable contract
Policy LoadPreprocessPredictOptional Optimize
engine-processRobotClientobservation only
Open-source backend islandLeRobotGR00TFuture model

Robot

Sensors / StateObservation inputcamera, joints, base state
Command TopicsCommand outputcmd_vel, trajectory, etc.
service callEngineCommandaction_listprocessed actionsone action / ticksensor / state readobservation to inferencecommand outbackend contract12345
  1. UI/CLI command enters Main. The command reaches main-runtime through the external service.
  2. Main requests Engine action. InferenceRequester sends one EngineCommand at a time.
  3. Engine reads Robot observation. The engine-side RobotClient reads camera, joint, and base state.
  4. Engine returns action_list. The backend policy loads the model, preprocesses observations, predicts, and optionally optimizes.
  5. Main buffers/processes/publishes. ActionChunkProcessor can turn 16 actions into a 100 Hz buffer, and ControlLoop publishes one action per tick.

The data flow is:

  1. The UI sends a LOAD, START, STOP, or UNLOAD style command.
  2. main-runtime receives the command and updates the session state.
  3. main-runtime asks engine-process to load a model or compute actions through an internal Zenoh service.
  4. engine-process reads robot observations, runs model inference, and returns an action chunk.
  5. main-runtime pushes the chunk into the action buffer and publishes one robot command per control-loop tick.

LeRobot and GR00T use the same runtime contract. The model loading, preprocessing, and prediction implementation are handled by each backend.

Inference Page

Use the Inference page to select a policy backend, start the matching Docker runtime, load a model, and run inference.

Cyclo Brain Inference Page

The top Inference control bar is shared by all backends.

ButtonDescription
StartLoads the model and starts inference. In paused state, resumes inference when the policy path is unchanged.
StopPauses inference. The model remains loaded in memory.
ClearStops inference and clears the model, session, and action buffer.
RecordStarts recording inference results when recording is enabled.
SaveSaves the current inference recording.
DiscardDiscards the current inference recording.

If Start is disabled, check the Docker backend state in the right panel. Common causes are OFF, Image missing, Warming up, Main Down, or Engine Down.

Model Selection

On the Inference page, select the policy backend and model family from Task Information > Model.

Cyclo Brain Model Selection

GroupModelBackendDescription
LeRobotACTlerobot_serverLoads a LeRobot ACT checkpoint.
LeRobotSmolVLAlerobot_serverLoads a LeRobot SmolVLA checkpoint and uses task instructions.
LeRobotXVLAlerobot_serverLoads a LeRobot XVLA checkpoint and uses task instructions.
LeRobotPi0lerobot_serverLoads a LeRobot Pi0 checkpoint and uses task instructions.
LeRobotPi0.5lerobot_serverLoads a LeRobot Pi0.5 checkpoint and uses task instructions.
LeRobotDiffusionlerobot_serverLoads a LeRobot Diffusion checkpoint.
GR00TGR00T N1.7groot_serverLoads an NVIDIA Isaac GR00T N1.7 checkpoint and uses task instructions.

The following entries can appear in the UI but are disabled until their runtime path is validated.

  • GreenVLA
  • OpenPI
  • RLDX-1

Docker Backend Control

After selecting a model, the matching Docker backend control appears in the right panel.

ButtonBehavior
ONCreates or starts the matching policy container. If it is already running, it restarts the container to reset the runtime.
RestartRestarts the policy container. Use this after model-load failures, stale services, or CUDA memory cleanup needs.
OFFStops the policy container without deleting the container or image.

Two process states are shown for each backend.

ProcessUp meansIf Down or Unknown
MainThe main-runtime service is alive.Press Restart to bring the backend up again.
EngineThe engine-process service is alive.Model loading or inference calls may fail. Press Restart first.

Main Up and Engine Up mean the backend processes are alive. They do not mean that a model is already loaded. Model loading happens after pressing Start with the current Policy Path.

LeRobot Deployment

LeRobot Inference Setup

  1. Select a policy under the LeRobot group.
  2. Check that LeRobot Docker is Running.
  3. Check that both Main and Engine are Up.
  4. Enter a Hugging Face repo ID or a local checkpoint path in Policy Path.
  5. For language-conditioned policies, enter Task Instruction.
  6. Set Inference Hz to match the model action generation rate.
  7. Set Control Hz to match the robot command publish rate.
  8. Click Start.

Example Hugging Face repo ID:

ROBOTIS/Act_test_20k

Example local checkpoint path:

/policy_checkpoints/lerobot/Act_test_20k

ACT and Diffusion do not use task instructions, so the task instruction field is hidden for those model families.

GR00T N1.7 Deployment

GR00T N1.7 Inference Setup

  1. Select GR00T N1.7 under the GR00T group.
  2. Check that GR00T Docker is Running.
  3. Check that both Main and Engine are Up.
  4. Enter the task instruction in Task Instruction.
  5. Enter the model path in Policy Path.
  6. Click Start.
  7. To update the instruction during inference, edit the text and click Update Task Instruction.

Example Hugging Face repo ID:

ROBOTIS/cyclo_intelligence_groot_n1.7_model

Example local checkpoint path:

/policy_checkpoints/groot/cyclo_intelligence_groot_n1.7_model

Model File Locations

Policy checkpoint folders are bind-mounted into each policy container.

BackendHost pathContainer path
LeRobot$HOME/cyclo_intelligence/cyclo_brain/policy/lerobot/checkpoints/policy_checkpoints/lerobot
GR00T$HOME/cyclo_intelligence/cyclo_brain/policy/groot/checkpoints/policy_checkpoints/groot

If the host model is here:

$HOME/cyclo_intelligence/cyclo_brain/policy/lerobot/checkpoints/Act_test_20k

Enter this path in the UI:

/policy_checkpoints/lerobot/Act_test_20k

Troubleshooting

Start Is Disabled

Check the backend status in the right panel.

  • Image missing: pull or install the required Docker image.
  • Stopped or Not created: click ON.
  • Warming up: wait until both Main and Engine are Up.
  • Main Down or Engine Down: click Restart.

Model Load Failed

  1. Check that Policy Path is correct.
  2. If you use a local path, make sure it is a container path such as /policy_checkpoints/....
  3. If you use a Hugging Face repo ID, check network access and token permissions.
  4. Check that the selected UI model family matches the checkpoint type.
  5. Click Clear to reset the inference session.
  6. If it still fails, restart the Docker backend and try again.

Dataset Conversion Failed

  1. Check that the task folder exists under /workspace/rosbag2.
  2. Check storage space before retrying conversion.
  3. If a LeRobot output already exists for the same source dataset, delete or rename the old output before running conversion again.
  4. Retry the conversion from the dataset tools page.