Skip to main content

Advanced Features

Overview

This section covers advanced control and autonomy features that extend the AI Worker's capabilities beyond basic imitation learning. These features enable more sophisticated task execution, decision-making, and adaptive behaviors in complex real-world scenarios.

Available Features

1. Cyclo Control

Cyclo Control is the software layer that turns easier robot commands, such as target hand poses or joint commands, into joint trajectories that the real robot can execute. It is useful when you want higher-level motion commands while still relying on the controller to generate safe robot motion.

  • Higher-Level Commanding: Command target poses or joint goals instead of manually sending every joint step
  • Interpolated Motion: Generate smooth MoveL and MoveJ motions from the current state to the goal over a requested time
  • QP-Based Safety: Apply constraints such as joint range, joint velocity, and self-collision avoidance while tracking the command

On AI Worker, this is especially helpful when you want motion that is easier to command than raw low-level control, but still filtered through the controller's safety-aware optimization.

Learn More About Cyclo Motion Controller

2. ROBOTIS Vuer

ROBOTIS Vuer lets AI Worker use a Meta Quest 3 headset together with a browser-based Vuer client for immersive robot interaction. The headset connects to the robot-side ROS 2 system through HTTPS/WSS, allowing the system to exchange pose, visualization, and control data in real time.

  • Immersive Monitoring: View the robot scene and related 3D information directly in the headset
  • Hand-Tracking Interaction: Use VR hand tracking and related input as references for robot control
  • Browser-Based Workflow: Start the VR session from the headset browser without installing a separate native application
  • ROS 2 Integration: Connect the Vuer-based VR interface with the robot-side ROS 2 stack for teleoperation and state visualization

In AI Worker, ROBOTIS Vuer is used as the front-end interface for VR teleoperation. Vuer handles the browser-side 3D scene and WebXR interaction, while ROS 2 nodes on the robot side process the incoming references and connect them to the robot control pipeline.

Learn More About ROBOTIS Vuer