Skip to main content

Software Architecture

AI Sapiens K1 runs its robot software inside the ai_sapiens Docker container on the NVIDIA® Jetson Orin™ NX 16GB module. The base system uses Cyclo OS, a Yocto Project-based operating system, with ROS 2 Jazzy and rmw_zenoh_cpp for low-latency robot communication.

The control stack is built around ROS 2 control. High-level robot commands are converted into joint commands, passed through the ROS 2 controller manager, written to DYNAMIXEL-Q actuators over multiple RS-485 buses at 6 Mbps, and reported back through ROS 2 state topics.

AI Sapiens Software Architecture Overview

Architecture Flow​

Runtime Stack​

LayerRole
NVIDIA® Jetson Orin™ NX 16GBOnboard compute module for robot runtime, ROS 2 nodes, and policy execution
Cyclo OSYocto Project-based robot operating system
ai_sapiens Docker containerRobot software container for the AI Sapiens ROS 2 stack
ROS 2 JazzyRobot middleware, node graph, topics, services, and ROS 2 control runtime
rmw_zenoh_cppDefault ROS 2 RMW layer for communication between robot-side nodes, containers, and external PCs

External PC setup is documented separately in ROS 2 Communication. The sections below focus on the onboard software architecture.

Control Flow​

The command path moves from a policy or user command down to the actuator bus:

ai_sapiens_sim2real produces robot joint commands from policy output, mode logic, and user command inputs. The joint_group_impedance_controller receives those commands and exposes them to dynamixel_hardware_interface through ROS 2 control command interfaces. The hardware interface uses DynamixelSDK to write position, feedforward torque, and impedance-control gains to the DYNAMIXEL-Q actuators.

State Flow​

The feedback path moves from the robot hardware back into ROS 2:

DYNAMIXEL-Q actuators report present position, present velocity, and present current through the hardware interface. The HAT board and IMU board are also exposed through the same ROS 2 control hardware layer, so emergency-stop state, remote-controller channels, and IMU measurements can be published as ROS 2 topics. Battery monitoring interfaces are available on the HAT board hardware layer.

ROS 2 Control Layer​

AI Sapiens K1 uses controller_manager at a 1 kHz update rate. The controller layer includes:

ComponentPurpose
joint_state_broadcasterPublishes actuator position, velocity, and effort as /joint_states
imu_sensor_broadcasterPublishes IMU orientation, angular velocity, and linear acceleration
rc_broadcasterPublishes remote-controller input and RC link status from the HAT board state interfaces (ai_sapiens_rc_broadcaster plugin)
joint_group_impedance_controllerReceives joint position, feedforward, kp, and kd commands for impedance control mode (ai_sapiens_joint_group_impedance_controller plugin)
dynamixel_hardware_interfaceBridges ROS 2 control command/state interfaces to DynamixelSDK
DynamixelSDKHandles packet communication with DYNAMIXEL-Q actuators and boards over RS-485

The controller command order is defined by the bringup controller configuration. For the detailed joint index map and command message definition, see ROS 2 Package Structure.

Main ROS 2 Interfaces​

/joint_statesHardware to ROS 2
Typesensor_msgs/msg/JointState

Joint position, velocity, and effort feedback.

/imu_sensor_broadcaster/imuHardware to ROS 2
Typesensor_msgs/msg/Imu

Pelvis IMU orientation, angular velocity, and linear acceleration.

/joint_group_impedance_controller/commandsROS 2 to controller
Typeai_sapiens_interfaces/msg/JointImpedanceCommand

Joint position, feedforward torque, and impedance-control gain command.

/ai_sapiens_rc/inputRC broadcaster to ROS 2
Typesensor_msgs/msg/Joy

Normalized remote-controller axes and buttons.

/ai_sapiens_rc/statusRC broadcaster to ROS 2
Typeai_sapiens_interfaces/msg/RcStatus

RC link, failsafe, and HAT-board status.

/cmd_velUser/API to runtime
Typegeometry_msgs/msg/Twist

Velocity command input for API-controlled behavior.

/ai_sapiens/api_heartbeatUser/API to runtime
Typeai_sapiens_interfaces/msg/ApiHeartbeat

Advancing-sequence heartbeat required while API authority is active.

/ai_sapiens/set_mode_by_nameUser/API to runtime
Typeai_sapiens_interfaces/srv/SetModeByName

Requests a named robot control mode.

/ai_sapiens/list_modesUser/API to runtime
Typeai_sapiens_interfaces/srv/ListModes

Lists available robot control modes.

/ai_sapiens/mode_statusRuntime to ROS 2
Typeai_sapiens_interfaces/msg/ModeStatus

Current mode and command authority status.