Skip to main content

Open Source

AI Sapiens is designed as an open platform. This page lists the public repositories used to inspect, modify, simulate, and build applications for the robot.

Where should I start?
  • For the K1 ROS 2 software stack, start with ai_sapiens.
  • To train or test policies in simulation, start with cyclo_lab.

AI Sapiens Repositories​

These repositories are maintained by ROBOTIS and provide the main software and documentation for AI Sapiens.

CategoryRepositoryWhat it providesGuide
Robot platformROS 2ROBOTIS-GIT/ai_sapiensK1 robot description, bringup, controllers, interfaces, Docker environment, and Sim2Real runtimeSoftware ArchitectureROS 2 Package Structure
SimulationReinforcement learningROBOTIS-GIT/cyclo_labIsaac Lab environments, task definitions, policy training, motion imitation, and Sim2Real workflows for ROBOTIS robotsCyclo Lab

Simulation Models​

The currently available robot-description and simulation models for AI Sapiens K1 are listed below.

FormatRepository locationUse
URDFai_sapiens_description/urdf/k1_rev1ROS 2 robot description, RViz visualization, and downstream model conversion
MJCFai_sapiens_description/mujoco/k1MuJoCo simulation model and scene configuration

USD is not yet publicly available. Its repository location will be added here when it is released.

Motion Generation and Retargeting​

These ROBOTIS repositories provide K1-specific integration for the AI Sapiens motion workflow.

CategoryRepositoryAI Sapiens role
Video-to-motion generationROBOTIS-GIT/GEM-XForked from NVlabs/GEM-XRecovers SOMA-format human motion from monocular video and adds the ai_sapiens_k1 retargeting path
Motion retargetingROBOTIS-GIT/soma-retargeterForked from NVIDIA/soma-retargeterConverts SOMA/BVH motion to K1 joint trajectories using the AI Sapiens robot description and mesh assets
Text-to-motion generationROBOTIS-GIT/kimodoForked from nv-tlabs/kimodoGenerates source motion from text and kinematic constraints for conversion or retargeting in the K1 motion workflow

See GEM-X, Soma-retargeter, and Kimodo for installation and AI Sapiens workflow details.

Shared ROBOTIS Software​

These ROBOTIS repositories provide actuator-control and learning components used by the wider AI Sapiens stack.

CategoryRepositoryRole
ROS 2 hardware interfaceROBOTIS-GIT/dynamixel_hardware_interfaceConnects ROS 2 control command and state interfaces to DYNAMIXEL actuators
Actuator communication SDKROBOTIS-GIT/DynamixelSDKImplements DYNAMIXEL packet communication used by the hardware interface
Imitation learning platformROBOTIS-GIT/cyclo_intelligenceData recording, dataset conversion, policy training, inference, and robot execution; the AI Sapiens guide is coming soon

Additional Resources​

ResourceAvailable filesGuide
AI Sapiens K1 hardware drawingPDFHardware Specifications

Planned Resources​

The source-code repositories are available above. The following additional resources are planned for future release.

Coming Soon

Hardware BoM​

The complete Bill of Materials for K1, including parts, quantities, and references, will be published for reproducible builds.

STEP Files​

Mechanical STEP files for core assemblies are planned so teams can inspect, customize, and integrate K1 hardware.

Tutorial Videos​

Tutorial videos covering bring-up through policy deployment will be added to help new users get started.

Open Source Licenses​

AreaDefault license
Hardware resources released by ROBOTISCERN-OHL-P-2.0
Software released by ROBOTISApache License 2.0
DocumentationCC BY 4.0

Always check the LICENSE, notices, and third-party license files in each repository before use. Those files are the source of truth and may contain additional terms for dependencies, models, datasets, or other bundled assets.