Skip to main content

Kimodo

Kimodo is NVIDIA Research's kinematic motion diffusion model for generating high-quality 3D human and humanoid robot motion from text prompts and kinematic constraints. It supports natural language prompts, full-body keyframes, sparse joint constraints, end-effector constraints, 2D waypoints, and 2D paths.

For AI Sapiens, use Kimodo as a motion authoring tool. Kimodo generates kinematic motion files; before a motion can run on AI Sapiens, it must be converted or retargeted into the AI Sapiens motion and control pipeline.

info

Kimodo is developed and maintained by NVIDIA Research. Use this guide to install Kimodo, generate source motion, and prepare the output for the AI Sapiens motion workflow. For the latest command options and model list, refer to the official Kimodo documentation and repository.

AI Sapiens Kimodo Demo​

Official Resources​

Kimodo Repository Used in This Guide

The installation commands in this guide use ROBOTIS-GIT/kimodo, forked from nv-tlabs/kimodo. The ROBOTIS fork includes a BVH export fix used in the AI Sapiens motion-retargeting workflow.

Requirements​

Kimodo is primarily tested on Linux. The official documentation lists the following baseline requirements:

  • Python 3.10+
  • PyTorch 2.0+
  • A CUDA®-capable NVIDIA GPU for practical generation speed
  • Hugging Face access token for the text encoder
  • Access to the gated meta-llama/Meta-Llama-3-8B-Instruct model on Hugging Face

Kimodo can run the text encoder on CPU when GPU memory is limited. NVIDIA notes that local GPU generation requires about 17 GB of VRAM when the text encoder also runs on GPU. If the GPU has less memory, run the text encoder on CPU with TEXT_ENCODER_DEVICE=cpu.

Set Up Hugging Face Access​

Kimodo uses a Llama-based text encoder. Before installing or running generation, prepare Hugging Face access:

  1. Request access to meta-llama/Meta-Llama-3-8B-Instruct.
  2. Create a Hugging Face access token from your Hugging Face account settings.
  3. Log in on the machine where Kimodo will run:
pip install --upgrade huggingface_hub
hf auth login

Alternatively, place the token directly at:

~/.cache/huggingface/token

Install Option 1: Docker​

Docker is the recommended setup path for AI Sapiens users because it keeps Kimodo's Python, CUDA, demo, and text-encoder dependencies isolated from the host system.

Clone Kimodo and enter the repository:

git clone https://github.com/ROBOTIS-GIT/kimodo.git
cd kimodo

Clone the modified Viser library inside the Kimodo directory:

git clone https://github.com/nv-tlabs/kimodo-viser.git

Make sure the Hugging Face token exists on the host:

hf auth login

Build and start the demo plus text-encoder service:

docker compose up -d --build

Or build and run services step by step:

docker compose build
docker compose up text-encoder
docker compose up demo

The first run can take several minutes because Docker images, dependencies, and model files are downloaded.

Install Option 2: Package Install​

Use this option when you want to generate motions or run the demo without modifying Kimodo source code and prefer a local Python environment.

Create a Python environment:

conda create -n kimodo python=3.10
conda activate kimodo

Install a PyTorch build that matches your CUDA version. Follow the official PyTorch installation selector for the exact command.

Install Kimodo:

pip install git+https://github.com/ROBOTIS-GIT/kimodo.git

To include the interactive demo dependencies:

pip install "kimodo[all] @ git+https://github.com/ROBOTIS-GIT/kimodo.git"

Install Option 3: Source Install​

Use this option when you plan to inspect, modify, or extend Kimodo.

Clone the repository:

git clone https://github.com/ROBOTIS-GIT/kimodo.git
cd kimodo

Create and activate an environment:

conda create -n kimodo python=3.10
conda activate kimodo

Install a PyTorch build that matches your CUDA version, then install Kimodo in editable mode:

pip install -e .

For the interactive demo, install all extras:

pip install -e ".[all]"

The interactive demo uses NVIDIA's modified Viser fork. For an editable Viser install, clone and install it inside the Kimodo repository:

git clone https://github.com/nv-tlabs/kimodo-viser.git
pip install -e kimodo-viser

Generate Motion from the Command Line​

The main command-line entry point is kimodo_gen.

Generate a simple walking motion:

kimodo_gen "A person walks forward." \
--model Kimodo-SOMA-RP-v1 \
--duration 5.0 \
--output output/walk_forward

Kimodo downloads the selected model automatically the first time it is used.

For repeated generation, start the text encoder once in a separate terminal:

kimodo_textencoder

If your GPU memory is limited, run the text encoder on CPU:

TEXT_ENCODER_DEVICE=cpu kimodo_textencoder

Then run kimodo_gen from another terminal in the same environment.

Docker CLI Usage​

When using Docker, run the same generation command inside the demo container:

docker compose run --rm demo kimodo_gen "A person walks forward." \
--model Kimodo-SOMA-RP-v1 \
--duration 5.0 \
--output output/walk_forward

If the demo container is already running, execute the command inside it:

docker compose exec demo kimodo_gen "A person walks forward." \
--model Kimodo-SOMA-RP-v1 \
--duration 5.0 \
--output output/walk_forward

Generate Multiple Motions​

To generate a sequence of prompts, separate sentences with periods and provide matching durations:

kimodo_gen "A person walks forward. A person turns left and waves." \
--duration "4.0 3.0" \
--output output/walk_turn_wave

Kimodo blends the prompt segments together. Use --num_transition_frames to control the transition length.

Use Constraints​

Kimodo can condition generation with constraint JSON files. Constraints can be saved from the interactive demo or written manually using NVIDIA's constraint format.

Example:

kimodo_gen "A person walks forward and picks something up from the ground." \
--model Kimodo-SOMA-RP-v1 \
--duration 5.0 \
--constraints kimodo/assets/demo/examples/kimodo-soma-rp/03_full_body_keyframes/constraints.json \
--output output/pickup_motion

Launch the Interactive Demo​

The interactive demo provides a browser UI for prompt timelines, constraints, visualization, saving, and loading motions.

Start the demo:

kimodo_demo

Open:

http://localhost:7860

With Docker:

docker compose up demo

To start both the demo and text encoder:

docker compose up

Output Files​

Kimodo's default output is an .npz motion file. When multiple samples are generated, files are saved with suffixes such as _00, _01, and so on.

Common output formats include:

Model typeOutput formatNotes
SOMA.npzContains global joint positions, rotations, contacts, root positions, and heading information.
SOMA.bvhAvailable with the --bvh flag. Use this export for Soma-retargeter.
G1.csvMuJoCo qpos CSV with root pose and G1 joint values.
SMPL-X.npzAMASS-style SMPL-X output.

For AI Sapiens, treat Kimodo output as source motion. Convert or retarget it into the AI Sapiens motion format before attempting to execute it on the robot.

Soma-retargeter Export Setting

When preparing Kimodo output for Soma-retargeter, export the motion as BVH and leave the standard T-pose option unchecked.

Useful CLI Options​

OptionDescription
--modelKimodo model checkpoint to use.
--durationMotion duration in seconds. For multiple prompts, pass space-separated durations in quotes.
--outputOutput file or folder stem.
--num_samplesNumber of motion variations to generate.
--seedSeed for reproducible generation.
--constraintsPath to a constraints JSON file.
--bvhExport BVH alongside NPZ for SOMA models.
--bvh_standard_tposeExport BVH with the standard T-pose rest pose. Do not enable this option when exporting for Soma-retargeter.
--no-postprocessDisable post-processing such as foot-skate cleanup and constraint optimization.

Check all options with:

kimodo_gen --help

AI Sapiens Workflow​

Use the following workflow when preparing Kimodo motion for AI Sapiens:

  1. Generate source motion in Kimodo with a SOMA model, such as Kimodo-SOMA-RP-v1.
  2. Preview the motion in the Kimodo interactive demo.
  3. Export the generated SOMA motion as .bvh with the standard T-pose option unchecked.
  4. Retarget the exported BVH motion data with Soma-retargeter.
  5. Test the motion in simulation before running it on hardware.
  6. Execute on the robot only after confirming joint limits, balance, contacts, and safety behavior.
warning

Do not execute generated Kimodo motion directly on AI Sapiens hardware. Create the motion with a SOMA model, export it, retarget it with Soma-retargeter, and validate the result before running it on the robot.

Attribution and Terms​

This page is an independent integration guide for AI Sapiens based on publicly available Kimodo documentation from NVIDIA.

  • Kimodo software, documentation, and model usage are governed by NVIDIA's official repository, documentation, and license/terms.
  • Use this page as operational guidance, and verify final legal or deployment requirements in official Kimodo sources before production or redistribution.