Skip to main content

GEM-X

GEM-X is a monocular whole-body 3D human motion estimation pipeline originally developed by NVIDIA. It recovers SOMA-format full-body motion (77 joints including body, hands, and face) from a single RGB video, then can retarget the recovered motion to humanoid robots.

For AI Sapiens, use the ROBOTIS-GIT/GEM-X fork. It wires retargeting through ROBOTIS-GIT/soma-retargeter and supports both unitree_g1 and ai_sapiens_k1. GEM-X output still needs conversion and validation in the AI Sapiens motion workflow before hardware execution.

info

Use the ROBOTIS GEM-X fork for AI Sapiens integration. Upstream research and pretrained checkpoints remain from NVIDIA (NVlabs/GEM-X, Hugging Face). Prefer ROBOTIS docs and install steps below for the latest fork-specific options.

AI Sapiens GEM-X Demo​

Resources​

What GEM-X Does​

  • Recovers full-body SOMA motion from monocular video.
  • Produces 77-joint 2D keypoints and 3D pose outputs.
  • Recovers global/world motion trajectory from dynamic camera video.
  • Optionally retargets recovered human motion to unitree_g1 or ai_sapiens_k1 through ROBOTIS soma-retargeter.

Requirements​

Linux setup baseline for the ROBOTIS fork:

  • Python 3.12+
  • CUDA-compatible NVIDIA GPU (recommended for full pipeline speed)
  • CUDA-compatible PyTorch build (cu129 recommended for RTX 50-series / Blackwell; cu126 also works on older GPUs)
  • git-lfs for SOMA assets
  • uv package manager

macOS Apple Silicon is supported through ONNX Runtime acceleration for demo usage. For full details, use the macOS installation guide in the ROBOTIS repository.

Install on Linux​

Clone the ROBOTIS GEM-X fork with submodules:

git clone --recursive https://github.com/ROBOTIS-GIT/GEM-X.git
cd GEM-X

If the repo was cloned without submodules:

git submodule update --init --recursive

Create and activate virtual environment:

pip install uv
uv venv .venv --python 3.12
source .venv/bin/activate

Install PyTorch matching your CUDA stack:

# Recommended for RTX 50-series / Blackwell
uv pip install torch torchvision --index-url https://download.pytorch.org/whl/cu129

# Or CUDA 12.6 on older GPUs
# uv pip install torch torchvision --index-url https://download.pytorch.org/whl/cu126

Install SOMA body model and pull LFS assets:

uv pip install -e third_party/soma
cd third_party/soma && git lfs pull && cd ../..

Install GEM and dependencies:

bash scripts/install_env.sh

Optional: install soma-retargeter for --retarget mode:

uv pip install -e third_party/soma-retargeter

Download Pretrained Model​

GEM-X can auto-download checkpoints when needed, or you can download manually:

huggingface-cli download nvidia/GEM-X gem_soma.ckpt --local-dir inputs/pretrained

Expected checkpoint path:

inputs/pretrained/gem_soma.ckpt

Run Full 3D Inference​

Run the standard pipeline:

python scripts/demo/demo_soma.py \
--video path/to/video.mp4 \
--output_root outputs \
--ckpt inputs/pretrained/gem_soma.ckpt

If --ckpt is omitted, GEM-X attempts automatic download from Hugging Face.

Useful Flags​

OptionDescription
--videoInput video path (required).
--ckptGEM pretrained checkpoint path.
--output_rootOutput root directory.
--static_camTreat camera as static (disables VO).
--verboseSave debug overlays and intermediate views.
--retargetRetarget recovered motion (requires ROBOTIS soma-retargeter).
--robotunitree_g1 (default) or ai_sapiens_k1.

Run ONNX-Accelerated Demo​

Use ONNX/TensorRT-capable path:

python scripts/demo/demo_soma_onnx.py \
--video path/to/video.mp4

This path can also run well on Apple Silicon with ONNX Runtime and CoreML (see the macOS guide in the ROBOTIS repository).

Run 2D Keypoint-Only Demo​

If you only need tracked SOMA 77-joint keypoints:

python scripts/demo/demo_2d_keypoints.py \
--video path/to/video.mp4

Output Files​

For demo_soma.py, GEM-X writes outputs under:

<output_root>/<video_name>/

Common outputs:

  • 0_kp2d77_overlay.mp4: 2D keypoint overlay
  • <video_name>_1_incam.mp4: in-camera mesh render
  • <video_name>_2_global.mp4: world/global render
  • <video_name>_3_incam_global_horiz.mp4: combined preview
  • preprocess/bbx.pt: tracked person bounding boxes
  • preprocess/vitpose.pt: 77-joint 2D keypoints
  • preprocess/hpe_results.pt: estimated 3D motion results

With --retarget enabled, additional outputs include:

--robotCSVPreview video
unitree_g1 (default)<video_name>_retarget_unitree_g1.csv<video_name>_4_unitree_g1_retarget.mp4
ai_sapiens_k1<video_name>_retarget_ai_sapiens_k1.csv<video_name>_4_ai_sapiens_k1_retarget.mp4

Also exported: matching .bvh next to the CSV stem.

Humanoid Retargeting (--retarget)​

GEM-X uses ROBOTIS-GIT/soma-retargeter for optional humanoid retargeting.

Supported robots:

  • unitree_g1 — Unitree G1 (29 DOF CSV)
  • ai_sapiens_k1 — AI Sapiens K1 / ai_sapiens target (23 DOF CSV)

Examples:

# Unitree G1
python scripts/demo/demo_soma.py --video path/to/video.mp4 --retarget --robot unitree_g1

# AI Sapiens K1
python scripts/demo/demo_soma.py --video path/to/video.mp4 --retarget --robot ai_sapiens_k1

Install retargeter deps once:

uv pip install -e third_party/soma-retargeter
# For K1, also ensure the AI Sapiens submodule/assets are present:
# git -C third_party/soma-retargeter submodule update --init --recursive
python third_party/soma-retargeter/tools/generate_ai_sapiens_retarget_mjcf.py --check

AI Sapiens Workflow​

Use the following workflow when preparing GEM-X motion for AI Sapiens:

  1. Prepare and clean monocular source video.
  2. Run GEM-X (demo_soma.py or demo_soma_onnx.py) to recover SOMA motion.
  3. Inspect outputs, especially 2D keypoint quality and global trajectory stability.
  4. Retarget with --retarget --robot ai_sapiens_k1, or convert exported BVH through Soma-retargeter.
  5. Convert the soma-retargeter CSV to Cyclo Lab motion NPZ/CSV with scripts/tools/motion/soma_retargeter_csv_converter.py, then validate with replay_csv.py (see Mimic).
  6. Validate in simulation before hardware execution.
  7. Execute on robot only after confirming limits, contacts, and stability.
warning

Do not run recovered motion on AI Sapiens hardware without retargeting and validation. Always test in simulation first and confirm safety constraints before real-robot execution.

Troubleshooting​

Common fixes:

  • git lfs pointer files instead of assets: run cd third_party/soma && git lfs pull.
  • CUDA/PyTorch mismatch: install the PyTorch build matching nvidia-smi driver capability (cu129 for RTX 50-series).
  • ModuleNotFoundError: gem: activate venv and rerun bash scripts/install_env.sh.
  • OpenGL/EGL rendering issues: set PYOPENGL_PLATFORM=egl and EGL_PLATFORM=surfaceless.
  • Empty third_party/soma-retargeter: run git submodule update --init --recursive third_party/soma-retargeter.

Notes on Training​

NVIDIA's upstream training recipe in GEM-X uses internal data (Bones RigPlay-1) and is not fully reproducible with public data only. Most AI Sapiens users should focus on inference and retargeting workflows unless they have appropriate dataset access.

Attribution and Terms​

This page is an AI Sapiens integration guide for the ROBOTIS-GIT/GEM-X fork, based on NVIDIA's publicly available GEM-X release.

  • The ROBOTIS fork builds on NVIDIA GEM-X (NVlabs/GEM-X).
  • GEM-X source code is released under Apache 2.0.
  • GEM-X model artifacts and checkpoints are governed by NVIDIA model terms on Hugging Face and the upstream release pages.
  • Verify the latest license and model terms before production deployment, redistribution, or commercial release.