Task Python API
pycm Module
Here we introduce two ways to use pycm module.
import pycm # pycm should NOT be omitted in the following code
pycm.led.on(pycm.const.RED)
from pycm import * # pycm should be omitted in the following code
led.on(const.RED)
We assume the SECOND case in the following description.
| Methods | Description | Parameter | Return | Example |
|---|---|---|---|---|
console(ch: int) -> None | Configure controller's communication channel | BLE (0)<br>UART (1)<br>USB (2) | None | console(BLE) |
delay(ms: int) -> None | Delay in milliseconds | 0 ~ 4,294,967,295 | None | delay(1000) |
millis() -> None | Milliseconds since controller turns on | None | 0 ~ 4294967295 | pre_time = millis() |
micros() -> None | Microseconds since controller turns on | None | 0 ~ 4294967295 | pre_time = micros() |
Submodules of pycm
| Submodules of pycm | Description |
|---|---|
| const | Constant values |
| led | LED control |
| info | Controller's information |
| eeprom | Controller's parameters stored in EEPROM area |
| rc | Remote control |
| etc | Miscellaneous functions |
| timer | Timer functions |
| button | Buttons |
| dxlbus | Batch controlling Dynamixel actuators |
| motion | Motion control |
| buzzer | Buzzer |
| mic | Microphone |
| imu | IMU(Inertial Measurement Unit) |
| OLLO | 5-pin port extension interface |
| DXL | Dynamixel actuator |
| rpi | Raspberry Pi interface |
Const Submodule
| Constant members of const | Description | Example |
|---|---|---|
| RED | Red color constant for controller's RGB LED | led.on(const.RED) |
| GREEN | Green color constant for controller's RGB LED | led.on(const.GREEN) |
| BLUE | Blue color constant for controller's RGB LED | led.on(const.BLUE) |
| ALL | White color constant for controller's RGB LED | led.on(const.ALL) |
| OLLO_WHEEL_SPEED | Use 5-pin servo motor in wheel mode | wheel = OLLO(1, const.OLLO_WHEEL_SPEED) |
| OLLO_JOINT_POSITION | Use 5-pin servo motor in joint mode and control its position | joint = OLLO(1, const.OLLO_JOINT_POSITION) |
| OLLO_JOINT_SPEED | Use 5-pin servo motor in joint mode and control its speed | speed = OLLO(1, const.OLLO_JOINT_SPEED) |
| OLLO_IR | IR sensor 5-pin device | ir = OLLO(1, const.OLLO_IR) |
| OLLO_DMS | DMS sensor 5-pin device | dms = OLLO(1, const.OLLO_DMS) |
| OLLO_TOUCH | Touch sensor 5-pin device | touch = OLLO(1, const.OLLO_TOUCH) |
| OLLO_LED | LED module 5-pin device | led = OLLO(1, const.OLLO_LED) |
| OLLO_USER | 5-pin user device | user = OLLO(1, const.OLLO_USER) |
| OLLO_TEMPERATURE | Temperature sensor 5-pin device | temperature = OLLO(1, const.OLLO_TEMPERATURE) |
| OLLO_MAGNET | Magnet sensor 5-pin device | magnet = OLLO(1, const.OLLO_MAGNET) |
| OLLO_MOTION_DETECTION | Motion detecting sensor 5-pin device | motion_detection = OLLO(1, const.OLLO_MOTION_DETECTION) |
| OLLO_COLOR | Color sensor 5-pin device | color = OLLO(1, const.OLLO_COLOR) |
| OLLO_MOISTURE | Moisture value of Moisture-Temperature sensor 5-pin device | moisture = OLLO(1, const.OLLO_MOISTURE) |
| OLLO_MOISTURE_TEMP | Temperature value of Moisture-Temperature sensor 5-pin device | temperature = OLLO(1, const.OLLO_MOISTURE_TEMP) |
| OLLO_BRIGHTNESS | Brightness sensor 5-pin device | brightness = OLLO(1, const.OLLO_BRIGHTNESS) |
| OLLO_RED_BRIGHTNESS | Brightness of red LED of Red-Blue LED | red = OLLO(1, const.OLLO_RED_BRIGHTNESS) |
| OLLO_BLUE_BRIGHTNESS | Brightness of blue LED of Red-Blue LED | blue = OLLO(1, const.OLLO_BLUE_BRIGHTNESS) |
| V | Vertical mode | imu.imu_type(const.V) |
| H | Horizontal mode | imu.imu_type(const.H) |
| JOINT | Joint mode of Dynamixel actuator | DXL(2).mode(const.JOINT) |
| WHEEL | Wheel mode of Dynamixel actuator | DXL(3).mode(const.WHEEL) |
Led Submodule
| Methods | Description | Parameter | Return | Example |
|---|---|---|---|---|
on(color: int) -> None | Turn on specified color of controller's LED | color: LED name<br>- const.RED / const.BLUE / const.GREEN | None | led.on(const.RED) |
off(color: int) -> None | Turn off specified color of controller's LED | color: LED name<br>- const.RED / const.BLUE / const.GREEN | None | led.off(const.RED | const.GREEN) |
set(color: int) -> None | Set controller's LED as specified color | color: LED name<br>- const.RED / const.BLUE / const.GREEN | None | led.set(const.BLUE) |
toggle(color: int) -> None | Toggle specified color of controller's LED | color: LED name<br>- const.RED / const.BLUE / const.GREEN | None | led.toggle(const.GREEN | const.BLUE) |
Info Submodule
| Methods of info submobule | Description | Example |
|---|---|---|
model_number() -> int | Return controller's model number (450) | info.model_number() |
fw_version() -> int | Return controller's firmware version | info.fw_version() |
id() -> int | Return controller's id (200) | info.id() |
boot_version() -> int | Return controller's bootloader version | info.boot_version() |
voltage() -> int | Return controller's voltage (unit: 0.1V) | info.voltage() |
temperature() -> int | Return controller's temperature (unit: °C) | info.temperature() |
address() -> str | Return controller's BLE MAC address as string | info.address() |
EEPROM Submodule
| Methods of eeprom submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
dxl_baud() -> int | Return controller's dynamixel bus baudrate | None | 0 : 9600bps<br>1 : 57600bps<br>2 : 115200bps<br>3 : 1000000bps<br>4 : 2000000bps<br>5 : 3000000bps<br>6 : 4000000bps<br>7 : 4500000bps | eeprom.dxl_baud() |
dxl_baud(baud: int) -> None | Set controller's dynamixel bus baudrate | 0 : 9600bps<br>1 : 57600bps<br>2 : 115200bps<br>3 : 1000000bps<br>4 : 2000000bps<br>5 : 3000000bps<br>6 : 4000000bps<br>7 : 4500000bps | None | eeprom.dxl_baud(3) |
uart_baud() -> int | Return controller's uart port baudrate | None | 0 : 9600bps<br>1 : 57600bps<br>2 : 115200bps<br>3 : 1000000bps<br>4 : 2000000bps<br>5 : 3000000bps<br>6 : 4000000bps<br>7 : 4500000bps | eeprom.uart_baud() |
uart_baud(baud: int) -> None | Set controller's uart port baudrate | 0 : 9600bps<br>1 : 57600bps<br>2 : 115200bps<br>3 : 1000000bps<br>4 : 2000000bps<br>5 : 3000000bps<br>6 : 4000000bps<br>7 : 4500000bps | None | eeprom.uart_baud(1) |
imu_type() -> int | Return controller's imu direction type | None | 0 : VERTICAL<br>1 : HORIZONTAL | eeprom.imu_type() |
imu_type(type:int) -> None | Set controller's imu direction type | const.V<br>const.H | None | eeprom.imu_type(const.V) |
RC Submodule
| Methods of rc submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
port(ch: int) -> None | Set controller's remote control channel | BLE (0)<br>UART (1)<br>USB (2) | None | rc.port(BLE) |
received() -> bool | Return if reveived a new remote control packet | None | True : new packet arrived<br>False : new packet not arrived | rc.received() |
read() -> int | Return last received remote control packet value | None | 0 ~ 65535 | rc.read() |
write(data: int) -> None | Send remote control packet value | 0 ~ 65535 | None | rc.write(128) |
Etc Submodule
| Methods of etc submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
print_screen(val: int) -> None | Print an integer value to task monitor with a space | -2,147,483,647 ~ 2,147,483,647 | None | etc.print_screen(100) |
println_screen(val: int) -> None | Print an integer value to task monitor with a new line | -2,147,483,647 ~ 2,147,483,647 | None | etc.println_screen(100) |
print_string(str: str) -> None | Print a string to task monitor with a space | max 19 bytes | None | etc.print_string("Hello world!") |
println_string(str: str) -> None | Print a string to task monitor with a new line | max 19 bytes | None | etc.println_string("Hello world!") |
port(ch: int) -> None | Set controller's print screen channel | BLE (0)<br>UART (1)<br>USB (2) | None | etc.port(BLE) |
Timer Submodule
| Methods of etc submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
init(ms: int, func: function) -> None | Register a callback function which will be called periodically<br>Only one function can be registered | ms<br>function calling period in millisecond<br>func<br>function to be called | None | timer.init(1000, func) |
start() -> None | Start the registered function callback process | None | None | timer.start() |
stop() -> None | stop the registered function callback process | None | None | timer.stop() |
Button Submodule
| Methods of button submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
pressed() -> bool | Return if controller's user button is pressed | None | True : pressed<br>False : not pressed | button.pressed() |
released() -> bool | Return if controller's user button is released after pressed | None | True : release event happened<br>False : release event not happened | button.released() |
millis() -> int | Return last pressed time in milliseconds | None | 0 ~ 65535 | button.millis() |
seconds() -> int | Return last pressed time in seconds | None | 0 ~ 255 | button.seconds() |
Dxlbus Submodule
| Methods of dxlbus submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
power_on() -> None | Turn on power for dynamixel bus | None | None | dxlbus.power_on() |
power_off() -> None | Turn off power for dynamixel bus | None | None | dxlbus.power_off() |
scan() -> int | Scan dynamixels, return the number of dynamixels found | None | 0 ~ 253 | dxlbus.scan() |
count() -> int | Return the number of found dynamixel(s) | None | 0 ~ 253 | dxlbus.count() |
torque_on() -> None | Turn on torque for all found dynamixel(s) | None | None | dxlbus.torque_on() |
torque_off() -> None | Turn off torque for all found dynamixel(s) | None | None | dxlbus.torque_off() |
reboot() -> None | Reboot all dynamixel(s) | None | None | dxlbus.reboot() |
Motion Submodule
| Methods of motion submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
speed() -> int | Return motion speed (%) | None | 20% ~ 200% | motion.speed() |
speed(speed: int) -> int | Set motion speed (%) | 20% ~ 200% | None | motion.speed(150) |
play(motion: int) -> None | Play a specified motion page or stop current motion | 0 : Stop motion using an Exit Motion Unit<br>1 ~ 65532 : Play motion with a specified page<br>65533 : Stop motion immediately<br>65534 : Stop motion at the current Key Frame<br>65535 : Stop motion at current unit | None | motion.play(1) |
play(motion: int, next: int) -> None | Play a specified motion with a motion reserved for playing contiguously | motion<br>0 : Stop motion using an Exit Motion Unit<br>1 ~ 65532 : Play motion with a specified page<br>65533 : Stop motion immediately<br>65534 : Stop motion at the current Key Frame<br>65535 : Stop motion at current unit<br><br>next<br>0 ~ 65534 : Page to move next.<br>65535 : No next page | None | motion.play(1, 2) |
next(next: int) -> None | Reserve the next motion to play contiguously. This function must be used before motion.play(motion) | next<br>0 ~ 65534 : Page to move next.<br>65535 : No next page | None | motion.next(2) |
status() -> bool | Return motion play status | None | True : Motion is being played<br>False : Motion is NOT being played | motion.status() |
count() -> int | Return the number of motions stored in FLASH memory | None | 0 ~ 1023 | motion.count() |
wait() -> None | Wait until current motion stops playing | None | None | motion.wait() |
Buzzer Submodule
| Methods of buzzer submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
melody(index) -> None | Play the specified melody by index. | 0 ~ 25 | None | buzzer.melody(1) |
note(index) -> None | Play the specified note by index for 0.3 sec | 0 ~ 51 | None | buzzer.note(1) |
note(index, ms) -> None | Play the specified note by index for specified time length | index<br> 0 ~ 51<br>ms(unit: 0.1s)<br>0 ~ 50 : 0 ~ 5.0s | buzzer.note(1, 10) | |
wait() -> None | Wait until current melody or note ends | None | None | buzzer.wait() |
Mic Submodule
| Methods of mic submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
counted() -> int | Return the final number of detected sound after the clapping finishes | None | 0 ~ 255 | mic.counted() |
counting() -> int | Return the real-time number of detected sound while the clapping continues | None | 0 ~ 255 | mic.counting() |
clear() -> int | Clear the final number of detected sound to zero | None | None | mic.clear() |
IMU Submodule
| Methods of imu submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
roll() -> int | Return the roll value of CM-550 controller | None | -18000 ~ 18000 | imu.roll() |
pitch() -> int | Return the pitch value of CM-550 controller | None | -9000 ~ 9000 | imu.pitch() |
yaw() -> int | Return the yaw value of CM-550 controller | None | -9000 ~ 9000 | imu.yaw() |
gyro_x() -> int | Return the Gyro X axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01degree/sec) | imu.gyro_x() |
gyro_y() -> int | Return the Gyro Y axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01degree/sec) | imu.gyro_y() |
gyro_z() -> int | Return the Gyro Z axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01degree/sec) | imu.gyro_z() |
accel_x() -> int | Return the accelerometer X axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01G) | imu.accel_x() |
accel_y() -> int | Return the accelerometer Y axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01G) | imu.accel_y() |
accel_z() -> int | Return the accelerometer Z axis value of CM-550 controller | None | -32768 ~ 32767 (unit: 0.01G) | imu.accel_z() |
OLLO Submodule
| Methods of OLLO submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
OLLO(port, mode) -> object | Create an object with Port Number and Device Mode | mode<br> const.OLLO_WHEEL_SPEED (port: 1 ~ 2)<br>const.OLLO_JOINT_POSITION (port: 1 ~ 2)<br>const.OLLO_JOINT_SPEED (port: 1 ~ 2)<br>const.OLLO_IR (port: 1 ~ 2)<br>const.OLLO_MOISTURE (port: 1 ~ 2)<br>const.OLLO_MOISTURE_TEMP (port: 1 ~ 2)<br>const.OLLO_RED_BRIGHTNESS (port: 1 ~ 2)<br>const.OLLO_BLUE_BRIGHTNESS (port: 1 ~ 2)<br>const.OLLO_DMS (port: 1 ~ 5)<br>const.OLLO_TOUCH (port: 1 ~ 5)<br>const.OLLO_LED (port: 1 ~ 5)<br>const.OLLO_USER (port: 1 ~ 5)<br>const.OLLO_TEMPERATURE (port: 1 ~ 5)<br>const.OLLO_MAGNET (port: 1 ~ 5)<br>const.OLLO_MOTION_DETECTION (port: 1 ~ 5)<br>const.OLLO_COLOR (port: 1 ~ 5)<br>const.OLLO_BRIGHTNESS (port: 1 ~ 5)<br> | 5-pin port object | obj = OLLO(1, OLLO_WHEEL_SPEED) |
read() -> int | Return the value of object | None | 0 ~ 2047 (mode: const.OLLO_WHEEL_SPEED)<br>0 ~ 1023 (mode: const.OLLO_JOINT_POSITION)<br>0 ~ 1023 (mode: const.OLLO_JOINT_SPEED)<br>0 ~ 1023 (mode: const.OLLO_IR)<br>0 ~ 100 (mode: const.OLLO_MOISTURE, unit: %)<br>-19 ~ 105 (mode: const.OLLO_MOISTURE_TEMP, unit: ℃)<br>0 ~ 100 (mode: const.OLLO_RED_BRIGHTNESS, unit: %)<br>0 ~ 100 (mode: const.OLLO_BLUE_BRIGHTNESS, unit: %)<br>0 ~ 1023 (mode: const.OLLO_DMS)<br>0, 1 (mode: const.OLLO_TOUCH)<br>0 ~ 3 (mode: const.OLLO_LED)<br>0 ~ 1023 (mode: const.OLLO_USER)<br>-20 ~ 120 (mode: const.OLLO_TEMPERATURE, unit: ℃)<br>0, 1 (mode: const.OLLO_MAGNET)<br>0 ~ 1 (mode: const.OLLO_MOTION_DETECTION)<br>0 ~ 6 (mode: const.OLLO_COLOR)<br>0 ~ 100 (mode: const.OLLO_BRIGHTNESS, unit: %)<br> | obj.read() |
write(speed) -> None | Set wheel speed of object of wheel mode<br>(mode: const.OLLO_WHEEL_SPEED) | 0 ~ 1023 : CCW (Counter clock wise) speed<br>1024 ~ 2047 : CW (Clockwise) speed | None | obj.write(512) |
write(position) -> None | Set joint position of object of joint mode<br>(mode: const.OLLO_JOINT_POSITION) | 0 ~ 1023 | None | obj.write(512) |
write(speed) -> None | Set moving speed of object of joint mode<br>(mode: const.OLLO_JOINT_POSITION) | 0 ~ 1023 | None | obj.write(256) |
write(pwm) -> None | Set pwm duty cycle of object of LED brightness mode<br>(mode: const.OLLO_RED_BRIGHTNESS / OLLO_BLUE_BRIGHTNESS) | 0 ~ 100 (unit: %) | None | obj.write(50) |
write(left, right) -> None | Set LED status of left and right LED of LED module<br>(mode: const.OLLO_LED) | 0, 1 | None | obj.write(1, 0) |
write(left, right) -> None | Set LED status of left and right output port of User Device<br>(mode: const.OLLO_USER) | 0, 1 | None | obj.write(1, 1) |
DXL Submodule
| Methods of DXL submobule | Description | Parameter | Return | Example |
|---|---|---|---|---|
DXL(id) -> object | Create an Dynamixel object with specified ID | 0 ~ 252 : Single ID<br>254 : Broadcast ID | Dynamixel object | obj = DXL(1) |
mode() -> int | Return mode number of Dynamixel object | None | 1 : Velocity Control Mode<br>3 : Position Control Mode<br>4 : Multi-turn Mode<br> | obj.mode() |
mode(mode) -> None | Set mode for Dynamixel object | 1 : Velocity Control Mode<br>3 : Position Control Mode<br>4 : Multi-turn Mode<br> | None | obj.mode(3) |
torque_on() -> None | Turn on torque for Dynamixel object | None | None | obj.torque_on() |
torque_off() -> None | Turn off torque for Dynamixel object | None | None | obj.torque_off() |
led_on() -> None | Turn on LED for Dynamixel object | None | None | obj.led_on() |
led_off() -> None | Turn off LED for Dynamixel object | None | None | obj.led_off() |
led_toggle() -> None | Toggle LED for Dynamixel object | None | None | obj.led_toggle() |
goal_velocity() -> int | Return goal velocity value | None | -1023 ~ 1023 (unit: 0.229 rev/min) | obj.goal_velocity() |
goal_velocity(v) -> None | Set goal velocity value | -1023 ~ 1023 (unit: 0.229 rev/min) | None | obj.goal_velocity(100) |
goal_position() -> int | Return goal position value | None | -4095 ~ 4095 | obj.goal_position() |
goal_position(p) -> None | Set goal position value | -4095 ~ 4095 | None | obj.goal_position(1024) |
is_moving() -> bool | Return moving status | None | True : Dynamixel is moving<br>False : Dynamixel is not moving | obj.is_moving() |
present_velocity() -> int | Return present velocity value | None | -1023 ~ 1023 (unit: 0.229 rev/min) | obj.present_velocity() |
present_position() -> int | Return present position value | None | -4095 ~ 4095 | obj.present_position() |
RPI Submodule
| Methods of rpi submodule | Description | Parameter | Return | Example |
|---|---|---|---|---|
mode() -> int | Return mode number of connected Raspberry Pi | None | 0 : Standby<br>1 : Color Detection<br>2 : Face Detection<br>3 : Streaming | rpi.mode() |
mode(mode: int) -> None | Set the mode of the connected Raspberry Pi | mode<br>0 : Standby<br>1 : Color Detection<br>2 : Face Detection<br>3 : Streaming | None | rpi.mode(1) |
sub_mode() -> int | Return the sub-mode of the current mode<br>(only for Color Detection Mode) | None | 1 : Red<br>2 : Orange<br>3 : Yellow<br>4 : Green<br>5 : Blue<br>6 : Purple<br>7 : White | rpi.sub_mode() |
sub_mode(mode: int) -> None | Set the sub-mode of the current mode<br>(only for Color Detection Mode) | mode<br>1 : Red<br>2 : Orange<br>3 : Yellow<br>4 : Green<br>5 : Blue<br>6 : Purple<br>7 : White | None | rpi.sub_mode(1) |
ip() -> tuple | Return the IP address of the connected Raspberry Pi as a tuple with 4 integers | None | IP address as a tuple<br>eg. (192, 168, 13, 5) | rpi.ip() |
position_x() -> int | Return the x-coordinate of the camera detection position | None | X-coordinate value | rpi.position_x() |
position_y() -> int | Return the y-coordinate of the camera detection position | None | Y-coordinate value | rpi.position_y() |
area() -> int | Return the detection area of the camera | None | Area value | rpi.area() |
resolution_w() -> int | Return the width of the camera resolution | None | Width in pixels | rpi.resolution_w() |
resolution_h() -> int | Return the height of the camera resolution | None | Height in pixels | rpi.resolution_h() |
h_max() -> int | Return the maximum hue value for color detection | None | 0 ~ 179 | rpi.h_max() |
h_max(h_max: int) -> None | Set the maximum hue value for color detection | 0 ~ 179 | None | rpi.h_max(179) |
h_min() -> int | Return the minimum hue value for color detection | None | 0 ~ 179 | rpi.h_min() |
h_min(h_min: int) -> None | Set the minimum hue value for color detection | 0 ~ 179 | None | rpi.h_min(0) |
s_max() -> int | Return the maximum saturation value for color detection | None | 0 ~ 255 | rpi.s_max() |
s_max(s_max: int) -> None | Set the maximum saturation value for color detection | 0 ~ 255 | None | rpi.s_max(255) |
s_min() -> int | Return the minimum saturation value for color detection | None | 0 ~ 255 | rpi.s_min() |
s_min(s_min: int) -> None | Set the minimum saturation value for color detection | 0 ~ 255 | None | rpi.s_min(0) |
v_max() -> int | Return the maximum value (brightness) for color detection | None | 0 ~ 255 | rpi.v_max() |
v_max(v_max: int) -> None | Set the maximum value (brightness) for color detection | 0 ~ 255 | None | rpi.v_max(255) |
v_min() -> int | Return the minimum value (brightness) for color detection | None | 0 ~ 255 | rpi.v_min() |
v_min(v_min: int) -> None | Set the minimum value (brightness) for color detection | 0 ~ 255 | None | rpi.v_min(0) |