Basic Usage
Convenience Features and Precautions
Mastering these CLI-specific features can significantly increase your workflow speed.
:::tip Productivity features
- Command Auto-completion: Press the Tab key after typing part of a command to complete it.
- Item Name Auto-completion: Long names like
Torque EnableandGoal Positioncan be completed via the Tab key. - Keyword Search: Enter a partial name (e.g.,
present) to see a list of matching control table items. - Command History: Use the arrow keys (
↑,↓) to recall previous commands. - ID Memory: Once an ID is specified, subsequent commands can omit the ID and will target the last accessed device.
- Omitting
set: You can enter an item name alone to enter control mode without typingseteach time.
:::
:::warning Precautions
- Firmware Management: Disconnecting power or cables during an
updatemay cause device failure. - Reconnect after a Factory Reset: A Protocol 1.0
resetalso restores the ID and baud rate defaults. Reopen the port with the changed settings and scan for the device again. - Port Occupancy: The
opencommand fails if another program (such as the DYNAMIXEL Wizard 2.0 GUI) is using the same serial port. Make sure only one process uses the port at a time.
:::
Quick Examples
Examples based on a typical CLI workflow.
Connection and Scan
List serial ports with port
>>> port
Available ports:
1. COM3 (USB Serial Device)
2. COM4 (USB Serial Port)
Open a serial port with open
>>> open COM3 57600
[Success] Port opened successfully
Scan DYNAMIXELs with scan
COM3, 57600bps > scan
broadcast ping : please wait...
Press Ctrl+C to cancel
[ID:001] XL330-M288, v53
[ID:004] XL330-M077, v53
broadcast ping : done
COM3, 57600bps >
Checking DYNAMIXEL Status
Check the current status with status
COM3, 57600bps > status 1
[ID:001] XL330-M288, v53
--------------------------------------------------
Operating Mode : Position control
Torque : OFF
LED : OFF
Hardware Error :
--------------------------------------------------
Position : 180.35 [°]
Velocity : 0.23 [rev/min]
Current : 0.00 [mA]
Voltage : 4.50 [V]
Temperature : 23 [°C]
COM3, 57600bps >
View the control table with table
COM3, 57600bps > table 1
[ID:001] XL330-M288, v53
0 : Model Number : 1200 : 0x04B0 : XL330-M288
2 : Model Information : 0 : 0x00000000 :
6 : Firmware Version : 53 : 0x35 :
7 : ID : 1 : 0x01 : ID 1
8 : Baud Rate (Bus) : 1 : 0x01 : 57600 bps
...
COM3, 57600bps >
Position Control and Monitoring
Enable torque for ID 1
COM3, 57600bps > set 1 Torque Enable 1
[ID:001] XL330-M288, v53
[INFO] Setting Torque Enable to 1
[ID:001] XL330-M288, v53
[Success] write Torque Enable 1 OK
Move to goal position 2048
COM3, 57600bps > set 1 Goal Position 2048
[ID:001] XL330-M288, v53
[INFO] Setting Goal Position to 2048
[ID:001] XL330-M288, v53
[Success] write Goal Position 2048 OK
Monitor the present position in real time (Ctrl+C to stop)
COM3, 57600bps > get 1 Present Position -c
[ID:001] XL330-M288, v53
Press Ctrl+C to stop continuous reading...
132 : Present Position : 2052 : 0x00000804 : 180.35 [°]
[INFO] KeyboardInterrupt
COM3, 57600bps >
Help
Use the help command to list all commands, or type help [command] for detailed usage and examples.
List all commands with help
>>> help
Available commands:
port - Prints a list of available serial ports on the system.
open - Open serial port.
close - Close serial port.
exit - Quit the program.
ping - Check the existence of a Device and basic information.
scan - Search connected DYNAMIXELs.
timeout - Set additional time for Timeout.
protocol - Set DYNAMIXEL protocol version.
table - Print the Control Table.
get - Get a value from Control Table.
set - Set a value on the Control Table.
status - Show DYNAMIXEL status summary.
reset - Reset the Control Table to its initial factory default settings.
reboot - Reboot the DYNAMIXEL.
clear - Initialize supported DYNAMIXEL state.
update - Update the DYNAMIXEL.
upgrade - Update DYNAMIXEL Wizard CLI to the latest version.
license - Display software and third-party license information.
copyright - Display copyright and third-party software notices.
Type "help [command]" for more information.
>>>
View get usage and examples with help get
COM3, 57600bps > help get
get : Get a value from Control Table.
use) get [id] <item name> [-c]
[id] : optional - Device ID (uses last ID if omitted)
<item name> : required - Control table item name
[-c] : optional - Continuous mode (updates value continuously)
ex1) get 1 Torque Enable
ex2) get Present Position
ex3) get 1 Present Position -c (continuous mode)
ex4) get -c Present Position (continuous mode with last ID)
<info> Do not need to enter full name.
1) Type "get 1 present".
2) It will be shown a list of readable items.
COM3, 57600bps >