For C# source code is only provided for Windows.
Compiler and Builder
Function References
-
The function reference file is located in
[DynamixelSDK folder]/c#/dynamixel_functions_csharp/[winXX]/dynamixel.cs
Building and Running the Sample Code
The DYNAMIXEL SDK sample code for C# uses the library files (.dll for Windows) compiled from the C# language source.
Each released DYNAMIXEL SDK has the latest library files in:
[DynamixelSDK folder]/c/build/[winXX]/output/dxl_xYY_c.dll
built by their own source code.
-
Open
read_write.slnfrom[DynamixelSDK folder]/C#/protocol2.0/read_write/win64/ -
Double click
ReadWrite.cs
-
Adjust the values surrounded with red circle to proper value as shown in the comment. Then click
Startin the Visual Studio toolbox above.
-
Console window will show the results