Skip to main content

This section provides instructions on how to configure the device.

Requirements

NOTE : The Quick Start Guide explains how to use DYNAMIXEL with a PC as the controller. Instead of a PC, controllers such as OpenCR, OpenRB, or Arduino can also be used.

In order to use DYNAMIXEL with a PC, you need a U2D2 to convert USB signals to TTL or RS-485.
The U2D2 does not supply power to the DYNAMIXEL, so a U2D2 Power Hub Board is also required to provide power.

info

USB2DYNAMIXEL Driver Installation

NOTE : Recent Linux include the kernel which contains the FT232RL driver for the FTDI driver used by the U2D2. Most Linux users won't need to install the driver manually.

Windows users need to install the FTDI driver to enable USB-to-serial communication.
Install the latest VCP driver from the FTDI Driver Download page.

Connecting The Motor

Please use an SMPS that matches the operating voltage of the motor you are using.

  • 12V for X Series (also for AX, EX, RX, and MX series)
  • 24V for P and Y series

How to connect the motor

Connect as shown below.
You can either daisy-chain the U2D2 and Power Hub Board (PHB) to the motor, or connect them separately.

You can connect multiple DYNAMIXELs in a daisy-chain configuration as shown below.

info

NOTE : You should match the port according to whether your DYNAMIXEL supports TTL or RS-485.
TTL: TTL-based DYNAMIXEL's have 3 pin connectors
RS-485: RS-485-based DYNAMIXEL's have 4 pin connectors.

Verifying Connection

Once all the above settings are complete, you can use the Dynamixel Wizard 2.0 to ensure the connection is working properly

danger

DON'T SKIP THIS STEP!
For checking and setting Motor ID, this process is essential.

  1. Install Dynamixel Wizard 2.0
  2. Scan the motor and Operate it
  3. Check and set the motor ID
  4. If the firmware is outdated, update it.