Skip to main content

This section provides examples of how to write code in C++ to read and write data to DYNAMIXEL motors.

warning

NOTE: This tutorial is based on XL-430-W250 DYNAMIXEL motors and uses Protocol 2.0.

Make cpp file

  • Create a CPP file and open it in a text editor. In this case, we use visual studio code, but you can use any text editor you prefer.
$ mkdir -p my_dxl_project/src
$ cd my_dxl_project/src
$ code my_read_write.cpp

Source Code Description

Add Header Files

  • Add dynamixel_sdk/dynamixel_sdk.h to the top of your CPP file. This header file includes all necessary functions and classes from the DYNAMIXEL SDK.
#include "dynamixel_sdk/dynamixel_sdk.h"
#include <iostream>

Initialize Handler Objects

  • Make main function and initialize the PortHandler and PacketHandler. Set the port name and protocol version according to your DYNAMIXEL setup. The example below uses /dev/ttyUSB0 as the port name and 2.0 as the protocol version.
int main(){
dynamixel::PortHandler *portHandler = dynamixel::PortHandler::getPortHandler("/dev/ttyUSB0"); // your dxl port name
dynamixel::PacketHandler *packetHandler = dynamixel::PacketHandler::getPacketHandler(2.0); //protocol version

Open Port and Set Baud Rate

  • Open the port and set the baud rate. The example below uses 57600 as the baud rate.
portHandler->openPort();
portHandler->setBaudRate(57600);

ERROR LOGGING

openPort() and setBaudRate() functions return a boolean value indicating success or failure. If you want to check for failure, you can write like below to print an error message and exit the program.

if (portHandler->openPort()) {
std::cout << "Succeeded to open the port!\n";
} else {
std::cout << "Failed to open the port!\n";
return 0;
}

if (portHandler->setBaudRate(57600)) {
std::cout << "Succeeded to change the baudrate!\n";
} else {
std::cout << "Failed to change the baudrate!\n";
return 0;
}

Write data to enable torque

  • Turn on the torque of the DYNAMIXEL.
uint8_t dxl_id = 1;
uint16_t torque_on_address = 64;
uint8_t data = 1; // 1 to turn on the torque, 0 to turn off
packetHandler->write1ByteTxRx(portHandler, dxl_id, torque_on_address, data);
  • id : Dynamixel ID you set
  • address : The address of the data you want to write. Refer to the Control Table of your DYNAMIXEL model, which can be found in its specification manual or Dynamixel Wizard 2.0. In this example, we use X series.
  • data : The data you want to write to the specified address.

ERROR LOGGING

write1ByteTxRx() returns a communication result. If you want to check the communication result and error, you can write the code as shown below. The dxl_comm_result, dxl_error variable should be declared beforehand.

uint8_t dxl_error = 0;
int dxl_comm_result = COMM_TX_FAIL; //COMM_TX_FAIL is a constant defined in the SDK
...
dxl_comm_result = packetHandler->write1ByteTxRx(portHandler, dxl_id, torque_on_address, data, &dxl_error);

if (dxl_comm_result != COMM_SUCCESS) {
std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
} else if (dxl_error != 0) {
std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
} else {
std::cout << "Dynamixel#1 has been successfully connected \n";
}

Get User Input

  • Get user input for the target position.
int target_position;
while(true){
std::cout << "Enter target position (0 ~ 4095): ";
std::cin >> target_position;
if(target_position == -1){
break; // Exit on -1 input
} else if(target_position < 0 || target_position > 4095){
std::cout << "Position must be between 0 and 4095." << std::endl;
continue;
}

Write data to set target position

  • Write the target position to the DYNAMIXEL.
uint16_t goal_position_address = 116;
packetHandler->write4ByteTxRx(portHandler, dxl_id, goal_position_address, uint32_t(target_position));

ERROR LOGGING

write4ByteTxRx() returns a communication result. If you want to check the communication result and error, you can write the code as shown below. The dxl_comm_result, dxl_error variable should be declared beforehand.

uint8_t dxl_error = 0;
int dxl_comm_result = COMM_TX_FAIL; //COMM_TX_FAIL is a constant defined in the SDK
...
dxl_comm_result = packetHandler->write4ByteTxRx(portHandler, dxl_id, goal_position_address, uint32_t(target_position), &dxl_error);
if (dxl_comm_result != COMM_SUCCESS) {
std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
} else if (dxl_error != 0) {
std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
}

Read data from DYNAMIXEL

  • Read the current position from the DYNAMIXEL.
uint16_t present_position_address = 132;
uint32_t present_position;
do {
packetHandler->read4ByteTxRx(portHandler, dxl_id, present_position_address, &present_position);
std::cout << "Current Position: " << present_position << std::endl;
} while (abs(static_cast<int>(target_position - present_position)) > 10);
}

ERROR LOGGING

read4ByteTxRx() returns a communication result. If you want to check the communication result and error, you can write the code as shown below. The dxl_comm_result, dxl_error variable should be declared beforehand.

uint8_t dxl_error = 0;
int dxl_comm_result = COMM_TX_FAIL; //COMM_TX_FAIL is a constant defined in the SDK
...
dxl_comm_result = packetHandler->read4ByteTxRx(portHandler, dxl_id, present_position_address, &present_position, &dxl_error);
if (dxl_comm_result != COMM_SUCCESS) {
std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
} else if (dxl_error != 0) {
std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
}
  • Turn off the torque when while loop is exited. And close the port.
data = 0; // 0 to turn off the torque
packetHandler->write1ByteTxRx(portHandler, dxl_id, torque_on_address, data);
portHandler->closePort();

return 0;
}

Compile and Run

  • Compile the code using g++.
$ g++ my_read_write.cpp -o my_read_write -ldxl_x64_cpp
$ ./my_read_write

Full Source Code

#include "dynamixel_sdk/dynamixel_sdk.h"
#include <iostream>

int main(){
dynamixel::PortHandler *portHandler = dynamixel::PortHandler::getPortHandler("/dev/ttyUSB0");
dynamixel::PacketHandler *packetHandler = dynamixel::PacketHandler::getPacketHandler(2.0);
if (portHandler->openPort()) {
std::cout << "Succeeded to open the port!\n";
} else {
std::cout << "Failed to open the port!\n";
return 0;
}

if (portHandler->setBaudRate(57600)) {
std::cout << "Succeeded to change the baudrate!\n";
} else {
std::cout << "Failed to change the baudrate!\n";
return 0;
}

uint8_t dxl_id = 1;
uint16_t torque_on_address = 64;
uint8_t data = 1;
uint8_t dxl_error = 0;
int dxl_comm_result = COMM_TX_FAIL;

dxl_comm_result = packetHandler->write1ByteTxRx(portHandler, dxl_id, torque_on_address, data, &dxl_error);
if (dxl_comm_result != COMM_SUCCESS) {
std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
} else if (dxl_error != 0) {
std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
} else {
std::cout << "Dynamixel#1 has been successfully connected \n";
}

int target_position;
while(true){
std::cout << "Enter target position (0 ~ 4095): ";
std::cin >> target_position;
if(target_position == -1){
break; // Exit on -1 input
} else if(target_position < 0 || target_position > 4095){
std::cout << "Position must be between 0 and 4095." << std::endl;
continue;
}

uint16_t goal_position_address = 116;
dxl_comm_result = packetHandler->write4ByteTxRx(portHandler, dxl_id, goal_position_address, uint32_t(target_position), &dxl_error);
if (dxl_comm_result != COMM_SUCCESS) {
std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
} else if (dxl_error != 0) {
std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
}

uint16_t present_position_address = 132;
uint32_t present_position;
do {
dxl_comm_result = packetHandler->read4ByteTxRx(portHandler, dxl_id, present_position_address, &present_position, &dxl_error);
if (dxl_comm_result != COMM_SUCCESS) {
std::cout << packetHandler->getTxRxResult(dxl_comm_result) << std::endl;
} else if (dxl_error != 0) {
std::cout << packetHandler->getRxPacketError(dxl_error) << std::endl;
}
std::cout << "Current Position: " << present_position << std::endl;
} while (abs(static_cast<int>(target_position - present_position)) > 10);
}

data = 0;
packetHandler->write1ByteTxRx(portHandler, dxl_id, torque_on_address, data);
portHandler->closePort();

return 0;
}