python_groupsyncread
-
Description
Base functions for simultaneous dynamixel control on reading to same length data on same control table address. The function is unavailable in protocol 1.0.
-
Members
None
-
Methods
| Methods | Description |
|---|---|
| GroupSyncRead | Initializes members of packet data pointer struct |
| addParam | Adds parameter storage for read |
| removeParam | Removes parameter on the storage |
| clearParam | Clears parameter storage |
| txPacket | Transmits packet to the number of DYNAMIXEL's |
| rxPacket | receives packet from the number of DYNAMIXEL's |
| txRxPacket | Transmits and receives packet on the number of DYNAMIXEL's |
| isAvailable | Checks whether there is available data in the data storage |
| getData | Gets data from received packet |
-
Enumerator
None
Method References
GroupSyncRead
- Syntax
GroupSyncRead(port, ph, start_address, data_length)
- Parameters
| Parameters | Description |
|---|---|
| port | PortHandler instance |
| ph | PacketHandler instance |
| start_address | Control table address to start reading data |
| data_length | Total data length |
-
Detailed Description
This function initializes the parameters for packet construction. The function resizes groupData struct and initialzes struct members.
addParam
- Syntax
addParam(dxl_id)
- Parameters
| Parameters | Description |
|---|---|
| dxl_id | DYNAMIXEL ID |
-
Detailed Description
This function pushes id to the DYNAMIXEL ID list, and initializes parameter storage It returns false when the class uses Protocol 1.0, or it returns true.
removeParam
- Syntax
removeParam(dxl_id)
- Parameters
| Parameters | Description |
|---|---|
| dxl_id | DYNAMIXEL ID |
-
Detailed Description
This function removes id and its data for write in the DYNAMIXEL ID list. It returns false when the class uses Protocol 1.0 or target ID does not exists in the ID list, or returns true.
clearParam
- Syntax
clearParam()
- Parameters
None
-
Detailed Description
This function clears DYNAMIXEL ID list. It returns false when the class uses Protocol 1.0, or returns true.
txPacket
- Syntax
txPacket()
- Parameters
None
-
Detailed Description
This function transmits the packet by using
syncReadTxfunction. The communication result and the hardware error are available when the function is terminated.
rxPacket
- Syntax
rxPacket()
- Parameters
None
-
Detailed Description
This function receives the packet by using
readRxfunction. The communication result and the hardware error are available when the function is terminated.
txRxPacket
- Syntax
txRxPacket()
- Parameters
None
-
Detailed Description
This function transmits and receives the packet by using
txPacketfunction andrxPacketfunction. The communication result and the hardware error are available when the function is terminated.
isAvailable
- Syntax
isAvailable(dxl_id, address, data_length)
- Parameters
| Parameters | Description |
|---|---|
| dxl_id | DYNAMIXEL ID |
| address | Address on the control table of DYNAMIXEL |
| data_length | data length |
-
Detailed Description
This function checks whether there is available data in the data storage. It returns false when used Protocol is 1.0 version or there is no data from target address, or returns true.
getData
- Syntax
getData(dxl_id, address, data_length)
- Parameters
| Parameters | Description |
|---|---|
| dxl_id | DYNAMIXEL ID |
| address | Address on the control table of DYNAMIXEL |
| data_length | data length |
-
Detailed Description
This function gets specific data from received packet. It returns false when the class uses Protocol 1.0 or there is no data from target address, or returns true.