labview_groupbulkread
-
Description
Base functions for simultaneous dynamixel control on reading to different length data on different control table address.
-
Members
None
-
Methods
| Methods | Description |
|---|---|
| groupBulkRead | Initializes members of packet data pointer struct |
| groupBulkReadAddParam | Adds parameter storage for read |
| groupBulkReadRemoveParam | Removes parameter on the storage |
| groupBulkReadClearParam | Clears parameter storage |
| groupBulkReadTxPacket | Transmits packet to the number of DYNAMIXEL's |
| groupBulkReadRxPacket | receives packet from the number of DYNAMIXEL's |
| groupBulkReadTxRxPacket | Transmits and receives packet on the number of DYNAMIXEL's |
| groupBulkReadIsAvailable | Checks whether there is available data in the data storage |
| groupBulkReadGetData | Gets data from received packet |
-
Enumerator
None
Method References
groupBulkRead
- Syntax
int groupBulkRead(int port_num, int protocol_version)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| protocol_version | Protocol version |
-
Detailed Description
This function initializes the parameters for packet construction. The function resizes groupData struct and initialzes struct members.
groupBulkReadAddParam
- Syntax
uint8_t groupBulkReadAddParam(int group_num, uint8_t id, uint16_t start_address, uint16_t data_length)
- Parameters
| Parameters | Description |
|---|---|
| group_num | Group number |
| id | DYNAMIXEL ID |
| start_address | Start address |
| data_length | Data length |
-
Detailed Description
This function pushes
idto the DYNAMIXEL ID list, and initializes the parameter storage bysetting start_addressanddata_length.
groupBulkReadRemoveParam
- Syntax
void groupBulkReadRemoveParam(int group_num, uint8_t id)
- Parameters
| Parameters | Description |
|---|---|
| group_num | Group number |
| id | DYNAMIXEL ID |
-
Detailed Description
This function removes target
idin the #group_numDYNAMIXEL ID list. It returns 0(false) when the class uses Protocol 1.0 .
groupBulkReadClearParam
- Syntax
void groupBulkReadClearParam(int group_num)
- Parameters
| Parameters | Description |
|---|---|
| group_num | Group number |
-
Detailed Description
This function clears the #
group_numDYNAMIXEL ID list. It returns 0(false) when the class uses Protocol 1.0, or returns 1(true).
groupBulkReadTxPacket
- Syntax
void groupBulkReadTxPacket(int group_num)
- Parameters
| Parameters | Description |
|---|---|
| group_num | Group number |
-
Detailed Description
This function transmits the packet by using
BulkReadTxThe communication result and the hardware error are available when the function is terminated.
groupBulkReadRxPacket
- Syntax
void groupBulkReadRxPacket(int group_num)
- Parameters
| Parameters | Description |
|---|---|
| group_num | Group number |
-
Detailed Description
This function receives the packet by using
ReadRxfunction. The communication result and the hardware error are available when the function is terminated.
groupBulkReadTxRxPacket
- Syntax
void groupBulkReadTxRxPacket(int group_num)
- Parameters
| Parameters | Description |
|---|---|
| group_num | Group number |
-
Detailed Description
This function transmits and receives the packet by using
groupBulkReadTxPacketfunction andgroupBulkReadRxPacketfunction. The communication result and the hardware error are available when the function is terminated.
groupBulkReadIsAvailable
- Syntax
uint8_t groupBulkReadIsAvailable(int group_num, uint8_t id, uint16_t address, uint16_t data_length)
- Parameters
| Parameters | Description |
|---|---|
| id | DYNAMIXEL ID |
| address | Address on the control table of DYNAMIXEL |
| data | Packet data |
-
Detailed Description
This function checks whether there is available data in the data storage. It returns 0(false) when there is no data from target address, or returns 1(true).
groupBulkReadGetData
- Syntax
uint32_t groupBulkReadGetData(int group_num, uint8_t id, uint16_t address, uint16_t data_length)
- Parameters
| Parameters | Description |
|---|---|
| group_num | Group number |
| id | DYNAMIXEL ID |
| address | Address on the control table of DYNAMIXEL |
| data_length | Data length |
-
Detailed Description
This function gets specific data from received packet. It returns 0(false) when there is no data from target address, or returns 1(true).