Skip to main content

csharp_groupsyncread

CSharp GroupSyncRead

  • Description

    Base functions for simultaneous dynamixel control on reading to same length data on same control table address. The function is unavailable in protocol 1.0.

  • Members

    None

  • Methods

MethodsDescription
groupSyncReadInitializes members of packet data pointer struct
groupSyncReadAddParamAdds parameter storage for read
groupSyncReadRemoveParamRemoves parameter on the storage
groupSyncReadClearParamClears parameter storage
groupSyncReadTxPacketTransmits packet to the number of DYNAMIXEL's
groupSyncReadRxPacketreceives packet from the number of DYNAMIXEL's
groupSyncReadTxRxPacketTransmits and receives packet on the number of DYNAMIXEL's
groupSyncReadIsAvailableChecks whether there is available data in the data storage
groupSyncReadGetDataGets data from received packet
  • Enumerator

    None

Method References

groupSyncRead
  • Syntax
int groupSyncRead(int port_num, int protocol_version, UInt16 start_address, UInt16 data_length)
  • Parameters
ParametersDescription
port_numPort number
protocol_versionProtocol version
start_addressControl table address to start reading data
data_lengthTotal data length
  • Detailed Description

    This function initializes the parameters for packet construction. The function resizes groupData struct and initialzes struct members.

groupSyncReadAddParam
  • Syntax
bool groupSyncReadAddParam(int group_num, byte id)
  • Parameters
ParametersDescription
group_numGroup number
idDYNAMIXEL ID
  • Detailed Description

    This function pushes id to the DYNAMIXEL ID list, and initializes #group_num parameter storage It returns false when the class uses Protocol 1.0, or it returns true.

groupSyncReadRemoveParam
  • Syntax
void groupSyncReadRemoveParam(int group_num, byte id)
  • Parameters
ParametersDescription
group_numGroup number
idDYNAMIXEL ID
  • Detailed Description

    This function removes id and its data for write in the #group_num DYNAMIXEL ID list. It returns false when the class uses Protocol 1.0 or target ID does not exists in the ID list, or returns true.

groupSyncReadClearParam
  • Syntax
void groupSyncReadClearParam(int group_num)
  • Parameters
ParametersDescription
group_numGroup number
  • Detailed Description

    This function clears #group_num DYNAMIXEL ID list. It returns false when the class uses Protocol 1.0, or returns true.

groupSyncReadTxPacket
  • Syntax
int groupSyncReadTxPacket(int group_num)
  • Parameters
ParametersDescription
group_numGroup number
  • Detailed Description

    This function transmits the packet by using SyncReadTx function. The communication result and the hardware error are available when the function is terminated.

groupSyncReadRxPacket
  • Syntax
int groupSyncReadRxPacket(int group_num)
  • Parameters
ParametersDescription
group_numGroup number
  • Detailed Description

    This function receives the packet by using ReadRx function. The communication result and the hardware error are available when the function is terminated.

groupSyncReadTxRxPacket
  • Syntax
int groupSyncReadTxRxPacket(int group_num)
  • Parameters
ParametersDescription
group_numGroup number
  • Detailed Description

    This function transmits and receives the packet by using TxPacket function and RxPacket function. The communication result and the hardware error are available when the function is terminated.

groupSyncReadIsAvailable
  • Syntax
bool groupSyncReadIsAvailable(int group_num, byte id, UInt16 address, UInt16 data_length)
  • Parameters
ParametersDescription
idDYNAMIXEL ID
addressAddress on the control table of DYNAMIXEL
dataPacket data
  • Detailed Description

    This function checks whether there is available data in the data storage. It returns false when used Protocol is 1.0 version or there is no data from target address, or returns true.

groupSyncReadGetData
  • Syntax
UInt32 groupSyncReadGetData(int group_num, byte id, UInt16 address, UInt16 data_length)
  • Parameters
ParametersDescription
group_numGroup number
idDYNAMIXEL ID
addressAddress on the control table of DYNAMIXEL
dataPacket data
  • Detailed Description

    This function gets specific data from received packet. It returns false when the class uses Protocol 1.0 or there is no data from target address, or returns true.