API Reference
C
C PortHandler
-
Description : Base functions for serial communication.
-
Members
| Members | Description |
|---|---|
| DEFAULT_BAUDRATE | :=1000000 Default Baudrate |
| g_used_port_num | Shows how much ports are in-use |
| g_is_using | Shows whether the port is in-use |
- Methods
| Methods | Description |
|---|---|
| portHandler | Initializes members of port data pointer struct |
| openPort | Opens a serial port |
| closePort | Closes a serial port |
| clearPort | Refreshes a serial port |
| setPortName | Sets a device name |
| getPortName | Gets a device name |
| setBaudrate | Sets a baudrate |
| getBaudrate | Gets a baudrate |
| getBytesAvailable | Checks how many bytes can be read in port buffer (Linux only) |
| readPort | Reads bytes from port buffer |
| writePort | Writes bytes to port buffer |
| setPacketTimeout | Sets timeout |
| setPacketTimeoutMSec | Sets timeout using micro second value |
| isPacketTimeout | Checks whether communication has been succeeded in timeout |
- Enumerator : None
Method References
C PortHandlerWindows
-
Description
PortHandler dependent functions for serial communication on Windows OS.
-
Members
None
-
Methods
| Methods | Description |
|---|---|
| portHandlerWindows | Initializes parameters for serial port control |
| openPortWindows | Opens a serial port |
| closePortWindows | Closes a serial port |
| clearPortWindows | Refreshes a serial port |
| setPortNameWindows | Sets a device name |
| getPortNameWindows | Gets a device name |
| setBaudrateWindows | Sets a baudrate |
| getBaudrateWindows | Gets a baudrate |
| readPortWindows | Reads bytes from port buffer |
| writePortWindows | Writes bytes to port buffer |
| setPacketTimeoutWindows | Sets timeout |
| setPacketTimeoutMSecWindows | Sets timeout using micro second |
| isPacketTimeoutWindows | Checks whether communication has been succeeded in timeout |
| getCurrentTimeWindows | Gets a current time |
| getTimeSinceStartWindows | Gets a time since start |
| setupPortWindows | Sets a port |
-
Enumerator
None
Method References
portHandlerWindows
- Syntax
int portHandlerWindows(const char *port_name)
- Parameters
| Parameters | Description |
|---|---|
| port_name | Port name |
-
Detailed Description
The function initializes the parameters for port control. At first, this checks if the port with same device name is set already in the
portDataWindowspointer struct. If it exists, the function returns the port number as what it has. If not, the function finds any free port, resizeportDataWindowsstruct and start to initialize struct members.
openPortWindows
- Syntax
uint8_t openPortWindows(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function opens the port by
SetBaudRateWindowsfunction usingDEFAULT_BAUDRATE. If the baudrate is needed to be changed to another baudrate value,SetBaudRateWindowsfunction should be called again after callingopenPortWindowsfunction. When the port succeeds to be opened, this function will return true, and if not, then false.
closePortWindows
- Syntax
void closePortWindows(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function sets
serial_handle_member ofportDataWindowsstruct toINVALID_HANDLE_VALUEso that the #port_numport won't be activated.
clearPortWindows
- Syntax
void clearPortWindows(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function clears the port by purging the RX buffer.
setPortNameWindows
- Syntax
void setPortNameWindows(int port_num, const char *port_name)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| port_name | Port name |
-
Detailed Description
This function sets the device name of the #
port_numport asport_name.
getPortNameWindows
- Syntax
char *getPortNameWindows(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function returns the device name which the #
port_numport is using.
setBaudrateWindows
- Syntax
uint8_t setBaudrateWindows(int port_num, const int baudrate)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| baudrate | Target baudrate |
-
Description
This function converts baudrate to baudrate type value at first. Secondly, it closes the port with ClosePort function, and opens the port with SetupPort function again. Finally, it returns port setup result.
getBaudrateWindows
- Syntax
int getBaudrateWindows(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function returns the baudrate value previously set.
readPortWindows
- Syntax
int readPortWindows(int port_num, uint8_t *packet, int length)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| packet | The number of data bytes read previously |
| length | Byte length for read |
-
Description
This function gets length byte data from port buffer and returns a number of read data bytes. On end-of-file, 0 is returned, on error it returns -1.
writePortWindows
- Syntax
int writePortWindows(int port_num, uint8_t *packet, int length)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| packet | The number of data bytes to write |
| length | Byte length for write |
-
Description
This function transmits length byte, and returns how much the data was written. On error, it returns -1.
setPacketTimeoutWindows
- Syntax
void setPacketTimeoutWindows (int port_num, uint16_t packet_length)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| packet_length | Target byte length for write |
-
Description
This function sets the start time when it transmits the packet, and set the timeout of packet transmission to be ready for deciding communication result.
SetPacketTimeoutMSecWindows
- Syntax
void SetPacketTimeoutMSecWindows (int port_num, double msec)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| msec | Miliseconds |
-
Description
This function sets the start time with
msecmilisecond value when it transmits the packet, and set the timeout of packet transmission to be ready for deciding communication result.
isPacketTimeoutWindows
- Syntax
uint8_t isPacketTimeoutWindows (int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function decides the timeover of packet communication. If the time limit is over, it returns false.
getCurrentTimeWindows
- Syntax
double getCurrentTimeWindows(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function gets a current time.
getTimeSinceStartWindows
- Syntax
double getTimeSinceStartWindows(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function gets a time since start.
setupPortWindows
- Syntax
uint8_t setupPortWindows (int port_num, const int baudrate)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| baudrate | Target baudrate |
-
Description
This function sets the port.
C PortHandlerLinux
-
Description
PortHandler dependent functions for serial communication on Linux OS.
-
Members
None
-
Methods
| Methods | Description |
|---|---|
| portHandleLinux | Initializes parameters for serial port control |
| openPortLinux | Opens a serial port |
| closePortLinux | Closes a serial port |
| clearPortLinux | Refreshes a serial port |
| setPortNameLinux | Sets a device name |
| getPortNameLinux | Gets a device name |
| setBaudrateLinux | Sets a baudrate |
| getBaudrateLinux | Gets a baudrate |
| getBytesAvailableLinux | Checks how many bytes can be read in port buffer |
| readPortLinux | Reads bytes from port buffer |
| writePortLinux | Writes bytes to port buffer |
| setPacketTimeoutLinux | Sets timeout |
| setPacketTimeoutMSecLinux | Sets timeout using micro second |
| isPacketTimeoutLinux | Checks whether communication has been succeeded in timeout |
| getCurrentTimeLinux | Gets a current time |
| getTimeSinceStartLinux | Gets a time since start |
| setupPortLinux | Sets a port |
| setCustomBaudrateLinux | Sets a custom baudrate |
| getCFlagBaud | Gets a baudrate |
-
Enumerator
None
Method References
portHandlerLinux
- Syntax
int portHandlerLinux(const char *port_name)
- Parameters
| Parameters | Description |
|---|---|
| port_name | Port name |
-
Detailed Description
The function initializes the parameters for port control. At first, this checks if the port with same device name is set already in the
portDataLinuxpointer struct. If it exists, the function returns the port number as what it has. If not, the function finds any free port, resizeportDataLinuxstruct and start to initialize struct members.
openPortLinux
- Syntax
uint8_t openPortLinux(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function opens the port by
SetBaudRateLinuxfunction usingDEFAULT_BAUDRATE. If the baudrate is needed to be changed to another baudrate value,SetBaudRateLinuxfunction should be called again after callingOpenPortLinuxfunction. When the port succeeds to be opened, this function will return true, and if not, then false.
closePortLinux
- Syntax
void closePortLinux(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function closes the port by closing the file descriptor.
clearPortLinux
- Syntax
void clearPortLinux(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function clears the port by flushing the file descriptor.
setPortNameLinux
- Syntax
void setPortNameLinux(int port_num, const char *port_name)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| port_name | Port name |
-
Detailed Description
This function sets the device name as port_name.
getPortNameLinux
- Syntax
char *getPortNameLinux(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function returns the device name which the port is using.
setBaudrateLinux
- Syntax
uint8_t setBaudrateLinux(int port_num, const int baudrate)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| baudrate | Target baudrate |
-
Description
This function converts
baudrateto baudrate type value at first. Secondly, it closes the port withClosePortLinuxfunction, and opens the port withSetupPortLinuxfunction again. If the value ofbaudrateis not in the compatible baudrate list, theSetCustomBaudrateLinuxfunction suggests the baudrate value which is closest of available baudrate value. Finally, it returns false.
getBaudrateLinux
- Syntax
int getBaudrateLinux(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function returns the baudrate value previously set.
getBytesAvailableLinux
- Syntax
int getBytesAvailableLinux(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function checks how much the data can be read, and returns its length.
readPortLinux
- Syntax
int readPortLinux(int port_num, uint8_t *packet, int length)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| packet | The number of data bytes read previously |
| length | Byte length for read |
-
Description
This function gets length byte data from port buffer and returns a number of read data bytes. On end-of-file, 0 is returned, on error it returns -1.
writePortLinux
- Syntax
int writePortLinux(int port_num, uint8_t *packet, int length)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| packet | The number of data bytes to write |
| length | Byte length for write |
-
Description
This function transmits length byte, and returns how much the data was written. On error, it returns -1.
setPacketTimeoutLinux
- Syntax
void setPacketTimeoutLinux (int port_num, uint16_t packet_length)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| Packet_length | Target byte length for write |
-
Description
This function sets the start time when it transmits the packet, and set the timeout of packet transmission to be ready for deciding communication result.
setPacketTimeoutMSecLinux
- Syntax
void setPacketTimeoutMSecLinux (int port_num, double msec)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| msec | Miliseconds |
-
Description
This function sets the start time with
msecmilisecond value when it transmits the packet, and set the timeout of packet transmission to be ready for deciding communication result.
isPacketTimeoutLinux
- Syntax
uint8_t isPacketTimeoutLinux(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function decides the timeover of packet communication. If the time limit is over, it returns false.
getCurrentTimeLinux
- Syntax
double getCurrentTimeLinux()
-
Parameters
None
-
Description
This function gets a current time.
getTimeSinceStartLinux
- Syntax
double getTimeSinceStartLinux(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function gets a time since start.
setupPortLinux
- Syntax
uint8_t setupPortLinux(int port_num, int cflag_baud)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| cflag_baud | Target baudrate |
-
Description
This function sets the port.
setCustomBaudrateLinux
- Syntax
uint8_t setCustomBaudrateLinux(int port_num, int speed)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| speed | communication speed |
-
Description
This function sets a custom baudrate.
getCFlagBaud
- Syntax
int getCFlagBaud(int baudrate)
- Parameters
| Parameters | Description |
|---|---|
| baudrate | Target baudrate |
-
Description
This function gets the baudrate.
C PortHandlerMac
-
Description
PortHandler dependent functions for serial communication on Mac OS.
-
Members
None
-
Methods
| Methods | Description |
|---|---|
| portHandleMac | Initializes parameters for serial port control |
| openPortMac | Opens a serial port |
| closePortMac | Closes a serial port |
| clearPortMac | Refreshes a serial port |
| setPortNameMac | Sets a device name |
| getPortNameMac | Gets a device name |
| setBaudrateMac | Sets a baudrate |
| getBaudrateMac | Gets a baudrate |
| getBytesAvailableMac | Checks how many bytes can be read in port buffer |
| readPortMac | Reads bytes from port buffer |
| writePortMac | Writes bytes to port buffer |
| setPacketTimeoutMac | Sets timeout |
| setPacketTimeoutMSecMac | Sets timeout using micro |
| isPacketTimeoutMac | Checks whether communication has been succeeded in timeout |
| getCurrentTimeMac | Gets a current time |
| getTimeSinceStartMac | Gets a time since start |
| setupPortMac | Sets a port |
| setCustomBaudrateMac | Sets a custom baudrate |
| getCFlagBaud | Gets a baudrate |
-
Enumerator
None
Method References
portHandlerMac
- Syntax
int portHandlerMac(const char *port_name)
- Parameters
| Parameters | Description |
|---|---|
| port_name | Port name |
-
Detailed Description
The function initializes the parameters for port control. At first, this checks if the port with same device name is set already in the
portDataMacpointer struct. If it exists, the function returns the port number as what it has. If not, the function finds any free port, resizeportDataMacstruct and start to initialize struct members.
openPortMac
- Syntax
uint8_t openPortMac(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function opens the port by
SetBaudRateMacfunction usingDEFAULT_BAUDRATE. If the baudrate is needed to be changed to another baudrate value,SetBaudRateMacfunction should be called again after callingOpenPortMacfunction. When the port succeeds to be opened, this function will return true, and if not, then false.
closePortMac
- Syntax
void closePortMac(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function closes the port by closing the file descriptor.
clearPortMac
- Syntax
void clearPortMac(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function clears the port by flushing the file descriptor.
setPortNameMac
- Syntax
void setPortNameMac(int port_num, const char *port_name)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| port_name | Port name |
-
Detailed Description
This function sets the device name as port_name.
getPortNameMac
- Syntax
char *getPortNameMac(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Detailed Description
This function returns the device name which the port is using.
setBaudrateMac
- Syntax
uint8_t setBaudrateMac(int port_num, const int baudrate)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| baudrate | Target baudrate |
-
Description
This function converts
baudrateto baudrate type value at first. Secondly, it closes the port withClosePortMacfunction, and opens the port withSetupPortMacfunction again. If the value ofbaudrateis not in the compatible baudrate list, theSetCustomBaudrateMacfunction suggests the baudrate value which is closest of available baudrate value. Finally, it returns false.
getBaudrateMac
- Syntax
int getBaudrateMac(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function returns the baudrate value previously set.
getBytesAvailableMac
- Syntax
int getBytesAvailableMac(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function checks how much the data can be read, and returns its length.
readPortMac
- Syntax
int readPortMac(int port_num, uint8_t *packet, int length)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| packet | The number of data bytes read previously |
| length | Byte length for read |
-
Description
This function gets length byte data from port buffer and returns a number of read data bytes. On end-of-file, 0 is returned, on error it returns -1.
writePortMac
- Syntax
int writePortMac(int port_num, uint8_t *packet, int length)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| packet | The number of data bytes to write |
| length | Byte length for write |
-
Description
This function transmits length byte, and returns how much the data was written. On error, it returns -1.
setPacketTimeoutMac
- Syntax
void setPacketTimeoutMac (int port_num, uint16_t packet_length)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| Packet_length | Target byte length for write |
-
Description
This function sets the start time when it transmits the packet, and set the timeout of packet transmission to be ready for deciding communication result.
setPacketTimeoutMSecMac
- Syntax
void setPacketTimeoutMSecMac (int port_num, double msec)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| msec | Miliseconds |
-
Description
This function sets the start time with
msecmilisecond value when it transmits the packet, and set the timeout of packet transmission to be ready for deciding communication result.
isPacketTimeoutMac
- Syntax
uint8_t isPacketTimeoutMac(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function decides the timeover of packet communication. If the time limit is over, it returns false.
getCurrentTimeMac
- Syntax
double getCurrentTimeMac()
-
Parameters
None
-
Description
This function gets a current time.
getTimeSinceStartMac
- Syntax
double getTimeSinceStartMac(int port_num)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
-
Description
This function gets a time since start.
setupPortMac
- Syntax
uint8_t setupPortMac(int port_num, int cflag_baud)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| cflag_baud | Target baudrate |
-
Description
This function sets the port.
setCustomBaudrateMac
- Syntax
uint8_t setCustomBaudrateMac(int port_num, int speed)
- Parameters
| Parameters | Description |
|---|---|
| port_num | Port number |
| speed | communication speed |
-
Description
This function sets a custom baudrate.
getCFlagBaud
- Syntax
int getCFlagBaud(int baudrate)
- Parameters
| Parameters | Description |
|---|---|
| baudrate | Target baudrate |
-
Description
This function gets the baudrate.