Skip to main content

noVNC

noVNC lets you access a remote desktop on the robot PC through a web browser without connecting an HDMI monitor. Cyclo Manager starts a noVNC server container that provides its own desktop environment, where you can use graphical applications such as DYNAMIXEL Wizard 2.

Use the Remote Desktop​

1. Start the noVNC Server​

Open noVNC in the Cyclo Manager navigation. Click the start button in NOVNC SERVER at the top of the page to start the noVNC container. Wait for the server to start and the connection screen to appear.

noVNC server start and log buttons

2. Connect to the Desktop​

Click Connect (연결 in the screenshot) to open the remote desktop.

noVNC connection screen with the Connect button
tip

If a connection failure message appears just after starting the server for the first time, refresh the Cyclo Manager page and connect again.

The remote desktop appears as shown below.

Connected noVNC desktop with the DYNAMIXEL Wizard 2 shortcut

3. Open DYNAMIXEL Wizard 2​

Open the Dynamixel Wizard 2 shortcut on the desktop to use DYNAMIXEL Wizard 2 in your browser. You can also open other installed tools from their desktop shortcuts.

DYNAMIXEL Wizard 2 open in the noVNC desktop

When finished, use the stop button in NOVNC SERVER at the top of the page to stop the noVNC container.