Skip to main content

Dashboard

Use Dashboard to monitor the Robot PC and manage containers, images, and software versions.

Dashboard Overview​

Dashboard brings system status, container management, and version management together on one page.

Cyclo Manager dashboard

System Status​

The System Status panel shows the Robot PC's CPU and memory usage, system and SSD storage usage, and temperature when available.

System Status panel showing CPU, memory, storage, and temperature

Click CPU to open CPU Usage and inspect the host processes using CPU resources. The panel shows overall CPU and memory usage, followed by each process's PID, user, CPU and memory usage, resident memory (RSS), and command.

CPU Usage panel showing host process resource usage

Container Management​

Manage Containers​

The Container Management panel lists Docker containers and their status. For each container, you can:

  • Start, stop, or restart the container.
  • View the container's logs.
  • Open a terminal inside the container.
  • View and edit the container's .bashrc configuration.

Container management

Use the .bashrc control for a container to inspect and edit its shell configuration. Changes do not alter the environment of already-running processes; restart the affected services or container when required.

Editing a container bashrc

Manage Docker Images​

Open Docker image management from the container management area to review image tags, size, and container usage. Delete an unused image or prune dangling images when needed. Images used by a container cannot be removed from this screen.

Docker image management

Version Management​

Use Version Management to inspect and update supported software packages, Cyclo Manager, and container agents.

Version management

Package Update​

Use Package Update to update a supported robot software repository and recreate its container. Click Update when an update is available.

Package update procedure
  1. Stop the running container when prompted.

    Stop the container before updating

  2. Choose how to handle local changes. Updates are supported on the main and jazzy branches.

    Choose how to handle local changes

  3. Select files to preserve as needed, including any robot-specific configuration.

    Select files to preserve

  4. Continue the update. Cyclo Manager updates the repository and recreates the container. Downloading an image may take several minutes.

    Update the repository and recreate the container

    Package update result

Cyclo Manager Update​

Use Cyclo Manager Update to update the CLI package and restart the Manager stack with matching API and web UI images. Click Update when a new version is available, then reopen the web UI after the update.

Cyclo Manager update details

Cyclo Manager update

The update also restarts the host agent. If the web update fails, connect to the Robot PC and run:

cyclo_manager update

You can also update manually from a terminal on the Robot PC:

pip install -U cyclo-manager
cyclo-manager down
cyclo-manager up --pull

The --pull option downloads the configured images before starting the updated stack. The down command stops and removes the Manager stack and its host-agent service; up sets them up again. Both cyclo-manager and cyclo_manager are supported command names.

Agent Update​

Use Agent Update when the s6 agent inside a managed container is incompatible with the installed Cyclo Manager version. In Container Agents, click Update for the affected container. The container may restart during the update.

Agent update screen

Container agent update