Model Inference with Web UI
Once your model is trained, you can deploy it on the AI Worker for inference.
Model Deployment and Inference
1. Prepare Your Model
Choose one of the following methods.
Option 1) Download your model from Hugging Face
You can download a policy model from Hugging Face. Detailed steps are provided below.
You can proceed to the next step: 👉 2. Launch the ROS 2 Follower Node
Option 2) Manually copy your model to the target directory
Please place your trained model in the following directory:
ROBOT PC
~/physical_ai_tools/lerobot/outputs/train/
Models trained on the Robot PC using Physical AI Tools are automatically saved to this path. However, if you downloaded the model from a hub (without using Physical AI Tools) or copied it from another PC, you need to move the model to this location.
Available Folder Structures
Please refer to the folder structure tree below:
The following folder structures are all valid (example_model_folder_1, 2, 3).
~/physical_ai_tools/lerobot/outputs/train/
├── example_model_folder_1
│ └── checkpoints/
│ ├── 000250/
│ │ ├── pretrained_model/
│ │ │ ├── config.json
│ │ │ ├── model.safetensors
│ │ │ └── train_config.json
│ │ └── training_state
│ │ ├── optimizer_param_groups.json
│ │ ├── optimizer_state.safetensors
│ │ ├── rng_state.safetensors
│ │ └── training_step.json
│ └── 000500/
│ ├── pretrained_model/
| │ └─ (...)
│ └── training_state/
| └─ (...)
├── example_model_folder_2/
│ ├── pretrained_model/
| | └─ (...)
│ └── training_state
| └─ (...)
└── example_model_folder_3/
├── config.json
├── model.safetensors
└── train_config.json
To copy your model from the User PC to the Robot PC, use the following command:
- Change ownership of the model directory.
ROBOT PC (not inside the Docker container)
sudo chown -R robotis ./
- Copy the model from the User PC to the Robot PC using the
scpcommand:
USER PC
scp -r <your model folder's directory> robotis@ffw-<your robot's serial number>.local:~/physical_ai_tools/lerobot/outputs/train
After placing the model in the above directory, you can access it from within the Docker container at:
/root/ros2_ws/src/physical_ai_tools/lerobot/outputs/train/
2. Launch the ROS 2 Follower Node
Please deactivate the ROS 2 teleoperation node launched in the Prerequisites > Launch the ROS 2 teleoperation node section before proceeding.
ROBOT PC
cd ~/ai_worker/docker && ./container.sh enter
ROBOT PC 🐋 AI WORKER
- FFW-BG2
- FFW-SG2
ffw_bg2_follower_ai
ffw_sg2_follower_ai
3. Run Inference
a. Launch Physical AI Server
If the Physical AI Server is already running, you can skip this step.
Enter the Physical AI Tools Docker container:
ROBOT PC
cd ~/physical_ai_tools && ./docker/container.sh enter
Then, launch the Physical AI Server with the following command:
ROBOT PC 🐋 PHYSICAL AI TOOLS
ai_server
b. Open the Web UI
Open your web browser and navigate the Web UI (Physical AI Manager).
(Refer to the Dataset Preparation > Recording > 1. Open the Web UI)
On the Home page, select the type of robot you are using.
c. Enter Task Instruction and Policy Path
Go to the Inference Page.
Enter Task Instruction and Policy Path in the Task Info Panel, located on the right side of the page.
- Task Information Field Descriptions
| Item | Description |
|---|---|
| Task Instruction | A sentence that tells the robot what action to perform, such as "pick and place object". |
Policy Path 🐋 PHYSICAL AI TOOLS | The absolute path to your trained model directory inside the Docker container(🐋 PHYSICAL AI TOOLS). This should point to the folder containing your trained model files such as config.json, model.safetensors, and train_config.json. See the Policy Path Example below for reference. |
| FPS | FPS should be set to the same FPS at which you collected the training data for your model, which serves as the control frequency. |
Entering Policy Path
You can either click the Browse Policy Path button to select the desired model folder, or directly enter the desired path in the text input field.


Download Policy Model from Hugging Face
You can download your model from Hugging Face.
Click the Download Policy button to open a popup for downloading a policy model.


Select the Hugging Face User ID and enter the repository to download.
Click the Download button to start the download.
When the download completes, click Finish to close the popup.
The downloaded model path is automatically filled into Policy Path.

⚠️ Important — Network recommendation: Policy models are typically large in size. A wired Ethernet connection is highly recommended for downloading to ensure stable and fast download speeds.
Policy Path Example
/root/ros2_ws/src/physical_ai_tools/lerobot/outputs/train/
└── example_model_folder/
├── pretrained_model/ # ← This folder contains config.json, model.safetensors, train_config.json
│ ├── config.json
│ ├── model.safetensors
│ └── train_config.json
└── training_state/
├── optimizer_param_groups.json
├── optimizer_state.safetensors
├── rng_state.safetensors
└── training_step.json
For a model folder structure like the one above, the Policy Path would be:
/root/ros2_ws/src/physical_ai_tools/lerobot/outputs/train/example_model_folder/pretrained_model/
Recording during inference will be supported in a future update. Coming soon!
d. Start Inference
To begin inference, use the Control Panel located at the bottom of the page:
- The
Startbutton begins inference. - The
Finishbutton stops inference.