Skip to main content

write

Description

This function writes data to specific memory addresses of DYNAMIXEL with a specific ID.

Syntax

  • write(id, addr, *p_data, data_length, timeout_ms)

Parameters

  • id : ID of a specific DYNAMIXEL. Data type : unsigned int8
  • addr : Specific memory address of DYNAMIXEL to write. Data type : unsigned int16
  • *p_data : Address of buffer that contains the data to send. Data type : unsigned int8 pointer
  • data_length : Size of the data in byte. Data type : unsigned int16
  • timeout_ms : Set Timeout in milliseconds. Data type : unsigned int32

Returns

  • True(1) on success.
  • False(0) on failure.

Example

#define LED_ADDR 65
#define LED_ADDR_LEN 1
#define TIMEOUT 10 //default communication timeout 10ms

const uint8_t DXL_DIR_PIN = 2; // DYNAMIXEL Shield DIR PIN
const uint8_t DXL_ID = 1;
const float DXL_PROTOCOL_VERSION = 2.0;
const uint8_t turn_on = 1;
const uint8_t turn_off = 0;

Dynamixel2Arduino dxl(DXL_SERIAL, DXL_DIR_PIN);

void setup() {
DEBUG_SERIAL.begin(115200);
dxl.begin(57600);
dxl.setPortProtocolVersion(DXL_PROTOCOL_VERSION);
}

void loop() {
// put your main code here, to run repeatedly:

// LED On
if(!dxl.write(DXL_ID, LED_ADDR, (uint8_t*)&turn_on, LED_ADDR_LEN, TIMEOUT)) {
DEBUG_SERIAL.println("Failed to turn on the LED.");
}
delay(500);

// LED Off
if(!dxl.write(DXL_ID, LED_ADDR, (uint8_t*)&turn_off, LED_ADDR_LEN, TIMEOUT)) {
DEBUG_SERIAL.println("Failed to turn off the LED.");
}
delay(500);
}