setGoalPWM
Description
This function controls PWM of DYNAMIXEL.
Syntax
- setGoalPWM(id, value, unit)
Parameters
- id : ID of a specific DYNAMIXEL. Data type : unsigned int8
- value : Goal PWM value in raw value(default) or percentage. Data type : float
- unit : Types of value. Data type : unsigned int8
- For raw value : UNIT_RAW (default)
- For Percentage value : UNIT_PERCENT
Returns
- True(1) on success.
- False(0) on failure.
Example
const int DXL_DIR_PIN = 2;
Dynamixel2Arduino dxl(Serial1, DXL_DIR_PIN);
dxl.setGoalPWM(1, 100); //use default raw value
dxl.setGoalPWM(2, 50.0, UNIT_PERCENT); //use percentage (-100 ~ 100 %)