getTorqueEnableStat
Description
getTorqueEnableStat() returns whether the torque of specific DYNAMIXEL is turned on or off.
Syntax
- getTorqueEnableStat(id)
Parameters
- id : ID of a specific DYNAMIXEL. Data type : unsigned int8
Returns
- True(1) when the torque is turned on.
- False(0) when the torque is turned off.
Example
Dynamixel2Arduino dxl(Serial1, DXL_DIR_PIN);
dxl.getTorqueEnableStat(1);