getPresentVelocity
Description
This function gets present velocity(wheel mode speed) of DYNAMIXEL.
Syntax
- getPresentVelocity(id, unit)
Parameters
- id : ID of a specific DYNAMIXEL. Data type : unsigned int8
- unit : Types of value. Data type : unsigned int8
- For raw value : UNIT_RAW (default)
- For RPM value : UNIT_RPM
- For Percentage value : UNIT_PERCENT
Returns
- Velocity value on success.
- False(0) on failure. Use
getLastErrorCode()to see if this value indicates an error.
Example
const int DXL_DIR_PIN = 2;
Dynamixel2Arduino dxl(Serial1, DXL_DIR_PIN);
Serial.print(dxl.getPresentVelocity(1)); //use default raw value
Serial.print(dxl.getPresentVelocity(2, UNIT_RPM)); //use RPM
Serial.print(dxl.getPresentVelocity(3, UNIT_PERCENT)); //use percentage (-100 ~ 100 %)