getPresentCurrent
Description
This function gets present current of DYNAMIXEL.
Syntax
- getPresentCurrent(id, value, unit)
Parameters
- id : ID of a specific DYNAMIXEL. Data type : unsigned int8
- value : Present Current value in raw value(default) or milli amphere or percentage. Data type : float
- unit : Types of value. Data type : unsigned int8
- For raw value : UNIT_RAW (default)
- For milli amphere(mA) : UNIT_MILLI_AMPERE
- For Percentage value : UNIT_PERCENT
Returns
- Present Current value on success.
- False(0) on failure. Use
getLastErrorCode()to see if this value indicates an error.
Example
const int DXL_DIR_PIN = 2;
Dynamixel2Arduino dxl(Serial1, DXL_DIR_PIN);
Serial.print(dxl.getPresentCurrent(1)); //use default raw value
Serial.print(dxl.getPresentCurrent(2, UNIT_MILLI_MAPERE)); //use mA
Serial.print(dxl.getPresentCurrent(3, UNIT_PERCENT)); //use percentage (-100 ~ 100 %)